Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE Support (Deutsch) 'system' cannot properly start Linux shell scripts
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 188 subscribers
  • Views 1250 views
  • Users 0 members are here
Related

'system' cannot properly start Linux shell scripts

e14 Contributor
e14 Contributor over 15 years ago

I cannot get my EAGLE 5.11.02 (Linux) to properly execute shell scripts

with parameters: The shell script 'test.sh' contains the lines

   #!/bin/bash

   echo parameter=[$1]

and, when manually executed via

   . test.sh abc

correctly outputs the text

   parameter=[abc]

 

So far, so good. From EAGLE, using the ULP syntax

   system(". test.sh abc");

by some reason only outputs

   parameter=[]

 

Is there any logical reason why EAGLE should behave that way? Do I make

wrong assumptions somewhere (I normally do NOT use Linux and therefore

do NOT know too much about it)? I'm currently trying this on

   Ubuntu 10.04 LTS - Lucid Lynx.

 

Andreas Weidner

 

 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    Am 11.09.2011 18:55, schrieb Andreas Weidner:

    I cannot get my EAGLE 5.11.02 (Linux) to properly execute shell scripts

    with parameters: The shell script 'test.sh' contains the lines

    #!/bin/bash

    echo parameter=[$1]

    and, when manually executed via

    . test.sh abc

    correctly outputs the text

    parameter=[abc]

     

    So far, so good. From EAGLE, using the ULP syntax

    system(". test.sh abc");

    by some reason only outputs

    parameter=[]

     

    Is there any logical reason why EAGLE should behave that way? Do I make

    wrong assumptions somewhere (I normally do NOT use Linux and therefore

    do NOT know too much about it)? I'm currently trying this on

    Ubuntu 10.04 LTS - Lucid Lynx.

     

    Andreas Weidner

     

     

    Why would you want to source the script from withing the system()?

    How about using system("test.sh abc") or system("./test.sh abc")?

     

    I mean, the . (source) is only useful, when you want to put the

    parameter into your current environment.

     

    main() { system(". test.sh abc"); } behaves like the behaviour you describe.

     

    --

    Christoph

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Am 13.09.2011 11:08, schrieb Christoph Kukulies:

    Why would you want to source the script from withing the system()?

     

    I do not understand your question (I understand the WORDS, but not the

    MEANING).

     

    How about using system("test.sh abc") or system("./test.sh abc")?

     

    See below.

     

    I mean, the . (source) is only useful, when you want to put the

    parameter into your current environment.

     

    As stated, I do not know Linux well. Therefore, I first test things from

    inside the shell, and afterwards try them with EAGLE's 'system' command.

    From the shell, typing

       test.sh abc

    didn't work at all. Neither did

       ./test.sh abc

    (both just produce NOTHING but error messages). Absolutely the ONLY

    thing that DID work from inside the shell was

       . test.sh abc

    which, unfortunately, doesn't work together with the 'system' command.

     

    Thanks for the tips, though. When I'm feeling extremely well and dare to

    boot into the overly confusing Linux the next time, I'll check whether

    your two suggestions work. If they DO, things are just getting even MORE

    confusing with Linux, because that would not only mean that there are

    cases when things work in the shell and NOT from EAGLE, but also the

    other way round. VERY strange.

     

    Andreas Weidner

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Am 13.09.2011 13:41, schrieb Andreas Weidner:

    Am 13.09.2011 11:08, schrieb Christoph Kukulies:

    >> Why would you want to source the script from withing the system()?

        Typo: "from within"

     

    Warum möchtest Du das Script "sourcen" (entspricht dem . (dot)-command)

     

     

    I do not understand your question (I understand the WORDS, but not the

    MEANING).

     

    >> How about using system("test.sh abc") or system("./test.sh abc")?

     

    See below.

     

    >> I mean, the . (source) is only useful, when you want to put the

    >> parameter into your current environment.

     

    As stated, I do not know Linux well. Therefore, I first test things from

    inside the shell, and afterwards try them with EAGLE's 'system' command.

    From the shell, typing

    test.sh abc

    didn't work at all. Neither did

    ./test.sh abc

    (both just produce NOTHING but error messages). Absolutely the ONLY

    thing that DID work from inside the shell was

    . test.sh abc

     

     

    wie gesagt: versuch's mit system("./test.sh abc")

    (vorher vielleicht noch ein chmod 755 test.sh)

     

    which, unfortunately, doesn't work together with the 'system' command.

     

    Thanks for the tips, though. When I'm feeling extremely well and dare to

    boot into the overly confusing Linux the next time, I'll check whether

    your two suggestions work. If they DO, things are just getting even MORE

    confusing with Linux, because that would not only mean that there are

    cases when things work in the shell and NOT from EAGLE, but also the

    other way round. VERY strange.

     

    Andreas Weidner

     

     

    --

    Christoph

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Am 13.09.2011 13:41, schrieb Andreas Weidner:

    Am 13.09.2011 11:08, schrieb Christoph Kukulies:

    >> Why would you want to source the script from withing the system()?

        Typo: "from within"

     

    Warum möchtest Du das Script "sourcen" (entspricht dem . (dot)-command)

     

     

    I do not understand your question (I understand the WORDS, but not the

    MEANING).

     

    >> How about using system("test.sh abc") or system("./test.sh abc")?

     

    See below.

     

    >> I mean, the . (source) is only useful, when you want to put the

    >> parameter into your current environment.

     

    As stated, I do not know Linux well. Therefore, I first test things from

    inside the shell, and afterwards try them with EAGLE's 'system' command.

    From the shell, typing

    test.sh abc

    didn't work at all. Neither did

    ./test.sh abc

    (both just produce NOTHING but error messages). Absolutely the ONLY

    thing that DID work from inside the shell was

    . test.sh abc

     

     

    wie gesagt: versuch's mit system("./test.sh abc")

    (vorher vielleicht noch ein chmod 755 test.sh)

     

    which, unfortunately, doesn't work together with the 'system' command.

     

    Thanks for the tips, though. When I'm feeling extremely well and dare to

    boot into the overly confusing Linux the next time, I'll check whether

    your two suggestions work. If they DO, things are just getting even MORE

    confusing with Linux, because that would not only mean that there are

    cases when things work in the shell and NOT from EAGLE, but also the

    other way round. VERY strange.

     

    Andreas Weidner

     

     

    --

    Christoph

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Am 14.09.2011 10:40, schrieb Andreas Weidner:

    Hallo Herr Kukulies,

     

    Am 13.09.2011 16:52, schrieb Christoph Kukulies:

    >> Warum möchtest Du das Script "sourcen" (entspricht dem . (dot)-command)

     

    Ich bin bei Linux extrem haeufig schwer von Begriff, daher muss ich

    leider nochmal nachfragen:

     

    UEBERSETZEN konnte ich den Text schon, aber VERSTEHEN tue ich ihn auch

    jetzt noch nicht: Ich weiss, was ein Skript ist (ich schreibe -zig). Ich

    weiss, was ein Source Code ist (ich schreibe -zig). Aber was BEDEUTET

    es, "ein Skript zu sourcen"? JEDES Skript ist fuer mich ein Source Code

     

    Hallo Herr Weidner,

     

    Der alleinstehende "." (Punkt, dot) ist ein eingebautes (built-in)

    (bourne) shell Kommando.

    csh (C-shell) kennt dafür "source" (glaube, in der bourne shell ist es

    auch alternativ zu "." möglich).

     

    Warum ihm der Begriff "source" (Quelle) gegeben wurde, kann ich im

    Moment auch nicht genau sagen. Vielleicht als Gegensatz zur sink (Senke).

     

    Ich habe gerade noch mal im Buch von Kochan/Woods "UNIX Shell

    Programming" nachgesehen. Dort steht:

     

    ...there is a shell built-in command . ((pronounced "dot") whose general

    format is

     

    . file

     

    and whose purpose is to execute the contents of file in the *current

    shell*. That is, commands from file are executed by the current shell

    *as if they were typed at the point". A subshell is not spawned by the

    program. The shell uses your PATH variable to find file, just like it

    does when executing other programs.

     

    Nun kann man vielleicht "source" besser verstehen. file wird als Quelle

    benutzt, aus der ihr Inhalt in den Punkt "fließt".

     

     

     

     

     

    irgendeiner Syntax. Kann man einen Source Code denn auch NICHT

    "sourcen"? Mir ist diese ganze Nomenklatur VOELLIG unverstaendlich.

     

    Falls Sie mir da weiterhelfen koennten, waere es vielleicht sinnvoll,

    dies unter Umgehung des Forums zu tun, damit dies nicht mit

    Erlaeuterungen gefuellt wird, die vielleicht jeder Linux-Benutzer

    auswendig weiss, nur ich eben nicht...

     

    Auf die Gefahr hin, daß ich gelyncht werde, hab' ich es jetzt trotzdem

    hier hineingeschrieben. image

     

     

    Vielen Dank fuer die Muehe,

    Andreas Weidner

     

     

    --

    Christoph Kukulies

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Am 14.09.2011 23:18, schrieb Andreas Weidner:

    Am 13.09.2011 16:52, schrieb Christoph Kukulies:

    >> wie gesagt: versuch's mit system("./test.sh abc")

     

    Hat alles nicht funktioniert.

     

    >> (vorher vielleicht noch ein chmod 755 test.sh)

     

    Aber DAS hat funktioniert und zeitigt folgende Veraenderungen:

    1. ". test.sh abc" vergisst zwar immer noch alle Parameter, aber

    2. "./test.sh abc" funktioniert jetzt OHNE Fehlermeldung.

     

    Um ein Shellskript aus EAGLE heraus zu erzeugen und danach mehrfach mit

    unterschiedlichen Parametern aufzurufen, ist also folgendes

    durchzufuehren (fuer die Leute, die genauso doof sind wie ich):

    3. Skript erzeugen mit

    output("dateinamemitpfad") printf("%s","<skriptinhalt>");

    4. Skript-Benutzerrechte veraendern mit

    system("chmod 755 'dateinamemitpfad'");

    5. Skript aufrufen mit

    system("'dateinamemitpfad' <parameter>");

     

    WUN-DER-BAR. Damit sollte ich unseren Simulatorsupport nicht nur unter

    Windows, sondern auch fuer Linux und Mac hinkriegen. Danke fuer die Hilfe.

     

    Andreas Weidner

     

     

    Zur Erläuterung Linux-Grundlagen,  drei markante Unterschiede zu Windows:

     

    a)  Bei einer Kommandoeingabe (Skript,  Anwendungsprogramm etc.) sucht

    Linux das Kommando im vorgegebenen Suchpfad (den anschauen: echo $PATH

    ),  aber aus Sicherheitsgründen absichtlich NICHT im aktuellen

    Verzeichnis.

    Einem Kommando im aktuellen Verzeichnis muss man also IMMER ./ für

    "hier" voranstellen (z.B. ./meinscript.sh ),  damit es überhaupt

    gefunden wird.  Oder den kompletten Pfad /home/meinname/meinscript.sh .

    Das könnte man zwar ändern ( . in den Suchpfad mit aufnehmen),  ist aber

    nicht empfehlenswert.

     

    Fertige Kommandos für alle Benutzer verlegt man üblicherweise nach

    /usr/local/bin (dazu root=Administrator-Rechte nötig);  das ist im

    Suchpfad,  dann klappt auch der einfache Aufruf mit zB meinscript.sh,

    und zwar für alle Benutzer.

     

    Für rein persönliche Kommandos kann man sich ein Unterverzeichnis bin

    anlegen (also /home/meinname/bin ) und das in den Pfad aufnehmen (

    PATH=$PATH:$HOME/bin )  Stellt man es vornean ( PATH=$HOME/bin:$PATH ),

      dann werden eigene Kommandos gegenüber gleichnamigen Systemkommandos

    vorrangig.

     

     

    b) Damit ein Kommando auch ausgeführt werden kann,  muss das Dateirecht

    x = Ausführbar für den betreffenden Benutzer gesetzt sein (das gibt es

    in Windows so nicht).  Bei Downloads oder mit dem Editor verfassten

    Skripten ist das zunächst nicht der Fall,  also manuell noch setzen per

    chmod 755 meinscript.sh .  (oder 750,  wenn es nur für eine bestimmte

    Benutzergruppe ausführbar sein soll;  oder 700,  wenn nur für mich.  Das

    steht oktal für je drei bits read / write /execute für Eigentümer /

    Benutzergruppe / Alle)

     

     

    c) Die Dateiendung "Extension" ist für Linux unwichtig,  rein kosmetisch

    für den Menschen.  Kommandos werden auf ihren Inhalt überprüft,  wie sie

    ausgeführt werden müssen.  Daher in Shellscripten als erste (quasi

    Kommentar-) Zeile z.B.

    #!/bin/sh

    als Anweisung, dieses Script mit dem Standard-Shell-Interpreter

    auszuführen.  Oder zB #!/bin/perl für ein Perl-Programm usw.

    Ohne diese "Hash-Bang-Zeile" müsste man das explizit angeben,  zB als

    /bin/sh ./meinscript.sh

     

    Grüße,  Hans

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Am 13.09.2011 16:52, schrieb Christoph Kukulies:

    wie gesagt: versuch's mit system("./test.sh abc")

     

    Hat alles nicht funktioniert.

     

    (vorher vielleicht noch ein chmod 755 test.sh)

     

    Aber DAS hat funktioniert und zeitigt folgende Veraenderungen:

      1. ". test.sh abc" vergisst zwar immer noch alle Parameter, aber

      2. "./test.sh abc" funktioniert jetzt OHNE Fehlermeldung.

     

    Um ein Shellskript aus EAGLE heraus zu erzeugen und danach mehrfach mit

    unterschiedlichen Parametern aufzurufen, ist also folgendes

    durchzufuehren (fuer die Leute, die genauso doof sind wie ich):

      3. Skript erzeugen mit

           output("dateinamemitpfad") printf("%s","");

     

    WUN-DER-BAR. Damit sollte ich unseren Simulatorsupport nicht nur unter

    Windows, sondern auch fuer Linux und Mac hinkriegen. Danke fuer die Hilfe.

     

    Andreas Weidner

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Hallo Herr Kukulies,

     

    Am 13.09.2011 16:52, schrieb Christoph Kukulies:

    Warum möchtest Du das Script "sourcen" (entspricht dem . (dot)-command)

     

    Ich bin bei Linux extrem haeufig schwer von Begriff, daher muss ich

    leider nochmal nachfragen:

     

    UEBERSETZEN konnte ich den Text schon, aber VERSTEHEN tue ich ihn auch

    jetzt noch nicht: Ich weiss, was ein Skript ist (ich schreibe -zig). Ich

    weiss, was ein Source Code ist (ich schreibe -zig). Aber was BEDEUTET

    es, "ein Skript zu sourcen"? JEDES Skript ist fuer mich ein Source Code

    irgendeiner Syntax. Kann man einen Source Code denn auch NICHT

    "sourcen"? Mir ist diese ganze Nomenklatur VOELLIG unverstaendlich.

     

    Falls Sie mir da weiterhelfen koennten, waere es vielleicht sinnvoll,

    dies unter Umgehung des Forums zu tun, damit dies nicht mit

    Erlaeuterungen gefuellt wird, die vielleicht jeder Linux-Benutzer

    auswendig weiss, nur ich eben nicht...

     

    Vielen Dank fuer die Muehe,

    Andreas Weidner