Is it possible to auto route just a partial part of the board?
Is it possible to auto route just a partial part of the board?
My previous post was written poorly and does not really work as described.
After a bit more testing on more complex designs:
Autorouting happens within the extremities of your design (components) and
limited by a dimension line outside of that area. If you draw the board
outline in the middle of your design the autorouter will route airwires
inside and outside that outline but not those that cross the outline.
Now, to recover from my previous post, it can be made to work the following
way:
Block out 'all' the area of your design that you do not want routed using
rectangles, or draw a polygon, on the 20-Dimension layer leaving only the
area of interest. You can leave your board outline, no need to move it to
another layer.
The exposed area alone will route. Airwires beneath the rectangles/polygon
and emerging from it will not route.
Remeber that there is a DRC setting for copper clearance from items in the
dimension layer so when you build the area to route make it a little
larger.
Deleting this 'blocking' from the Dimension layer later maybe safer/easier
than using the Restrict layers. This technique masks both the top and
bottom layers at the same time making it quicker than the restrict method
when identical top/bottom masking is required.
Try it, it's very workable.
I've attached the experiment I did with Hexapod from the Examples folder.
The first images show an airwire in the top right that looks like it should
have been routed and is not. I suspect this is to do with the DRC distance
settting keeping traces away from dimension layer objects. When I opened up
the polygon a little more as in the last image the routing occurred.
Warren
--
Web access to CadSoft support forums at www.eaglecentral.ca. Where the CadSoft EAGLE community meets.
Gary Gofstein wrote:
On 5/30/2011 10:52 AM, Dominic Hoeglinger wrote:
>> Am 04.08.2010 23:16, schrieb Harry H. Arends:
>>> Is it possible to auto route just a partial part of the board?
>>
Autorouting takes place inside the bounds of the board outline in the
dimension layer20.
If you wish to autoroute a small area, the following works:
1) Move your board outline to another user defined layer (temporarily)
2) Draw an outline around the area to be autorouted (in layer 20 Dimension)
3) Autoroute
4) Restore the board outline to the correct layer
Airwires not ending within the boundaries do not get routed.
HTH
Warren
On 5/30/2011 10:52 AM, Dominic Hoeglinger wrote:
Am 04.08.2010 23:16, schrieb Harry H. Arends:
>> Is it possible to auto route just a partial part of the board?
Just a random guess but maybe through laying a STOP polygon around the
areas you dont want to route and later removing them.
a polygon in the stop layer makes holes in the solder mask. the restrict
and keepOut layers can be used to control where traces are routed and
components are placed. but I think the question is whether individual
nets can be autorouted or left unautorouted and the answer is yes. HELP
AUTO for info.
Am 04.08.2010 23:16, schrieb Harry H. Arends:
Is it possible to auto route just a partial part of the board?
Just a random guess but maybe through laying a STOP polygon around the
areas you dont want to route and later removing them.
Harry
Seems like we cannot tell exactly what you mean.
- Olin just had his standard autoanswer on, correct in both cases anyway 
- Jorge and myself read question as some signals and not others
- Morgan might have read question correctly by pointing you into restricting
board usage
Maybe you could pinpoint which of the two interpretations you had in mind,
maybe a third one
Christen
On 8/4/2010 5:16 PM, Harry H. Arends wrote:
Is it possible to auto route just a partial part of the board?
Hi Harry,
If your not as command line inclined, you can click on the autorouter
icon. When the dialog pops up look at the bottom of the screen you'll
see a select button click it.
Now EAGLE will allow you to select the signals you want to route. Once
your done selecting click the GO button and the autorouter will route
the selected traces.
hth,
Jorge Garcia
Cadsoft Computer
Harry H. Arends wrote:
Is it possible to auto route just a partial part of the board?
Searching in help for restrict gives:
"If required, restricted areas for the Autorouter can be defined as
RECTangles, POLYGONs, or CIRCLEs on the tRestrict, bRestrict, or
vRestrict layers. Note: areas enclosed by wires drawn on the Dimension
layer are borders for the Autorouter, too. "
I do not think you can say route lower left of schematics (or any rectangle)
But you can do auto on signals like gnd vcc like this
AUTO GND VCC
Christen Fihl
Info wrote on Wed, 04 August 2010 17:16
Is it possible to auto route just a partial part of the board?
Yes.
--
Web access to CadSoft support forums at www.eaglecentral.ca. Where the CadSoft EAGLE community meets.