Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) Place text along a round route
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 188 subscribers
  • Views 547 views
  • Users 0 members are here
Related

Place text along a round route

e14 Contributor
e14 Contributor over 15 years ago

I know you can place text rotated with this command: Text SR15 '3' (28 7);

But I need to place that text along a circle width a 28mm diameter.

 

Now I could make a script for all 48 numbers, run it and place them by hand

along a circle line.

But is it possible to do the same with text, as I would do placing holes,

and if so how does the command looks like?

 

Regards

 

Harry

 

 

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    Am 24.12.2010 14:27, schrieb Harry H. Arends:

    I know you can place text rotated with this command: Text SR15 '3' (28 7);

    But I need to place that text along a circle width a 28mm diameter.

     

    Now I could make a script for all 48 numbers, run it and place them by

    hand along a circle line.

    But is it possible to do the same with text, as I would do placing

    holes, and if so how does the command looks like?

     

    Regards

     

    Harry

     

    GRID MM;

    Text SR5  '1' (P28  5);

    Text SR10 '2' (P28 10);

    Text SR15 '3' (P28 15);

    Text SR20 '4' (P28 20);

    Text SR25 '5' (P28 25);

    ...

     

     

    Please read HELP - Editor Commands - Command Syntax:

    ...

    P   Polar coordinates (relative to the mark, x = radius, y = angle in

         degrees, counterclockwise)

     

     

     

    Mit freundlichen Grüßen / Best regards

     

    Alfred Zaffran

    --

    _____________________________________________________________

    Alfred Zaffran              Support

    CadSoft Computer GmbH       Hotline:   08635-698930

    Pleidolfweg 15              FAX:       08635-698940

    84568 Pleiskirchen          eMail: <alf@cadsoft.de>

                                 Web:   <www.cadsoft.de>

    Registergericht: Amtsgericht Traunstein HRB 5573

    Geschäftsführer: Dipl.-Ing. Klaus Schmidinger, Bodo Badnowitz

    _____________________________________________________________

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    Harry H. Arends schrieb:

     

    I know you can place text rotated with this command: Text SR15 '3' (28 7);

    But I need to place that text along a circle width a 28mm diameter.

     

    Now I could make a script for all 48 numbers, run it and place them by hand

    along a circle line.

     

    If you generate a script, this could as well contain the needed

    coordinates on the circle. (I would write a small script generator in

    Delphi, if I'd need this functionality more than once.)

     

    But is it possible to do the same with text, as I would do placing holes,

    and if so how does the command looks like?

     

    If you need it only once: I think there is a ULP that places copies of

    some objects in a circle at regular angles - it was mentioned here (in

    one of the groups) not too long ago. You could use that to generate

    circular copies of one number, and then "change text" on them manually.

     

    Tilmann