Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) Clear circular space in bottom layer?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 189 subscribers
  • Views 719 views
  • Users 0 members are here
Related

Clear circular space in bottom layer?

e5frog
e5frog over 15 years ago

Great forum this, quick and good answers, been scratching my head with this

one as well.

 

I have a small project, about 10x10xm bottom layer, smaller rectangle on

the top layer.

 

Trick here is that there's supposed to be a hole near the middle, the top

layer is supposed to have copper to the edge of the hole so that's solved.

My problem is that on the bottom layer I need to have a copper free area of

1mm around the 2mm hole (1mm radius hole, 2mm radius free space)

 

I have tried bRestrict and bKeepout, didn't help, I guess these are perhaps

just to keep away components from that area?

 

I had some result using a polygon, but the copper around the hole was not

circular around the edge (not when viewing Gerber either) and polygons are

enormous in size, 1.5MB instead of 1kB file...

 

I've also thought about using "Holes" but there's no restriction you can

set to the layer. I basically just need to do the same as the bStop layer

but for the bottom layer instead.

 

 

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

     

    "Fredric" wrote

    Great forum this, quick and good answers, been scratching my head with

    this

    one as well.

     

    I have a small project, about 10x10xm bottom layer, smaller rectangle on

    the top layer.

     

    Trick here is that there's supposed to be a hole near the middle, the top

    layer is supposed to have copper to the edge of the hole so that's solved.

    My problem is that on the bottom layer I need to have a copper free area

    of

    1mm around the 2mm hole (1mm radius hole, 2mm radius free space)

     

    I have tried bRestrict and bKeepout, didn't help, I guess these are

    perhaps

    just to keep away components from that area?

     

    I had some result using a polygon, but the copper around the hole was not

    circular around the edge (not when viewing Gerber either) and polygons are

    enormous in size, 1.5MB instead of 1kB file...

     

    I've also thought about using "Holes" but there's no restriction you can

    set to the layer. I basically just need to do the same as the bStop layer

    but for the bottom layer instead.

     

     

     

    When you use polygons, set the wire size to as large as you can and still

    retain the detail you want. Try 10mil for a start. Large file sizes arise

    from using zero width.

     

    It's unclear what kind of copper you have on the bottom of your board.

    (.....> I had some result using a polygon, but the copper around the hole

    was not

    circular around the edge...)

     

    Post an image of your board.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e5frog
    e5frog over 15 years ago in reply to e14 Contributor

    I just want a solid layer, a hole near the middle, 1mm clear space around

    the hole on the bottom layer. So a 3mm empty space in the form of a circle,

    I was hoping to be able to use the rectangle for this and just clear that

    space somehow... When making the regtangle as a polygon I have tried

    various method of making the clearance in the bottom layer but the polygon

    part doesn't get completely round but jagged.

     

    I can try adding width to it though.

     

     

     

    It's the center hole that needs the bottom layer cleared around it.

     

    This is not the actual design, the measurements differ, I just wanted to

    try and sort it out at home.

     

     

    Seeing the editor of the gerber files today simply taking the rectangle and

    a filled circle, setting the circle as negative and adding them together

    makes all this a quite painful process. It's so simple but not in Eagle...

    begin 644 Image1.png

    MB5!.1PT&@H````-24A$4@```XH```J"`(```#S-#<M````*W1%6'1#<F5A

    M=&EO;B!4:6UE`&WE(#(T(&IA;B`R,#$Q(#(S.C`V.C$U("LP,3`P)=R@)P``

    M``=T24U%!]L!&!8'`](#"#,````)<$A9<P``"Q(```L2`=+=?OP````$9T%-

    M00``L8\+_&$%``!#.TE$051XVNR=#W05U9W'9]Y[^0\$R'\QDH!*-&XKK\

    M49-2-1[HLM:LT(NJ0>66VW/0>.[=;=)!Y;B^3T=%U=+`O6]L@63N-QK7_VSMSWYLV;_V]FWA2[>\,[ESW\SO

    MWOG-3.;[?O?/L,%@D`$``````"`U<"2[`@```````$2`/`4``````"D$Y"D`

    M`````$@A($\!`````$`84">=F]_\,'MW?&N2&)`?'S,\Y@7$D1]Z9(-0``

    M`(QK1/4/'A8,1O;[7T42>TKF19-%UT="D;VQ/HRZ@Z\RO[XOHLESI4Q:?Q

    M/M(4DBQBCVC5R/IE9J)F0D%<+865]HVVWVC6:YA(SP`````RHJ.G-=M.!`4V

    M5Y6M>^>==64VEA9E7\FT+24*I9S8UEF=0(5:MK26:6[MYM/=K<U,[=(E=CM0

    MZJS08=:$#SF.I6E7)#D%1T$$57ES;?@":ZNL*]?75PFK>=GLRA8WK0UW:=0P

    MX96NSIJ*LM1P(````)`B:#;NRP,JM@?I!)OE=2V1$KNWKZ]K::DKMU@2>>H3

    MA;II>S=O=OO&4#A5%&/CS8MC:2$U2U(F9*U(GW:[B3HMB[(<CQ+5_2G(<GF.

    M)-OZR8Q<)Z7'Y0>IK;;P]]&',$'%$W4J?WE.F;;%D'D56TL8T[&5PI&S=&

    MN4!T=6W:)#M!H4W"=8LXSIK'JI9MZ.SB=^MV5S[]=*6P$KE.E`J5WB`J50T?

    M@JW7DK0XT6$K>!4```"PC6AYRCS51K&VS>6NY\.125KF]>;TC1B]S#CMBL

    MJVP+AP`CVY6MVQ*"%H-@E1JY8Z]S(^)!R).O(AMI?;A6VZ6YLK-S"[N<,F

    MJJ'"1,%":>V[FRIG"P9DKK.OQ&@B_N0"Q]P)E.?P<`HMY/BV2K>94ZE(2V?%

    M%EH64T>O$`VW1WU;MN[I#4V\(SC?;7@ZYM/.A2&)T%,Z&>%:!=LV-'$N$%U=

    M*_-5_";4C=^_X5CT6-E%?2G2W<7.=%5RRKYE>CK1%:HP@TBJZJ-UYX]@RI

    M8?6[7NI5````P#8T&_?%7Y''/]-4+3RZ6DQI&K%](CPY2;'MR2H3ALP4'2E(

    M"`A5-S%<%"L4V>IV5RY[LJ*3/.%)Q:)4@V&(I2:Z_X9ED>+DKK.O1#$B?Y8M

    MK:TA-9'GT"V)IN&JQFJLW1)]J2DT,"D2N+7B%:;H_^-N0Z7IU&?&=GK;@B

    M0@7K^4U<M[*&CL\QH76B4NXIGURHHE8Y5:BKA-YH?(;1&J]EU+XMN3JF&-

    MNU[7JP```(!98IE82D.\IBRT;U]4CJB+8CADRXN%]MV=%67DF4^>\-RCWMSQ

    M\5JAO;59LK_,=?:5:(ZJS5Q-ENU.6-NLDMMEKB-JRZPZY8*(X8Z_H1)EISZY

    M'B,U;!).-"=6N[IM"9G'5JZ%N]Z````USB&Y2GW`\UR=J&2%)TMS:W2+XU

    M%Z"-@F\)E3<4AP,_0J&<6-BTJ9/YI*[=YM7#57*NNJZZT@9K;"Q1L2#N

    MT(C,D?0+;NW;3::8GD(E+1_M!75%GJ;I>Z[LEMG=75G2;CZ63O<(\"#N[4

    M,]&M_5Q@5HCYB:\N-2]%'9)UCW$_7<@YIR>Z;#;3O)Y>`.K(;Q"EJL;E6I)Y

    M1A6Q5P$````[,!X]Y<::=%9;F\$HJF\K,5&UF1M@S:VL=U=&1=3XOHC5YLJ)

    MEIXH0LX$,LA\H4%4K$0DM(S)!D4V>%^<<MU]8I$3AKK.Q16"N`ZW)'

    M\QMN6BEQ*BA9!ZA18L);,2C7'[(?K#,IBH)U-1L2XQ/S%6/D@J_$I-X

    MXP````!B$#T%```````I1"PC]P$``````(@SD*<``````""%@#P%```````I

    MA.N-75N370<```````!"8&@4```D@C=V;7UXY>/)K@4``%P#N(8&CB2[#@``

    M,%'`OUP``-`%?4\!`````$``7D``````!2",C3&#C>=1AFQWW=QAFI[.H)

    M6[>!T^<Z.O[B=.3:8RX8]%_V!,;\B?$,```D`,A3``!(*%TGNXZZ#T[-+];?

    MU,#0U7/O'3SV_5_V_/Q-(E3?60``&`/O([ONMD[Y%2_R!"\FN3)ZI0

    MVJPWVW1IFD+<E[:4O'4>GNLY17.,;ZQVA@.6XQH(#DOYCP)(.`/)4[="B6

    MPR>N(Z2+Y-X7`ONOKR%6L8G\YFP4"@[]5W,ZXOR*NY0V.;<_.?OF&9<^

    M/7[UU$#.W-(D'A<``-B%B_\=?WCYBMJA@7C)4PT5*,'@,\-&61D,!EF6E2^M

    M'".M@UV/0*)-Z^O)WXK&1D80J223+$UH5LD!:J?5ZJ_H,6&&,H-&5`YV9T-#

    M@V07XDF2=3Z51/9B&0"..+8F(Q<B2IW;D*,5="CU),VM2\PJ@:D@O?

    MH,TTQP5#_V^#S,4_'<VY=%5#GK(.Q_3[;Q]HWI]S2WEF:8'%([+"*[_=9WSC

    M)[ZU)(E5!0"D/FQ?7U]Q<3'Y'3]T+E[3G?#2C3Q<V?;V=L4-JJJJR%=D:>2?

    M.[&F-E=KK&(H5IE[O.OPK-ES=6T*QI\!&J8#6M3AFA3G@;P]!,(5]1IRJ:

    MI8%/B9J4I(4<[>BIACS5-:)VR&H>BTE,B#<6ZQC31FRIB14CBA>\P:O=R$6;

    M+#3JEF?@-ZU!A2IHT_KZD;AJ&_&4B.AK[7]9M$FU*T%6I[VYZ'5SY.[@C=

    M-JOATX.O?-QX/5H?<_*7IDR77K'CC[9L>5KC[GU.R"Y7=ES"P<?O_@Q0^/

    M,?Y`^G73"Q]>W+]SS[2J6UW3)Y]]\X.QLQ=)/2;=6I:W[*\N[/_\_/Y#Q.#4

    MQ?-R[_X*T;)VG#=E_N,W;<$%VXULR7ZT[KN/57_GB1_1U?]ZY7EYFB3B5U4`

    M0.KCTOT='X_6:CE$F\:TO23`:2)01_?B3%'M+/G.IKD)J??,N4ZN31L:(EW1

    MPIFQ(:A&ZD"Y[A$<JQL]U2Y%UXBBK_BPUIP@]Y0/BI?&PUV2S;A]F="I-&U$

    M3.*-A%S-1OF$.W.R,/^X:?$WHDT9PS%4ZFUR\S2&[QGKT5-!FPIG@)XE_@SI

    M6]9NL_)=&#WQ['\[,],SRPK90(!Q.`?>V-_WVGO3[KGE8L>1T<][BAZYN_NG

    MNW>JXS.\,ZO%=O'NO8.9Y<7G=[1=_JQ[RH*;+GYTS'MF..O&DA//[LBI

    M+"/5(HF;7_JGN#;]CXV-,;Z`..<G=QZDB1]_.%^R*?TK$:;"]S0?"A6`B8Q.

    MWU/Z<A0_4;[<HWL.^)J"`15>K#5\C4RZXDX5+N`1\NV%#QL6/:/S)M&H)E

    M&Q@J5$TA]IY:'P9A&[7HJ:[SA0TTC*CN2[47W9LN67:(,>E&8LWTOG9!5)18

    M6<;4;U`%4X+=^(B)T#>I\(\CXJ!GEIRTXA;;'+@4%M*FRLZT^A-9_>-:1Z

    M0CS58E6IRZFCA@:4XZF*:/<]]8V,L]?GOFS1R;/GTY/1ST^ZX<[TOFY]

    ME1L"8[Y+GY[P#HV0*SMK=K%KVN1)MY:[ID\BJ\$QO^?D0-'JJJ)5]W[Y\N[1

    MPSV>T<<61FSGGV4\?L//=KD[3\?5WGJ]7J=/NGL`3_LN/5G"S_S1?[O5Z:

    M$+2I!&A3`("1OJ<A_2;3<F;Z:-J"8NB4,1:JE'0PM4N;ROL)6`S/-#2$)*A$

    MB38(7YAUG3SJ)HZDBOVC&ST5VU$,QYH(:;.RL<KB"A!HA1AD25=)@RMSO#

    MMT&3^A.53)?FC`1#UZDT;05)1Q2R;&]OO_?>>VF.\7-'=9XP8(X&*07E9T8%

    M"I<`RRJD)9EZ*(ZLGA[#@VX)?]MC&M3QEC?4]81=6B>P?/O?OG8""04SDS

    MZZ:2@H<77_SPF'_D2MOWY_]D\>$C:.:[F=3KSE8./:K$_Q>CUILLFMB#8E

    M2U]T_I@W-,.`F@9%]!0`X#(PAE2J2N,9;=1".W1J\,%#5914GUD^'O%CWDJ#

    MOA@J0RWJ40ER!\K3!J.GVD:$M)GH:;3V,A$!%10AT:9"VIS'+.[.V!@]54I;

    M1+AE!&$JG"^#&D[0IL.=)6(5)@457QMX8/F(TDJ//D&QAS@SAZ2NHC'BEE

    M)7HJ]HR\K5\;[38K1YJ+&#J_[_.Q<Y?&SEX@RM*9DY51FE_X=]QPH@O[#WWY

    MB[>R9I44K;S'>V:X=^L[M,IXV`=61DC'QUOV[ZE:[3IH]+S8=JQR[@\7C9

    M:!GZ_=:7RQUDR7#^"5;RG<7=SF%-@4`Z/<]%>M1NWXS-"_8=.M@;%""U*+

    MUXJUJ>:A!,4R5&S+JV=XOW_=N-BK<TW??4B!'574(QGBIS%&3\763.]K

    M%W9%3_DV_7#?4SNBIQ1!FRHJ2"/4KX-616TJ4F$0GV!@80M"D=&B56J+8X

    M4)-C9C5;K-*YA2O.9K9]_\8/C]@X$Q7WK1M,FWWWCE6&_O?^XFI]TW<KG@

    MFXL'WM@_\O$7Y$(7W[GI*^69Y87I>?GEJR]CVQ#Q.O5P>G+@Y;7VI)M*

    M'$Z'WV]UQG[QOU:U`_1X/XQ_TLUQ^CJ4RTWT81/%E(E6SRSJ:*:0#`A,7(

    MO<1;4J>"(V-W+!Q^=)`V"!85:6VD<Z31O=9(FFVTZE'W,_\N>QZ?#,8/^J

    M_)0Z-3&`JD45YQ8BF#T5.1I0..70&!24G&.:FTQ\M8@CKZ:-B$F\D="/

    M@>C^N(Q-G4TI!B?-B`E+VI0>FK8`-7SX0JQ4&!IE5]]3QI0V9?3ZGK(.1]'J

    MJOR_71CT<R.-G)EI;$;:S2\^X;_*C2@:_K]/SN_I+/WN-Z8MG4_^A3ES,EFG

    MH[QAC2,SW3<\<OT_KV!\@3.OMSE<CBMSRXZNS;LN,YT=NN@?O4J^E11TP>/O

    MZ!U=.",[-\.I6V==3>_U>C+X/J9/_.L5Y8?]X7[F_ID'5*]7KP``"@@\/`

    MTL,:5-C_Y>#A]]:.YVH>)I:]G)/S+=<Q2<0(>=31YS%YX`D?<7Z*(&A'

    MBF):O&7\C"A"IZ649-+0%S%I4-6)C8AGE3)MQ)::6#$B=R.=]Y2/IMHC4A7K

    MJ383G!ARG3?9I%(J6N>ZBI!B=)9I<0Y-A9D<$NS>J(UEQ+.N<E.GS28?

    MHDVYC(PTNEKPT(;F^HOKF86YV23;0I^99LSH<%SK<Q__EM>/_]INK)_L

    M'UK8?879]-FE<Z.@1WM6;-*!M\X.D;$A?RY<A8X]X!LK3E`#T>CY\?N4^T

    M5F2-%VE"9))/R1-HZ<``"!H;ZG-FE31C->J2-2Y44(CT#ZF#$H4MEP8:&$

    M3=/R"V)4,3]UD,PJ)1]D)DX;B9Z:-J+F1CJP6J5<0[/VC#,C=$Y^]6D68NAK

    M(8$47D!F.1DJ;7XRY&T[XM'2IG!MKZU'&KCHFR)G@ICI&"XKOZB!)5S)^V

    M]+:'T_S\VAR8'%5M-TT+T5.R^JO:'K*JV/<4``#$

    MZ/<]M4;*D##,P8G/<TOFC/8?T282J:OH'F#PVL"F^@_YR@PC32_50T4DIQ

    MU)1!U,)%0DC5A$VE]OT&R3:QOCB*2AGQQ$\:6VKW/;5H1//`I;OP9[:!G'&#

    MDF[\&5&9H58P8C*&JJ$^C9\XQ<O;Q,MLQ<>FO"I/&""B2K=4D!O(WO>:YA56

    MZ/:2E1.G=_4Y<SR9DO;P1Q.9_&C7_M\W;^7/O%@ZUC63W]_L/A&/7Y5\^;

    M?E]Y#E=SACU_-;"AM>_Q^=,?FI-KNG2OUQ.(GO>4K@J91)O25=JX+YF*7[P4

    MYRNF;70:`"`U,=+W-/2?-SS/4=0R82.!PL%1?D4J0R-]]G45JB30)R0'K<W#

    MGX#H*5&B3ZUGJ&!E3+W1E%&9\502G(NU[ZDY(S$1/K,Q2#KYC)@FC%BLB=J8

    M?5MJ$G:X8,2ZFZ48/W>VG.60J7ZW\:E/C4R#(&C38'V0;60%A6I+]-0<!MJL

    M;(-<)VGY4URY.6G7Y>_I&5TT(_M?EQ2]X;[X/T<O++H^.Q`,]E[TMIV\=-7/

    MW%Z2;:4@K]?K]T?)4[IEJ^O[ENSHR2<3>1I'HJ%IUBQ.^.$H_BAS`%8.*@

    M,^^I[E/3R(0CUM&-=AB-B&@\PZW5/![14R8<0*4)(8=AS#]3)8%/`7&.[KN(

    M;#$2NRMBUX5%K#F%*I&5IL6EQIC]F`Y'(S@J'C5GUXQF2<>@0C4X15?(U0T,

    MITU%.4ETE)%Y3TB\EXKHA0#P?PLY[1,9V&.D]ZLE[R!'_Q?W#4_YW;ILV<

    M8KYEG'?&A4(1/U/H*OBI;"EN2+POE,`)@Y&IYJ863"$7X;Y>>KJ%E?)_BC

    M&QDU^RQJ[.I!6!4-;#,X(PM04CG13%#E%TJ2U&3DB).GHZ!:-8EPD6M3

    MXT8DLE)#7&K71'O&4X-&8OJ).`ZT*457H1J?/C8RH4<#MSJX_IKO>VH0!\N.

    M^8.#H[YI7%=5A7LVR`1STAT-=Q<=&_\W36RYI:QTLGF%:IQT6E:GD8`C!Q

    M,#+OJ0Y&0A&V/#5M,6)79U-%4FT@E!R#C;#:Y]06(^8P;G-(4_!9KY@1([HS

    MGMI8$V8<:5.AD-Z=4&\7AKE,1K+O$J>IA%E3TTISTW[P_ID7;L_)R$QG

    M':SR;I8?J0_RZ0[20:;[7,FIJ<$;V.\='/NH;+9ULONIS^<[\KO;A-4[

    M?B==BK>E?\0-])6?HV7G3(0J0!,#-C/#WZ0@-_QXX/C78=GS9X[P<V.[J-

    M,U9U1.M;NUM>QY>^3CY=3<6R"TNB8B36MN3L8N.SK&O;.G>I/W$Z_8:"

    M[D!:FH.9F9L^=,5W>F2,)X8]E;D96:GL=9'[@,`@(VX$O,['@```"5A?4\

    M<USDPZ5N2.+&\/Y>5DN\B&)VXNS:,Z\@LQD>P4``"X%BZ\DWQL''@+``!`

    M@\3T/04`@&L7AW43$X<X-41>6V;'?=W&&:GLZ@E;-P/OZ@,`@`F-*]D5``"`

    MB07:K```0!NV>><ODUT'````````0IA\6S<```````#QP(4&)@``````D#J@

    M[VD2.#$8/CHF5/],0_:S<_-OF-.\;P9&1.S;@````"8"(PW>=KRR63784H

    M:F[[EB3G4^G=]!S_UVWE)?DQVIM8'BD]2/N%35Q4H&I7#<`````3!#BT^3

    M\E:8U?<W)+A$-7:\VR#WP\='SJQ^8&'AM,DF#)*]EBZHV/&'CGDS9MI5R52N

    M&P`````F(.,M>DJ)4X?:O,(Y[TAP\W:[Y9U?7;SDK@<4OQJ\,&I._U'(

    MOL1"/(XNQ>L&````@`F"2_O])?E%%8/];H.)B0#1IG??<[?N9GO_N%=-GB:%

    M9)TC4JX\LZ&A09SU/I5R?`*`````%(1%__^DL/5]0JO@-:T#1&$A.'LT-]

    M&M\6Y)786QS+)F?^K\;&1DF.7%D2M.LFV86L2L3H2UMV)O[0`````)"RN!;<

    M]?7E]8POF171)>>YI4;F::=M:7)K@AA<'A0XUO;Y:D5A/@E3<3Z6Z^OEZ\

    MVL`CR4GV(0(```!@7.%(<UP8&C@R=$ZYLZ9$W&@G8J'W]545:N:>)^@`<:

    M5E84K:PH6?F"?H]1PSA=K,;'QMJS/.)$K!`]2B6ID```````2&4<`Z?/=73\

    MQ>G(5?PZ7HW[/1UO,VN?9%KVQ%F?[M_Z&/-#=_\N]X''CM9N/6"O\6_7_$`W

    MQR)!'G$"`````&!\X#[GAZ<FE<R%)[]K8P?[/Z_KG[WM[;RZ\WKUS5_'IC

    M17X1]ZG_@`EE%H5RHNLD?RZUWN$G'`ZB@/OM:Z];SZ7KVCYIZ3IVP1PV?/

    MGPGZ?52)DB5)TX^00S9(F"?%,6SZ8:+CV>;:]`$`````DH5.W]/XC-SOW?-[

    MYAN;9RPN6[OBQ8Z>;_/=2=N>.?8]]V`]PWSP0OZS76;MBVX)F*-]V[%H5Z

    MG88Y4+_@/?ZW;L8FM]\K\'>J,4WS/VB_131J79X;<SG_5;S__]BA^1].IE

    M&U][Z_E_X-,$DBXJNM[>DZ0;-Q6?"WN+MHZ\<RK&0@$```!``Q??]U3U#99Q

    M:=SG6O9KFHA.+*UZ\J&M>WIJUY#,ZN?J%O'?ELY:RFUSREW]7-,B^;ZGW,RK

    MQ>]&EY?RRG.TMI=_;4)<]GE2U=H)U!!H0K:E.2P_`8Q&10/S=KD+Y=.M7@

    MX'T-,'(?`````#&A,]I/.C9V]+:MF]T3-T=>G>WC7RB41[CK<RLY3WKW[N

    MH(GQV=.';YQUCJ[CT50J#1MP@+5HQ95Z?W=^\QDE7WG<"KFAX@.`:3::89

    MT-B!`:99-IOXP=C8CA_"MH@]4:P8[8QLUK(1311UDEK&4M42@D1XIP_O'N

    M[(YB.5Z'C:TA2Q(YC`D,PTSOK3[5MV_7

    MX]:M5]]#U>>C4OG>6[=.GQK[CZ]_YW&3_X>0S:/A-'T?Y`=:N0\`;+`N<T]'

    ML'\3O^YCN]=<82'YTE]?<V_N:O-E-"WONNW;FNW<&K;:=N_W/W;G

    M8L>YISO?>^GG;[UGY98?W/*MU[UV%)M2A53:7S8=7+:&;8(I`#`&NLP]'?[@

    M?GUD/S-J_]:5\?TGVNY;^=U?WW[S)OF_F,X>_>GUJY__U.[WS0WLWH]OYZ

    MMJMNN'7WW&P2PRM7WG3CSA'](PXWFX8-I$(Q-=U,RK)]`&!"=)E[.GS;+K]Q

    MW53#G=<MUE/C%0=:;GCK)Y86/U$_N//ZF5M?NVW;SL;UUIFF>7-/=]9N7*@-

    MT<</?:O26Q,`F-X3ZV>;B[83KJG:24SZS0-IMG37@UE9!\`8.-UF7O:=<%

    MT\C$//0=Z;^[7_'@ZO_,KBJ`J???CI\X=>>NE(M?KR\O)T>$\_"J?)#<5;

    MRRZ&KQOV7__2+IE?L`0$F5:>WKOKURYO6T/M.J:?3:C#S4-ONW9EGZGX

    MO'BDOC`_I-)L-DU/PPU]RP[NMYYNL`%7[D<2D0&`5Y`N<T^+F*AQY!WG7W3?

    M`_]4J9S<];8BK65#9]NA_'*GG#8MVV][!0!@N(8S]S2V;+IYRXX1M?S=]^

    M_[L':N'44TY\]OD73GO5S_3W]>2[20LCG4Q]PT`F!#3@S<1FR]HU9V%_*\

    M8<?6K]_YP[?\VW/.V3K3ZW<//GWXF]]?2%J8PX!`!.B&EOA<Q\:.GX#^Y_

    MZM'%GHO6,Z>=\L8=9UYT]DF3V3<`8!(IP``1&3Z]MON+L/``#0,-"CWH?H

    M+V_\;-E=&'\?VGU5\7_GY.;(9_$"`&-IM#!\KNPYKOWO6]LKLPMFJU/P@'

    M1?Z1TYL_\KY:V1T'`"9+="OWK_G/5Y?=A?'7TS]R5/\'!@`8>U-E=X!7C-G=

    M<X,W`@"0KQ%/#S[QD[ONL<3ID[;X&,``,AJQ-.''GGH_H5[7C-SY@8?Q?Q

    M/[]F;NMG[RZ[&QW<<_W6W1__\Z?*[@8`P,@TYIZ^Z<WOV?5K5U1>WNCC7'?7

    M=G]T?SU!7WG3C9]X6X=/*_4;WO[ISWSNBF'$W<>=NU_>MT-3UZU<VO7//H

    M;_SAY=N:_NEX9[6\7[W_)SUOY0WL]
    I/7;_VO-[VSS9T``..@$4\W33U[

    MZ."S&W<X[N?_6CEDPN+KT\BX\=W?O;NEO"7N/*ONL>GMS]IS=4/OV9QA]*

    M_NZ;;OC.U'F?^HUP?L_MH3\K%=9K__RIG5<\V7(E$Y$]_2_@_E_\PS/_+I

    MFR[]TWLNK[UF+\<`"`2\2Z-NO6;5[YW)8%M>-E[WCDTHC]2L'G:]GW7/[GYQWV3M7(:V#WQN\3.?>D?ZZ>L_L9H('W_P

    MP0O..;/=E35W%]_\Q_JXNQWOO7M]S[Q(;_%P(`L!'BC:=KSGSMA0\^_&B;

    M#S[_Z[OK*7/WU]9GM0?O/^^W%Q8_>>6?_-&UE7!PTTV/Y5Q?]=@3][_CK9?D

    M#IJOS$S=??M[U\J9K5>][@YIY[:P+OO6X>`H`C=70CQM;V?MQH7%^NN&

    M"V^X=MUJH5`!W7KN.]#_.L]./N/UQX\L9WW;JV/JGU2G>/?>WCLVV#=<&?

    MF?2\>#D9`.`5);IM=MXZM%[SSOW-SI?/9YYVUPAW:^]]*/WOIDI7)FSI6\

    M_M='\S_0ZQ_-_,PG'_[6Z]YE:10`,);BK9Z^]]+/W[HR-_2Q']SRK=>]MI[&

    MGKII][KOQLON?ZQLS1I[Z:O.\SS[5!\WOOM35?QKUV_6A]^]9OOOV\

    MK6VN9'JXLTW_"KV,N3$,X>T/2P``V&CQ5D_?=M4-M^Z>FVULS-2R['WK

    MN??^3OW3Q-Y/+@QG_?[KW_6;?_39.YZZ/"S`#POJDX,W[?[]Y$_4SJK\WN_,

    M_=[J7ZS?TWHE,[[?I?\9S7]H:_[/?/R..[]SX>7B*0`PGJI+BPME]Z'N]MON

    M2-Z_>]?W>GH<_-#5-X%Z_J<3:#=\_U6V\Z]SW==.(II[YFVU_>-DB

    M_\CAYB]H_:1]]4.';PO7)S=/;=X8Q3_:P$`QEC[P?U]P_,S,XEK^2@OW;W

    M[9_+OLKF45M\!UGW[DHU$_->J/[O_T;]N3'P`86^T']VNU6GHPOW=/KXV&

    M/'KMM<OA]KKJN'*_-[X:V_UE?A7E-V)CE[_B2=O.V/*YT"`!M@^'-/DR2:

    M!M,@G(:0DI(J```E*9C]3044-,R:A%-1=/JZO5PGESOFE!KM3\HQ]D_/7Z

    MC[QYRXZRNPP`3)"A+8UJGTVKU<IR_4I:34T2:J7=*/_MM]WQH=U7E?VOP3I?

    M_$:M["X``!.G3?5T9K9Y)5.?$;9:;;POKXWUIP/]1OGC]Y'WU<KN`@`P<=K$

    MTR2,9A-JP6P:XF:2.]<FGB:I='TVK72NG@(`0&7H3XU*<F<(H(U,6FQD'P``

    M@I$\-2K44)?77ZD(I@``=#/\>)IDT'W[YT(>S5XL^Y<"`/`,)+JJ3``$!_

    MACSW%```!M$FGC9M+-6ZSQ0``(Q(XVERNX5```3RN````1$4\!`(C(2%;N

    MPR!V[?I2V5T`@!C=?/.'R^["1E`]!0`@(N(I```1$4\!`(C(R.>>IMNFAOVJ

    MFDX!`""K$4]G9@T_7AI<4_!AG)R9W(EN[=_TRD``2&-K@?4JF:```@@R

    MN]OM<PY/T#N#72Y+UI?!\``)H,;>YI4P9-I9&T5JM5E%<!`,A5='!_9O]<

    M>'6ZH>W@?K90.KWZ#16```FU@9M*5H"@!`$4.IG@?GJ:7C'9%`"`@D:U

    M<C\Y2*\HG0(`4%!C:52ZODE4X``,HSJL']0-T4`(">-&\LE>YOFK-(OZWP

    M+"AY%`"`08QDY7YV@52G`P``:-5Q6_ZEO>UW,)VIU0]:JZ2M*_=S#A19`0!H

    MJVCU-!LHVX;IG7Z^0=E_VH``"5P!UW"9W56JZP$``+3J;>ZI<`D`P$AM

    MT$--`0"@"/$4`("(B<``$1$/`4`("+B0``$9E^*%[RW!N=LO+/L?`0"`

    M6$Q+AP``Q,/@/@``$9F^Z<XG'EU\MM>OS9QVRAMWG'G1V2>5W7\``,;*]/O>

    M_`OG;)WI]6L'GS[\S>_7GR`EH0(`,$13?633Q);37WWIF9<-]39?<?`("Q

    MTO_<TR2A+CW[KV7W'P"`L9(73ZO5:MG=`P!@LDQWB!DT1]>7FY>',SLW/A

    M8&EQH?A'```0M(GV;II\82:!-`T>F:/\S\"`(!4W@:\FBOI5,``!C0].!-

    MI)86%SJ-X.=\!```J75H_70A59*16B9]L`FO,1```$:]73(NDS?[@_K8^&

    M@Z:YIYT^`@"`5".>IMFT*:2V9M:<A!I"9]N53SD?`0!`JA%/D\09DF@V>C8E

    MT=8;``!@N-;FGA;)G5WO"6/WZ5!^P8\``"!8MS0J/WT6K)OF#-\;V0<`(-_4

    MX$VDTJFEV6VDNGX$``"ID^-,M\4`("-UYZFLVCQ;-I=NR=5O3A\!`$"J

    MX!27JI@``;2\N:?YV?39YU\X]903RX_``!C9>I'3R[U\;6#3Q_^IT_

    M?,..K67W'P"`L3]C;_[QT<7G^WU:S.GG?&'6=>=/9)9?<?`("Q,GWY6\^J

    M5,XJNQL``%`WS'U/`0!@0.(I```1&6T\G9F=\XPH``"*ZQA/!XR5^_8?$$P!

    M`.A5QW@ZX+.=YO?N"2W4:C4U5```"IKN]$$2*`=_^FC20MK.4!H$`&"\->)I

    M4W4SR9%IIFRZ7J31]%MI.Y7U414``-I:JYXV!<<0);,7!Q^@EU`!`,@WJKFG

    M``#0A[5XVK2`J>EX6&N;0@&U[%\-`$"D.@[N9T_;SD,%`("A&]K*_7W[#W2]

    M.+]W3]F_%P"`J)4P]]2L5@``.EFKGF;'[M,E]@;T`0#82-51U#*S^YX6_,KM

    MM]WQH=U7E?VO011V[?I2V5T`@!C=?/.'R^["1N@XN]N"@#`QK/O0``$5$]

    M!0`@(ATWEAJD>JKR"@!`?Z8&;P(``(9%/`4`("+B0``$1%/`0"(B'@`$!$

    MQ%,``"2B*<SLW/I1J=%C@$`8!36JJ?I9J7)0:?C7EO?M_]`"5R+0``132V

    MY2\8/7M*J-E(NKR\G+P?.GA?V;\7`("HC7;N::U6J\BF```4MC;WM,C=Q<?H

    M]T_D#U-LVG2PN8M.\KU0``1&I4U=/:BJ:+9J`"`)!OA'-/@R2D5JO5LG\F

    M``"O#-.C:'1F=BY;.DV/VY94`0`@U8BG2:`L4ADM<EM3-@W2*]=>>VW9/QD`

    M@'@-N7K:FDW#:?*>!E-+`$`Z&28<T_;9M.PJU0@F`(`D&8U=,07M,MI=)L

    MI4"`%#0\/<]G=^[IR;`@#0E[5]3]/HF1QT.B[8J&P`$!_VLP]+7<+[E3

    M,`4`H`^C>FH4``#T03P%`"`BXBD``!$13P$`B(AX"@!`1,13```B(IX"`!"1

    M0O$T;,Y??%O^XG<"`$!6]WB:9LWEY>7-6W84N;]6JTFH``#T83K_XVPVK11[

    M2.G2XD:4(L_:`H``"KY\;2/;!I(J```]=C/.T[FP82*@``?6@?3P?,ID%(

    MJ.$]G);]8P$`B-VZ>-JZGJE:K;9IWC03!-J:%Q"!0`@W]K*_20+J^HK!9-

    MV\KY*%]:1@4`@$X:\31DT\KZ<?SE=GK]`TDJW;QECV64`$`R%N<#_)IFE.

    MS5X<\&\<.EA/J,E[9?UP/P``-&E43Y.\6*U6TVR:'(<KR7&1K?B["@FU8@8J

    M``"YUN:>)JDQFTV'V="-DW>95,``'*L>ZCIH8/WC2Z;`@!`5WG;\O>]2#0

    M2@$`Z%5S/$T7UZ?9M(^E43G!-'P4EDD!`$"3-M73,+@_R()]Z1,`@/Y,#=X$

    M```,BW@*`$!$Q%,``"(BG@(`$!'Q%`"`B(BG``!$I&Q5K7::?]I+K>````

    M@UNW[VFU6JVTRZ!]9--]LXV=>>'_8A4``#&6".>I@+JJR$U&P2[;MN&H)I

    MRE"I`X_WM_7'878'P\</'597<!1FM>MJ:4/%U-.0J$"`-#5NL']

    M\#C3$%)#-NU5.J8/``!]:-R?RE3YNQU3']^<2&\6J]K@``=#7=>FDFDR.;

    MYJ$.R'HI``#R-<?3-)N&5)J<#IA0DQ;2<JQ4"@!`OG7QM"F;5E;72Q5/J&U'

    M\),6:K(I```%K,T];<VFP5(OL;+3W--:V;\3`(!7A$(/-4T2:K5:W;QEQR!_

    M:<;2```NFG>][16J[0=Q$\^[77Z:>M`?W8>@``M&JS[VDG2;@LOD8J'=^O

    MK8;4$'S-511%0"`)H4&]X,"JCI%T,VS>91V10`@%8]Q-/^I#$TFU!E4P``

    MVAIY/,V230$`R+>A\10``/*)IP``1$0\!0`@(N(I```1$4\!`(B(>`H`0$2F

    MN]Z1/IMT?N`-H6;VUYM:VFMC*0``VBM4/4V":?+:EWD>:1]"-LT>``!`D[7J

    M:?:AHVV3:$BH^354]5$```;1J)[.K.31F<PX?OK*WCU(#37-K,(K``"=U.-I

    M6C=-WF>ZI<^<ZFG]N[5\FK;2/ZG``!0"?%T9,XEP9;_Y1\O:F%;!AM_10`

    M`)&N%4$DR;Y@P``$"^$<;3M%:J8@H`0$'=]SWM26NA5#8%`"XQMH]'R0

    M@?AZ$JW5%S]UBJ3I<#\``356!J53AM6NSL?V.I;N$5```:@_LAH>9ORQ^N

    MYV_+G[.G:?:I4;8^!0"@K;6YI]FB9C:#IE&U:S;MKM;XSYG:7,6T5```6A1:

    M&A42ZH#9=&GOPDQE+DVHLBD``VZQ]-!Z89]3']O85FN`(`,)E&N.]I)[(I

    M``"=E!!/`0"@$_$4`("(B<``$1$/`4`("+B0``$1%/`0"(2)M]3V_^W_\G

    M/=[UV\INX<``$R0YNII-INVG@(`P$BMJYZ&,/JQCWTLO?%+WPAN:B&"@#`

    MQF@_]W1I<2&\PNG,[%S9_00`8")8&@4`0$36!O?3::9A0#][4W*E['X"`#`1

    MVE=//[8B>\7X/@``&Z!-/$V#:5-"!0"`46L33].A?&/Z``!L,$NC``"(B'@*

    M`$!$IMM>-:P/`$`I5$\!`(C(6O5TUZ^\Q>Y1``"4:]W@?OH44P``*(7!?0``

    M(B>`@`0$?$4`("(B<``$1$/`4`("+B*0``$1%/`0"(2/-#3;,[\X=M4,.5

    MGK9$W;?_0'H\OW=/>B4<`P!`)VVJITD23<-HDDW#::\/E$J2:!I&DVP:3K.Q

    M%0``6DVW7FHMH/:AM8```!=M:>5M8'TU!#[:G=$$FSP3344,OO0``1W]

    MTJAT-#]Y3P]Z;3H=S4_>TX.R?R\``%%K'MQ/JZ2M-=3BTBII:PT5``!R-,?3

    M?1VJI/,]K=P?1B,``$R@1CS-!LK6$)E\FMZ0$S&'T@@``).L$4_3O)@-D5E%

    M`N50&@$`8)(U#^X/)4&H0``]=YY7ZZN#Y=;E_I?<5]NLP_7?A?Z6OM/P``

    MDZ;]QE)#><Y3WT^<`@!@8DT5OW7P74M#,35]E?W;`0"(3M%X.O1G/O7]N%0`

    M`,98^W@:AO6SD;2/@?XPK)]](&KK`0``9%4C28JWWW;'AW9?578OB,*N75\J

    MNPN,ROG?^.RNP#CXX&+KRZ["VRTFV_<-E=V`@]S#T%`(!1$T\!`(B(>`H`

    M0$3$4P``(B*>`@`0$?$4`("(=(RGX:E.V7<``!BUZ9S/^LBF.5OWUVJU]#B2

    MS58!`(A-QW@ZQ`29#:8``)!C9YVK9(6#ZSIHU#3-I5`0`H8MW<TR1$)J]:

    MK=;TWD>X3()IR;]?1T`@,G4?FE4F$:,Y&T(,$4`(">K`WN)U%R9G8N>4^'

    MYON6UDW_G4``S"MF>-I5.>ZVA6@@%`$#?UN)I)UF/QMD<%_I%`"`/K39

    M6"H,[J=#_#V-]8?2J6P`$!_UL533X<"`!<ZY9&E=T9```FW52G#YJ>:*JP

    M"@#`!ICJ>H=@"@#`AIGN]$$8ZT]'_`L._9LA``#`(+I73P$`8,.(IP``1$0\

    M!0`@(N(I```1$4\!`(B(>`H`0$3$4P``(C)=Y*;LSOP#[FR:-&5O5```.ND8

    M3T?QLCT0:D2@``;:V+IYTB::U6"P?S>_?T_9?2QF53```ZZ?)0T\2^_0?"

    M@6P`,"HM8FGV00IFP(`L)'R5N[I@``;"U>!IRY'#']%.R0``1;2?>SK$

    MNJE@"@!`<6T&]X<[II]S!0``FC3'4_--`0`H46-P/P3*$>UOFEXQW`\`0+XV

    M<T'7C<-QQX6!0!`5\V#\;T`0`HT;IX.M(]I&16``"Z:@SN#R4["J````QH

    M:O`F``!@6,13```B(IX"`!`1\10`@(B(IP``1$0\!0`@(HUX.K-_+GD-V-90

    M&@$`8)5XVF:*>OY<G9'X]5CUES?R('ZP>P!:14@<C>?>"C[2J^_ZOUOKMK

    MP(0:R>#TN*>))LF[Y5,;`4@-DD>W?72YN2USWO#P<AH<JF0(GJ\71I;^-I

    M3\G!TN)]X;5<JR2OXM)&PI="-JW5UJX#$)6032LK8?3YK_]=N)A<^=JKGTM/

    M`39>HWI:#Z8#Y\BTD7VK%=/YQ85]LZJG$+4GUBN[.VR0D$U??/'%;#:MK$35

    M#QP-3O*#[#!ACX/Y])J$DV31)JV;\1Z"C)HV>M2DZ3=PEU$J1UT\V__LY#

    M?W5'>CV-JKO?\_Z_^/:M97<3F%`CF7N:)E354XA9R*;I:<BF$NKD"&'TY)-/

    M?O'%%RN9;-I43P788-,C:C=)J$D\#0FU[-\(M-&438-L0FW]E+%1/6G3J1^^

    M[-C!I\,2J%=5L>/'Y=-@4B,IY6L@G5ZBB(3$X&E5`GP?*1H\]]X9:FBS]S

    MV<534U.R*5"ZCH/[AQ87KJNM7J4ZW-F@CP&AT&L<WOC9DFQZ_/CQLGL!

    MD#OW='[],OP^U$?V:Y4!&P%&)R>AEMTU1BC=WS05QO1?N.5[/W/9Q965M5/_

    M_I??6W8W@0G596G4@`DUK-P?/.8"HZ-6.IFR"34[WS1)J%][]7-A73]`*;JO

    MW$_#9:^/.:UD]CT=I!%@U"34R102:M-:J.3!PZ?ZJE10(D;2R5A,O:ZG%/

    MX7)F9>7S.R!2OT)4K7&@&&KC6/-EVQ+FI")`GUQK_]>A))TU>HFUH@!91H

    MA"OW@R2)+JTDU7%/3/[:V7_7J"A=6V^-?N3J=,XOH0E*7HMOSI(T][>O9I

    MIC3))OVW0@P(IUJJ+(I`"7JH7HZE$PIF$)4VB;4LCL%P$0;>`^$#EY%("H

    M%!W<!P"`#2">`@`0$?$4`("(B*<``$1DN&'[BVW!=NO[#L?P0``&(Q+1T"

    M`!`/@_L``$1$/`4`("+B0``$1%/`0"(B'@`$!$>HBG,[-SR:OL#@,`,,ZF

    M"]Y7/)CFW[FTN%#V3P8`(%Z%JJ=IXBP>+I,[TYNSQP``D*-[/.TOFQ:\"```

    M65WBZ;"R::^-```PF?+B:1_9%```!M$QGLJF``!LO/;Q5#8%``4;>I;`H`

    M0%F:XZEL"@!`B=;%4]D4`(!RK<53V10`@-(UXNDHLFG:9O$'H@(`,.&FLR?#

    MK9NJP@(`T*M&/!4E`0"(P=3@30``P+"(IP``1$0\!0`@(N(I```1$4\!`(B(

    M>`H`0$3$4P``(C==YO_X'DO5:KI5?"\?S>/<4;'4HC``!,H'7Q-(F5V4P9

    MI%<*ALNA-`(`P&1:&]Q/8V7ROK2XD[2BZ$FFF\HC0``,$:\32-E4F4;"IP

    M)J?AD:==P50&@$`8)(UXFD8>V\=E$MEC_SVAI*(P``3)T<]6R9T8NOI1

    M;>UH30"`,#DFAZ\B508O@<`@Q0`@(B(IP``1&3=W-.<-?6K']4&^6-#

    M:00`@#$VS)7[75FY#P!`OD8\G=[)V3'F=FYIAIJ<II<K*R$R[Z?3241@``

    M&'MK_=#:JRM:KIOP%B9/C5-@4`(,>ZC:72[)B-I^%XP%@YE$8``!A[S?N>

    MA@0Y]!PIF`(`4(2-I0``B(AX"@!`1,13```B(IX"`!`1\10`@(B(IP``1&1Z

    M\"9RA"=%-5E:7"C[5P,`$*F15T]#&,V^`P!`)XWJ:=LR9UN]1LRDY>0KZ7O9

    MOQ<`@*BMJYZV5CH'J7V&,)K-IJJG``#D6XNG33FR[7OQ=MMF4]53``#RK<73
    MKMFT>.VS4S95/04`(-_:ROW!JZ?9&P:OOP(`,(&&7#U-9ZD.6'\%`&`R#7GN
    MZ1!GKP(`,(&&7ST=RNQ5```FD^HI```143T%`"`BJJ<``$1D7?6TZWM7JJ<`
    M``RBL>_IL(*CZBD``(.8&KR))@/67P$`F&33@S>1,G8/`,"`AE\]!0"`OHFG
    M``!$1#P%`"`BXBD``!$13P$`B,@PX^G,_KGD5?8O`@#@%6QH\30-IA(J``!]
    M:[/O:6N^7-IK0U,``#9"<_6T;>VS2$$TC;"ULG\2``"O7.OB:4X,+9A00TC=

    M9WP?`("K,73K@&TX*32>0D5`(!];8T:M_^`T5NDU`!`.A/QWA:J]0&61$E

    MH0(`T(>.\71^[YX!FY90`0#H5<=X.I0]]B54``!Z,O*'FDJH```4MQ9/N\XT

    MK?6[I:F$"@!`0>NJISD)-633OB>DI@EU*',&```85\V#^VT3ZH#9-$@2:FWU

    M6$(%`"MZ=9+24)MW=]T\(7\``#0U73;JR,HTGP#7730794!0!@C$T/WD1/

    M!%,``'*,?&,I```H3CP%`"`BXBD``!$13P$`B(AX"@!`1,13```BTC&>MN[,

    M#P``HS;,?4]G9N>6%A>RI\E[N!*.4]G;```@U;YZFJ3)6JW6E"F[2D)G^I40

    M5=,KX3A[````K9KCZ;[]!T*R3.)I")<]C?(W)=1>`RX``!.N.9Z&5)J>AIQ:

    MOGL^Y"*0``O5H73YLFCP;9@FBME\'`(#B&DNCTA'\[%!Z_'\WCTY;365

    M77,N`@!`6XWJ:9(O:MU)D+?(.``!MK1O<;SN.7WS(?GYQ(4F?

    M7=_+_LD``,2KS=*H;$(-.TP5;"NMC(8,VOI>43T%`"!7\[;\81`_)-2F5?P`

    M`#!J[;?E3_<];M[``!,EJG!FP``@&'I&$^[KM-O\Y7U$TS;MBW-`H`@!S#

    MK)X66;9O:10``#F&&4\[+=AONX0?``!:F7L*`$!$Q%,``"(BG@(`$)'IP9L`

    M.B!BZ\NNPL`Q$[U%`"`B$P__-"]Y?;@W.T7EOV/``!`+:E0P``XF%P'P"`

    MB(BG``!$1#P%`"`BXBD``!%IQ-.9_7/)__6(O<TV3P[EW,``!-ZO$T#9TY

    MZ;/(/4V2,'IH<:'3*0``M!KFX'Y3>34)H]ER:=,I``"TJL?3I;V-HF:M\WWI

    M1G-3;+EU9G9'<EKWS<=<GIRG'VM++Z#@``3:;#?Z2A<]_^N?F6`!HNS@_C

    M[RTMWI=DT2][!\.`$",IIO.DQC:E%#;!M962<`-!=1ZTMU;3Y;9U<:7$VB

    MX?302D(M^U<#`!"IZ=9(:'65HYK*Z<%VUHJ?"<``35?FE4K>6@B#YVG@(`

    M@*SIP9L(UNT\55NNK$;;VNHJJ/34]%,``#H99O6T"-D4`(`<;:JG3>OT+8T"

    M`&##-%=/6\-H6"E5ITDF%H=!0#`(!K5TU#XK'58IY]=R]]W`VN?'^I[!\,

    M`$#,ZM73=%53K?-]Z4>=UN:GCX-7]=5FM/C<HNG`(`@`ZF!F\BL.8)`(#!

    MU>-I.EZ?,W!?Z)Z5;)J\A]>UE<JUZ6F!KP,`0&/N:9'4V&NR/+2X,,C7`0"8

    M0$,;W`<`@,&)IP``1$0\!0`@(N(I```1$4\!`(B(>`H`0$3$4P``(C+=>FEF

    M]L#ZYYO6EA;W]-KN4!H!`&#2K*N>[MM_8&9VLF12XLF=>>Y&+R4<$6A]((

    M``"3J;J4>;;32JQLG.Z;G0L'\RM7LA_ER[DSYZ/;;[OC0[NO*OM?@RCLVO6E

    MLKL``#&Z>8/E]V%C;`VN#\S>Z`I.X9@FN3494*Z,H-70;HDWMJF6C;I-;X

    M*T;Y`0!H+SNX7YO9/Y>\DG"9S9=)-ET]K15HL.L]11H!`&!"U:NG220-)TM[

    M5ZJG>MO31703@71UAOF<<`U%:S[WRQJ0(``$R4>O4T2:6-8-I98P;J2GFU

    MTPUM$V?K5SK="0``ZZJGX:!6ZWAW3HI-JZ?9.FO:5-)RUP0,``#U>!J"XTSM

    MP->E45ZP?WP]*HE<-:3D/AGEKS=J>M\C\%`&"BK:W<#UN39A?O9R>)%MQ8

    M:J616GKG_&I%MI&`"].!0#`9%KWU*A:K98FR/GUZ%F/\K7=&<ZIM]3(P``

    M39J:UAL^SS2)%8N+U>JU4KAS?E[:\2V_1LRP\`;4W<MORIE6WS][1<7*A6

    M0[@L.LH_>",``$R:J>WKH3+HM73D38"`,"XZB&>5BK#B96R0``G?063P$`

    M83$4P``(B>`@`0$?$4`("(B*<``$1DW;ZGQX\?^^='_N<33][R+TOW'CUZ

    MY(033MBRY<S9V0M?MVJDT[\=V5W%0"`\;<63Y>6?G#/WUS>>:,7WK]+\W.

    MOOODDX\=/7IH:>G'#SYXWS=ON^+G?_X7YB[X;U/5UY3=80``QEDCGB;9]/OW

    M7/V>]_R'V=G-E<ISE<KASWWN^
    \<_CJJV>W;CWK+6\YY:Z[%KYSYV67[/S*
    MIDVS9?<9`("Q59][>OSXL7OIIL-OWRE_+%[_XP)_]V8^_.6_3:YLVO33

    M=[QC:LN69^[YARO*WW%%96'CVJ:=>3`Y6

    MM:O7W))Y:<__?&AI_]7V7T&`&!LU>/I4T_][0477)1FTY5796GIZ-2RROW

    MA.N5J:G*[B\@_Z3-E]QD`@%5CZ?_LG3O[.SIF6SZW#O?V?AXY>!P>OJ2QG[]ZTJ7+LV')_

    M?PD``JJ5T\W;=KTXHL',]GTN0]^\.RYN<J99RY_\(/K[CYZM'""65W&0"`

    M\56OGF[9LO4G/WG\K+-.RH[O?0CQYYYIOGN'_X<L89)Y;=9P``QE8]GLYN

    M3<//OC#L\XZ.SN__&/M[G['_ZA<N'<Q67W&0"`L54?W'_MMM]\]-&E(T>>

    MSLX]/>><^BOKD4<J+[U4G3WC=\ON,P``8ZL>3T_<=.'V<]]PYYT_3K-IJ\.'

    M]_^=F7GQ9<>/WY1V7T&`&!L387_.'_[_F>?.?G;WSY\[%CC@Q_]J/X'GFD

    M\I6O5"ZYY,)7O^KZLCL,`,`X:\33:O6D2]Y\RPLO_/Q?_$5U8:%RY$C]XM&C

    M]83ZU:]6[KZ[LMO?\_IIWYQ>?F4LCL,`,`XFUX[FC[UC;]TRT>_NH/_]\?

    M?M;!X\=6S[AA,J6,S;-S>V</>-WCQ_:-F&IP``C-ATT_G/G?ZK[WC;KS9=

    M/'Z\[&X"`#`9ILKN````K!%/`0"(B'@*`$!$Q%,``"(BG@(`$!'Q%`"`B(BG

    M``!$1#P%`"`BXBD``!$13P$`B(AX"@!`1,13```B(IX"`!`1\10`@(B(IP``

    M1$0\!0`@(N(I```1$4\!`(B(>`H`0$3$4P``(B>`@`0$?$4`("(B<``$1$

    M/`4`("+B0``$1%/`0"(B'@`$!$Q%,``"(BG@(`$!'Q%`"`B(BG``!$1#P%

    M`"`BXBD``!$13P$`B(AX"@!`1,13```B(IX"`!`1\10`@(B(IP``1$0\!0`@

    M(N(I```1$4\!`(B(>`H`0$3$4P``(B>`@`0$?$4`("(B<``$1$/`4`("+B

    M0``$1%/`0"(B'@`$!$Q%,``"(BG@(`$!'Q%`"`B(BG``!$1#P%`"`BXBD`

    M`!$13P$`B(AX"@!`1,13```B(IX"`!`1\10`@(B(IP``1$0\!0`@(N(I```1

    M$4\!`(B(>`H`0$3$4P``(B>`@`0$?$4`("(B<``$1$/`4`("+B*0``$1%/

    M`0"(B'@*`$!$Q%,``"(BG@(`$!'Q%`"`B(BG``!$1#PE.C??_.&RNP``E$8\

    M)3K5:K7L@``I1%/B<[R\G970``2B.>$AW54P"89.(IT5$]!8!))IX2'=53

    M`)ADXBG143T%@$DFGA(=U5,`F&3B*=%1/06`22:>$AW54P"89--E=X`)E630

    MY>7E_MYW[?I2V=T'`$9%/*4<802_[7O(H#GW>.HI`(PQ@_M$Q]Q3`)ADXBG1

    M,?<4`":9>$IT5$\!8))IT1']10`)IEX2G143P%@DHFG1$?U%``FF7A=%1/

    M`6"2B:=$1_44`":9>$IT5$\!8)*)IP``1"2BAYH^_9,GRNX"```EBRB>GGK:

    M&2><LGX_8<./7'2II/[C4``,,443Q-LNF++S[_TDLO'#OV\O'CQY>7D]?R

    M\>/'PJ=A/N+*E9=/.V,G_W9TX\<=>3Q5,`@/$243Q-)-GTQ!-//EYW;'G%

    MRN5&,%U1_^CPX:>3>)K<7)G:7':7`0`8IKCBZ6K=='DUF];?[[MOX8(+=E3J

    M)\>S:[J/''G!#D0``&,FKGB:J9LVDFB239/W^^^_;_OV[>EM(94>/7I$/`4`

    M&#.QQ=-C23Y-3T,V3:QDT:],%]^>7JU`EE=QD`@&&**YZN:,PTS633<].+

    MU6HU'=]/@NR4ZBD`P'B)YZ&D?TD@Z;9]+SSS@O7PVEV[NGR\O%5?44`&"L

    MQ!9/&NB+KA@Q_WWWY=<>?#!![=OWUZMUI]N5<CC27\80+`\M24ZBD`P%B)

    M*YZ&C4U#&$T3ZD,//;1][GIG-35;!J(IP``8V6J[`ZLDVYN&E[GGW]N/[0

    M0P^'1?IA17]VB!\`@'$26_4T%$?70O/V[=L?>NBA<
    ])W-#.KA?,;@/`#!F

    MXHJG85O^:G5YM59:KY(FV33="36S8W]E9?]3\10`8*S$%4]?\YHMAP__)!,Z

    MJ]GM3D,J/7[\VFGUI]E>N))Y7=7P``ABRB>/K88PO;MLV]M4_53F!Q[X

    MOV>==5[9708`8,BF;[_MCK[T'#ZZ;,"W_W_///'3OV\LLO'UV_0C]5G9HZ

    MX913?O;
    ]_PP@L_?>;I@V7W&@"`8:HN+2Z4W0<``&CX__=X.*H4)A;B````

    )`$E%3D2N0F""

    `

    end

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e5frog

    On 1/24/2011 2:10 PM, Fredric wrote:

    I just want a solid layer, a hole near the middle, 1mm clear space around

    the hole on the bottom layer. So a 3mm empty space in the form of a circle,

    I was hoping to be able to use the rectangle for this and just clear that

    space somehow... When making the regtangle as a polygon I have tried

    various method of making the clearance in the bottom layer but the polygon

    part doesn't get completely round but jagged.

     

    I can try adding width to it though.

     

    >

     

    It's the center hole that needs the bottom layer cleared around it.

     

    This is not the actual design, the measurements differ, I just wanted to

    try and sort it out at home.

     

    >

    Seeing the editor of the gerber files today simply taking the rectangle and

    a filled circle, setting the circle as negative and adding them together

    makes all this a quite painful process. It's so simple but not in

    Eagle... begin 644 Image1.png

    MB5!.1PT&@H````-24A$4@```XH```J"`(```#S-#<M````*W1%6'1#<F5A

     

    You need to use the circle command to draw the bStop. It works best to

    do it from the command line, see "help circle" for the somewhat weird

    syntax. Use the HOLE command to make the proper size hole. I assume you

    got this far. The polygon surrounding the hole will avoid it by an

    amount set in the DRC. If there is nothing on your board but this hole,

    you could just change the clearance parameter ( You can figure out which

    one, between dimension and signal probably).

     

    Otherwise you draw a filled circle in the bStop layer. How do you do

    that? choose circle command, it will ask for the center of the circle,

    use the center of the hole, now go up to the parameter bar and set the

    circles width ( yes width) to zero! This makes the circle filled. That's

    right a width of zero is full width. How did you not intuitively know

    this? image Okay, it will now ask you to click on the outer diameter of

    the circle. Done.

     

    the real pro way to do this is to set the MARK and issue the commands

    HOLE x (R0 0) then CIR 0 (R0 0) (R0 y)   where x and y are drill

    diameter and stop radius. You can also use CHANGE to post-humously set

    the diameter to zero, hence fill the circle.

     

    Good Luck

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e5frog

    On 1/24/2011 2:10 PM, Fredric wrote:

    I just want a solid layer, a hole near the middle, 1mm clear space around

    the hole on the bottom layer. So a 3mm empty space in the form of a circle,

    I was hoping to be able to use the rectangle for this and just clear that

    space somehow... When making the regtangle as a polygon I have tried

    various method of making the clearance in the bottom layer but the polygon

    part doesn't get completely round but jagged.

     

    I can try adding width to it though.

     

    >

     

    It's the center hole that needs the bottom layer cleared around it.

     

    This is not the actual design, the measurements differ, I just wanted to

    try and sort it out at home.

     

    >

    Seeing the editor of the gerber files today simply taking the rectangle and

    a filled circle, setting the circle as negative and adding them together

    makes all this a quite painful process. It's so simple but not in

    Eagle... begin 644 Image1.png

    MB5!.1PT&@H````-24A$4@```XH```J"`(```#S-#<M````*W1%6'1#<F5A

     

    You need to use the circle command to draw the bStop. It works best to

    do it from the command line, see "help circle" for the somewhat weird

    syntax. Use the HOLE command to make the proper size hole. I assume you

    got this far. The polygon surrounding the hole will avoid it by an

    amount set in the DRC. If there is nothing on your board but this hole,

    you could just change the clearance parameter ( You can figure out which

    one, between dimension and signal probably).

     

    Otherwise you draw a filled circle in the bStop layer. How do you do

    that? choose circle command, it will ask for the center of the circle,

    use the center of the hole, now go up to the parameter bar and set the

    circles width ( yes width) to zero! This makes the circle filled. That's

    right a width of zero is full width. How did you not intuitively know

    this? image Okay, it will now ask you to click on the outer diameter of

    the circle. Done.

     

    the real pro way to do this is to set the MARK and issue the commands

    HOLE x (R0 0) then CIR 0 (R0 0) (R0 y)   where x and y are drill

    diameter and stop radius. You can also use CHANGE to post-humously set

    the diameter to zero, hence fill the circle.

     

    Good Luck