Hi,
How do I create a stencil file which does not contain vias? I have an
Eagle Cad board design. I would like to process a cam file to
generate an output stencil file.
Thanks for any suggestions.
marc
--
Hi,
How do I create a stencil file which does not contain vias? I have an
Eagle Cad board design. I would like to process a cam file to
generate an output stencil file.
Thanks for any suggestions.
marc
--
Marc D Ronell <mronell@alumni.upenn.edu> wrote:
How do I create a stencil file which does not contain vias? I have an
Eagle Cad board design. I would like to process a cam file to
generate an output stencil file.
There is a drc setting for a via diameter limit wich masks vias below the
chosen diameter.
Am 10.03.2011 07:37, schrieb Morten Leikvoll:
Marc D Ronell <mronell@alumni.upenn.edu> wrote:
>> How do I create a stencil file which does not contain vias? I have an
>> Eagle Cad board design. I would like to process a cam file to
>> generate an output stencil file.
There is a drc setting for a via diameter limit wich masks vias below the
chosen diameter.
Just as addendum:
The limit value refers to the drill diameter of the via.
--
Mit freundlichen Gruessen / Best regards
Richard Hammerl
CadSoft Support -- hotline@cadsoft.de
FAQ: http://www.cadsoft.de/faq.htm
Am 10.03.2011 07:37, schrieb Morten Leikvoll:
Marc D Ronell <mronell@alumni.upenn.edu> wrote:
>> How do I create a stencil file which does not contain vias? I have an
>> Eagle Cad board design. I would like to process a cam file to
>> generate an output stencil file.
There is a drc setting for a via diameter limit wich masks vias below the
chosen diameter.
Just as addendum:
The limit value refers to the drill diameter of the via.
--
Mit freundlichen Gruessen / Best regards
Richard Hammerl
CadSoft Support -- hotline@cadsoft.de
FAQ: http://www.cadsoft.de/faq.htm
Marc D Ronell <mronell@alumni.upenn.edu> wrote:
If I run the gerb274x.cam job and Add a job (tab) with just the Pads
layer (17) and the tCream layer (31), I get a result which looks
reasonable in gerbv for a potential stencil. Does that approach seem
reasonable? Or does it miss something that I am not aware of yet?
That will plug all pins of through hole devices?
>>>>> "Richard" == Richard Hammerl <ric@cadsoft.de> writes:
Richard> Am 10.03.2011 07:37, schrieb Morten Leikvoll:
>> Marc D Ronell <mronell@alumni.upenn.edu> wrote:
>>> How do I create a stencil file which does not contain vias? I
>>> have an Eagle Cad board design. I would like to process a cam
>>> file to generate an output stencil file.
>>
>> There is a drc setting for a via diameter limit wich masks vias
>> below the chosen diameter.
Richard> Just as addendum: The limit value refers to the drill
Richard> diameter of the via.
If I run the gerb274x.cam job and Add a job (tab) with just the Pads
layer (17) and the tCream layer (31), I get a result which looks
reasonable in gerbv for a potential stencil. Does that approach seem
reasonable? Or does it miss something that I am not aware of yet?
Thanks,
Marc
--