Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) Re: Circuit duplication
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 188 subscribers
  • Views 353 views
  • Users 0 members are here
Related

Re: Circuit duplication

e14 Contributor
e14 Contributor over 15 years ago

hi.

 

you can copy only the .brd file with a diferent name, then, you can

duplicate.

 

warning: the new brd don't will have a schematic so, you use only for

make a panel.

 

greetings.

 

-


Mensaje original-----

De: Sharp <flakerpower@hotmail.com>

Reply-to: Sharp <flakerpower@hotmail.com>

Asunto: Re: Circuit duplication

Fecha: Wed, 13 Apr 2011 12:41:08 -0300

Grupos de noticias: eagle.userchat.eng

 

Hi, that´s working for the schematic, but when it start duplicating on the

board, there´s an error.

"Can´t execute while command is running in other window"

 

How can I fix that?

 

The error message comes for every line in the script, several times.

It´s like I copy and paste on the schematic, I still need to route on the

board, and that´s not what the script should do, right?

 

 

 

 

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    Am 13.04.2011 17:41, schrieb Sharp:

    Hi, that´s working for the schematic, but when it start duplicating on the

    board, there´s an error.

    "Can´t execute while command is running in other window"

     

    How can I fix that?

     

    The error message comes for every line in the script, several times.

    It´s like I copy and paste on the schematic, I still need to route on the

    board, and that´s not what the script should do, right?

     

     

     

    Procedure:

     

    1. Finish the part of the schematic you want to duplicate

     

    2. Place the packages in the layout

     

    3. Route the tracks (manually or with the Autorouter)

     

    4. Close the Schematic Editor

     

    5. Copy the routed layout as often as you need it with

        GROUP CUT PASTE .. PASTE .. PASTE ..

     

    6. Switch to the schematic again (EAGLE reports inconsitency)

     

    7. Multiply the schematic as you did it in the layout

        with GROUP CUT PASTE .. PASTE .. PASTE ..

        (The parts that you are pasting into the schematic

        will not appear in the layout due to the inconsistency.

        This is the intention here).

     

    8. Use EXPORT NETSCRIPT to output the netlist as script file

     

    9. Import the netscript with SCRIPT into the layout.

        (The numbering of the components and of the nets is the

        same as it is in the schematic. Exceptions are nets that

        have a supply pin or are marked with a LABEL, like GND,

        VCC, 0V......)

        The Board does not have supply pins nor labels, so this

        signals will be enumerated continuously. Copys of GND

        will be named GND1, GND2, and so on.

        While importing the netscript you have to connect for example

        GND1 and GND, the resulting name is GND, then. GND and

        GND2 will become GND, too....

     

    10. Start ERC and and check/restore consitency

     

    11. Route the remaining airwires between the copied parts

         of your design.

     

     

     

    Mit freundlichen Grüßen / Best regards

     

    Alfred Zaffran

    --

    _____________________________________________________________

    Alfred Zaffran              Support

    CadSoft Computer GmbH       Hotline:   08635-698930

    Pleidolfweg 15              FAX:       08635-698940

    84568 Pleiskirchen          eMail: <alf@cadsoft.de>

                                 Web:   <www.cadsoft.de>

    Registergericht: Amtsgericht Traunstein HRB 5573

    Geschäftsführer: Dipl.-Ing. Klaus Schmidinger, Bodo Badnowitz

    _____________________________________________________________

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    hi.

     

    you can copy only the .brd file with a diferent name, then, you can

    duplicate.

     

    warning: the new brd don't will have a schematic so, you use only for

    make a panel.

     

    greetings.

     

    -


    Mensaje original-----

    De: Sharp <flakerpower@hotmail.com>

    Reply-to: Sharp <flakerpower@hotmail.com>

    Asunto: Re: Circuit duplication

    Fecha: Wed, 13 Apr 2011 12:41:08 -0300

    Grupos de noticias: eagle.userchat.eng

     

    Hi, that´s working for the schematic, but when it start duplicating on the

    board, there´s an error.

    "Can´t execute while command is running in other window"

     

    How can I fix that?

     

    The error message comes for every line in the script, several times.

    It´s like I copy and paste on the schematic, I still need to route on the

    board, and that´s not what the script should do, right?