Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) GND and Supply layer polygons
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 188 subscribers
  • Views 430 views
  • Users 0 members are here
Related

GND and Supply layer polygons

e14 Contributor
e14 Contributor over 15 years ago

Hi,

I am currently designing a 4 layer board using layer 2 as GND and layer 3 as

VCC. Everything has come together well, but I need to isolate an area around

some connectors and Relays which will carry 240VAC.

How do I manipulate the default polygon on these layers which appears to

cover the entire board layer to the edges. (also not considered good

practice as a 1-2mm gap to the board edge is recommended to prevent short

circuits when the board is manufactured).

 

Ken

 

 

 

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    Ken Mcnabb schrieb:

     

    I am currently designing a 4 layer board using layer 2 as GND and layer 3 as

    VCC. Everything has come together well, but I need to isolate an area around

    some connectors and Relays which will carry 240VAC.

    How do I manipulate the default polygon on these layers which appears to

    cover the entire board layer to the edges.

     

    Do not use supply layers, use real polygons instead. Then you can easily

    define the outlines by yourself.

     

    Additionally, the distance to the borders is specified in the DRC

    parameters.

     

    The distance to other signal types can be set by using "classes" - see

    HELP CLASS (and/or the manual) for details. Here, you'd need a class for

    the signals carrying mains voltage, then set the minimum distance

    between this class and all other classes to (say) 6 mm, and (say) 2 mm

    within this class. The supply polygon (of one of the other classes) will

    automatically keep this distance from all objects carrying line voltage

    then (when calculated with ratsnest). Take care to run the DRC also to

    check for distance violations.

     

    Finally, common layers for ML4 are 1, 2, 15 and 16 (15 instead of 3).

     

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Ken Mcnabb schrieb:

     

    I am currently designing a 4 layer board using layer 2 as GND and layer 3 as

    VCC. Everything has come together well, but I need to isolate an area around

    some connectors and Relays which will carry 240VAC.

    How do I manipulate the default polygon on these layers which appears to

    cover the entire board layer to the edges.

     

    Do not use supply layers, use real polygons instead. Then you can easily

    define the outlines by yourself.

     

    Additionally, the distance to the borders is specified in the DRC

    parameters.

     

    The distance to other signal types can be set by using "classes" - see

    HELP CLASS (and/or the manual) for details. Here, you'd need a class for

    the signals carrying mains voltage, then set the minimum distance

    between this class and all other classes to (say) 6 mm, and (say) 2 mm

    within this class. The supply polygon (of one of the other classes) will

    automatically keep this distance from all objects carrying line voltage

    then (when calculated with ratsnest). Take care to run the DRC also to

    check for distance violations.

     

    Finally, common layers for ML4 are 1, 2, 15 and 16 (15 instead of 3).

     

    Tilmann