Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) Re: Remember projects used?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 187 subscribers
  • Views 300 views
  • Users 0 members are here
Related

Re: Remember projects used?

e14 Contributor
e14 Contributor over 15 years ago

Just looked at this again, and the problem seems to be dependant on the

'Projects' entry in the 'Directories' dialog box.

 

I have observed the following:

C:\

   Always opens with tree collapsed.

C:\SVN

   Works correctly and expands tree to currently open project.

C:\SVN\

   Works correctly and expands tree to currently open project.

C:

   Displays tree for Eagle program folder (C:\Program Files\EAGLE-5.11.0)

 

So I think the issue is that I was trying to display the tree starting from

the root directory of the C drive (I want to access projects in both C:\SVN

and C:\work).

 

This looks like a minor bug that has been introduced in version 5 as I have

verified that C:\ works fine in 4.16r2.

 

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 15 years ago

    I do not see any difference when I open Eagle V4.15 or V5.3. In both the

    applications, the project tree is always collapsed

     

    S

     

    "Oppie" <Oppie@saynotospam.com> wrote in message

    news:h4uqbt$3ta$1@cheetah.cadsoft.de...

    Just wondering, iirc, on earlier versions (V4?) of Eagle, if I exited

    control panel with design projects closed but project tree expanded out,

    then restarted Eagle, the tree was left open. I'm running Eagle 5.6 now

    and the projects directory is always collapsed when I start the control

    panel.

     

    Am I mistaken or is there a setting that recalls the state which the

    control panel was closed in?  All directories are mapped to a network

    drive so they get backed up.

     

    tia - Oppie

     

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 15 years ago

    On Fri, 31 Jul 2009 09:07:14 -0400, "Oppie" <Oppie@saynotospam.com>

    wrote:

     

    Just wondering, iirc, on earlier versions (V4?) of Eagle, if I exited

    control panel with design projects closed but project tree expanded out,

    then restarted Eagle, the tree was left open. I'm running Eagle 5.6 now and

    the projects directory is always collapsed when I start the control panel.

     

    The difference is whether or not a project is marked as "open" (with a

    green dot after it in the project tree).  If there is such a project,

    then the project tree starts opened.  If not, the project tree starts

    collapsed.  Note that you can edit a board and schematic without

    turning on the green dot.  And here's another thing that green dot

    does.  It makes the "Add Device" use the custom set of libraries for

    that project.  If you open the same schematic without the green dot,

    then  you will get a different set of libraries.

     

     

    Robert Scott

    Real-Time Specialties

    Ypsilanti, Michigan