Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) Custom pad shapes
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 188 subscribers
  • Views 504 views
  • Users 0 members are here
Related

Custom pad shapes

cosborne2000
cosborne2000 over 15 years ago

Is there a "correct" way to create a through hole pad with different diameters on the top and bottom (same drill size of course)?

I've created a part that attaches with a small screw with a spacer on the opposite side.  The bottom pad needs to be large (0.3inches) to cover the area under the bolt head.

The top pad just needs to be large enough for the plated through hole.  Using a standard pad (large diameter on both sides) makes routing very difficult in that area.

 

I created a circle around the pad in the bottom copper and solder stop layers for now.  This works but always generates a DRC error which I have to ignore.

In Orcad and Altium I simply make the correct padstack -- is there some type of equivalent in Eagle?

 

Thank you for your help,

Chris

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    cosborne2000 wrote:

    Is there a "correct" way to create a through hole pad with different

    diameters on the top and bottom (same drill size of course)?

    I've created a part that attaches with a small screw with a spacer on

    the opposite side. The bottom pad needs to be large (0.3inches) to

    cover the area under the bolt head. The top pad just needs to be

    large enough for the plated through hole. Using a standard pad (large

    diameter on both sides) makes routing very difficult in that area.

     

    I created a circle around the pad in the bottom copper and solder

    stop layers for now. This works but always generates a DRC error

    which I have to ignore.

    In Orcad and Altium I simply make the correct padstack -- is there

    some type of equivalent in Eagle?

     

     

    Eagle does not currently have pad stacks. They are on the wish list.

    For the large pad, draw a polygon circle (0.3inches) over that bottom pad

    and give it the same 'name' as the signal to the pad you are covering.

    In this way you will not get a DRC error.

    In the library part to remind you of the need for the large pad, create the

    polygon/circle on  a custom layer or doc layer. In this way it can be used

    as a template for the size of the polygon when you draw it in the board

    editor.

     

    Warren

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    "Warren Brayshaw" <warrenbrayshaw@paradise.net.nz> wrote:

    cosborne2000 wrote:

    >> Is there a "correct" way to create a through hole pad with different

    >> diameters on the top and bottom (same drill size of course)?

    >> I've created a part that attaches with a small screw with a spacer on

    >> the opposite side. The bottom pad needs to be large (0.3inches) to

    >> cover the area under the bolt head. The top pad just needs to be

    >> large enough for the plated through hole. Using a standard pad (large

    >> diameter on both sides) makes routing very difficult in that area.

    >>

    >> I created a circle around the pad in the bottom copper and solder

    >> stop layers for now. This works but always generates a DRC error

    >> which I have to ignore.

    >> In Orcad and Altium I simply make the correct padstack -- is there

    >> some type of equivalent in Eagle?

    >>

     

    Eagle does not currently have pad stacks. They are on the wish list.

    For the large pad, draw a polygon circle (0.3inches) over that bottom pad

    and give it the same 'name' as the signal to the pad you are covering.

    In this way you will not get a DRC error.

    In the library part to remind you of the need for the large pad, create the

    polygon/circle on  a custom layer or doc layer. In this way it can be used

    as a template for the size of the polygon when you draw it in the board

    editor.

     

    Alternatively I guess you can just use keepout/restrict in library. The

    spacer side doesnt need to be fully filled, but you want to avoid shorts

    and components.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    On 07/07/2011 01:13 AM, Morten Leikvoll wrote:

    "Warren Brayshaw" <warrenbrayshaw@paradise.net.nz> wrote:

    >> cosborne2000 wrote:

    >>> Is there a "correct" way to create a through hole pad with different

    >>> diameters on the top and bottom (same drill size of course)?

    >>> I've created a part that attaches with a small screw with a spacer on

    >>> the opposite side. The bottom pad needs to be large (0.3inches) to

    >>> cover the area under the bolt head. The top pad just needs to be

    >>> large enough for the plated through hole. Using a standard pad (large

    >>> diameter on both sides) makes routing very difficult in that area.

    >>>

    >>> I created a circle around the pad in the bottom copper and solder

    >>> stop layers for now. This works but always generates a DRC error

    >>> which I have to ignore.

    >>> In Orcad and Altium I simply make the correct padstack -- is there

    >>> some type of equivalent in Eagle?

    >>>

    >> Eagle does not currently have pad stacks. They are on the wish list.

    >> For the large pad, draw a polygon circle (0.3inches) over that bottom pad

    >> and give it the same 'name' as the signal to the pad you are covering.

    >> In this way you will not get a DRC error.

    >> In the library part to remind you of the need for the large pad, create the

    >> polygon/circle on  a custom layer or doc layer. In this way it can be used

    >> as a template for the size of the polygon when you draw it in the board

    >> editor.

    Alternatively I guess you can just use keepout/restrict in library. The

    spacer side doesnt need to be fully filled, but you want to avoid shorts

    and components.

    In addition to the keepout/restrict layers, you could draw the circle in

    the library on a layer that is included with your copper layer in your

    cam job.  You'd have to keep the keepout and restrict layers since DRC

    doesn't understand that the additional layer is destined to be copper.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    On 07/07/2011 01:13 AM, Morten Leikvoll wrote:

    "Warren Brayshaw" <warrenbrayshaw@paradise.net.nz> wrote:

    >> cosborne2000 wrote:

    >>> Is there a "correct" way to create a through hole pad with different

    >>> diameters on the top and bottom (same drill size of course)?

    >>> I've created a part that attaches with a small screw with a spacer on

    >>> the opposite side. The bottom pad needs to be large (0.3inches) to

    >>> cover the area under the bolt head. The top pad just needs to be

    >>> large enough for the plated through hole. Using a standard pad (large

    >>> diameter on both sides) makes routing very difficult in that area.

    >>>

    >>> I created a circle around the pad in the bottom copper and solder

    >>> stop layers for now. This works but always generates a DRC error

    >>> which I have to ignore.

    >>> In Orcad and Altium I simply make the correct padstack -- is there

    >>> some type of equivalent in Eagle?

    >>>

    >> Eagle does not currently have pad stacks. They are on the wish list.

    >> For the large pad, draw a polygon circle (0.3inches) over that bottom pad

    >> and give it the same 'name' as the signal to the pad you are covering.

    >> In this way you will not get a DRC error.

    >> In the library part to remind you of the need for the large pad, create the

    >> polygon/circle on  a custom layer or doc layer. In this way it can be used

    >> as a template for the size of the polygon when you draw it in the board

    >> editor.

    Alternatively I guess you can just use keepout/restrict in library. The

    spacer side doesnt need to be fully filled, but you want to avoid shorts

    and components.

    In addition to the keepout/restrict layers, you could draw the circle in

    the library on a layer that is included with your copper layer in your

    cam job.  You'd have to keep the keepout and restrict layers since DRC

    doesn't understand that the additional layer is destined to be copper.