Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) settings for masks solder stop and cream
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 187 subscribers
  • Views 1114 views
  • Users 0 members are here
Related

settings for masks solder stop and cream

hansi99
hansi99 over 15 years ago

who can please explain the min,  % and max values?

  • Sign in to reply
  • Cancel
Parents
  • Richard_H
    Richard_H over 15 years ago

    Am 07.07.2011 15:14, schrieb hansi99:

    who can please explain the min,  % and max values?

     

     

     

    Here helps a look into the manual......

     

    Masks:

     

    Settings for the overmeasure of the solder stop mask (Stop) and the

    solder cream mask (Cream) are made here.

    The default value for solder stop is 4 mil, i.e. minimum value is

    maximum value is 4 mil. The percent value has no effect in this case.

    The value for the cream frame is set to 0, which means that it has the

    same dimensions as the SMD.

    If values are given in percent, in the case of SMDs and pads of the form

    Long or Offset, the smaller dimension is the significant one. The values

    are constrained by minimum and maximum values.

     

    The value for Cream is given positively, as is Frame, although its

    effect is to reduce the size of the solder cream mask (cream frame).

    The solder cream mask is only generated for SMDs, and is displayed on

    layer 31, tCream, or layer 32, bCream.

    The solder stop mask is drawn in layers 29, tStop, or 30, bStop.

     

    Setting the flag STOP or CREAM (only for SMD) to OFF for a pad or SMD at

    the Package definition forbids EAGLE to generate a solder stop mask or a

    cream frame for it.

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/faq.htm

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Richard_H
    Richard_H over 15 years ago

    Am 07.07.2011 15:14, schrieb hansi99:

    who can please explain the min,  % and max values?

     

     

     

    Here helps a look into the manual......

     

    Masks:

     

    Settings for the overmeasure of the solder stop mask (Stop) and the

    solder cream mask (Cream) are made here.

    The default value for solder stop is 4 mil, i.e. minimum value is

    maximum value is 4 mil. The percent value has no effect in this case.

    The value for the cream frame is set to 0, which means that it has the

    same dimensions as the SMD.

    If values are given in percent, in the case of SMDs and pads of the form

    Long or Offset, the smaller dimension is the significant one. The values

    are constrained by minimum and maximum values.

     

    The value for Cream is given positively, as is Frame, although its

    effect is to reduce the size of the solder cream mask (cream frame).

    The solder cream mask is only generated for SMDs, and is displayed on

    layer 31, tCream, or layer 32, bCream.

    The solder stop mask is drawn in layers 29, tStop, or 30, bStop.

     

    Setting the flag STOP or CREAM (only for SMD) to OFF for a pad or SMD at

    the Package definition forbids EAGLE to generate a solder stop mask or a

    cream frame for it.

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/faq.htm