Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) Delete individual signals
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 188 subscribers
  • Views 1042 views
  • Users 0 members are here
Related

Delete individual signals

e14 Contributor
e14 Contributor over 15 years ago

Greetings,

 

I'm trying to use Eagle's scripting commands to delete a particular signal present on the board.  Typing "delete signals" will delete all signals, but I just want to delete one signal by its name, using script commands only.  (I don't want to undo any more routing than necessary by issuing a command to delete signals, and consequently have to add them all back again and start over in the routing process.)  It appears the delete command wants an element name as its argument, and not a signal name.  I can delete a particular airwire using the delete command if I give it a coordinate of the airwire as its argument, however I cannot know this coordinate information outside of the board where I'm generating the script, so this way won't work for me.

 

I am using the layout editor only (no forward/back-annotation with a schematic).  The reason why we are not using the schematic editor is because we are developing a new PCB hardware description language called PHDL (similar to VHDL) that describes PCB schematics in pure text, therefore there is no need for the schematic capture side of the tools.  It is our hope that hierarchical PCB IP can be generated and "instanced" in new PCB designs, alleviating the bottleneck inherent with re-inventing a new PCB from scratch every time.

 

With that, does anyone know if the delete command supports deleting entire signals from within the layout editor, and what its syntax is?

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    On 8/15/2011 6:22 PM, Brad R wrote:

    Greetings,

     

    I'm trying to use Eagle's scripting commands to delete a particular signal present on the board.  Typing "delete signals" will delete all signals, but I just want to delete one signal by its name, using script commands only.  (I don't want to undo any more routing than necessary by issuing a command to delete signals, and consequently have to add them all back again and start over in the routing process.)  It appears the delete command wants an element name as its argument, and not a signal name.  I can delete a particular airwire using the delete command if I give it a coordinate of the airwire as its argument, however I cannot know this coordinate information outside of the board where I'm generating the script, so this way won't work for me.

     

    I am using the layout editor only (no forward/back-annotation with a schematic).  The reason why we are not using the schematic editor is because we are developing a new PCB hardware description language called PHDL (similar to VHDL) that describes PCB schematics in pure text, therefore there is no need for the schematic capture side of the tools.  It is our hope that hierarchical PCB IP can be generated and "instanced" in new PCB designs, alleviating the bottleneck inherent with re-inventing a new PCB from scratch every time.

     

    With that, does anyone know if the delete command supports deleting entire signals from within the layout editor, and what its syntax is?

     

     

    Hi Brad,

     

    I believe Warren's description is correct. I just wanted to add that

    with the next release of EAGLE our file format will be XML and

    completely text-based. So the capabilities you are seeking to create

    with PHDL will become available.

     

    hth,

     

    Jorge Garcia.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    Brad R wrote:

     

    With that, does anyone know if the delete command supports deleting

    entire signals from within the layout editor, and what its syntax is?

     

    As I understand it, this cannot be done,  I'm prepared to be corrected

    though.

     

    An option is a small ULP which you call from your script that finds the

    coords and deletes the signal at that time.

    If the signal is routed,first ripup the signal by name and then find the

    coords of the remaining airwire/airwires and delete them.

     

    HTH

    Warren