Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) Standard for library creation version
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 19 replies
  • Subscribers 188 subscribers
  • Views 3260 views
  • Users 0 members are here
Related

Standard for library creation version

e14 Contributor
e14 Contributor over 14 years ago

Hello,

 

See below, we welcome any suggestions and feedback in preparations for

final release.

 

Best Regards,

Cadsoft Support Team.

 

Library Management and Part Creation Standard v0.1

by Cadsoft Computer Support

10/13/2011

 

Objective: The intent of this document is to provide a BASIC guideline

as to the best practices for developing user libraries. We have noticed

differing levels of quality among user contributed libraries and our

hope is that by developing this standard we will help raise the overall

quality of user contributed libraries.

 

Usage: This document is split up into four main sections, Library,

Symbols, Packages, and Devices. Under each main section the best

practices for that section are outlined followed by some supplemental

recommendations which are generally applicable, however they are not as

strictly recommended as the best practices.

 

Libraries

1.Do not modify EAGLE's default libraries. They represent a known state

which support staff can rely on when assisting users. The preferred

approach is to copy elements into a user made library and then modify

them to suit your needs.

Copy procedures are discussed in the EAGLE manual section 8.12.

2.User libraries should not be stored in EAGLE's internal lib folder.

The reason being that if anything should happen to your EAGLE

installation(deletion, uninstall, viruses, hardware failure, etc.) your

libraries will be gone with it. It therefore recommended to store your

libraries in a separate location that can be easily backed up.

 

Recommendations for Libraries

1.In light of practice number 2 listed above, below are some suggestions

for best use of user developed libraries.

Some users like to make a separate library for each project they work on

and store it along with the board and schematic file that way everything

is together and easily accessible. A simple USE command in the

schematic/board editor will make the library active and available for

the ADD command.

Another possible scheme, is to store all of the libraries in a single

folder located outside of EAGLE's internal directory, and then include

it's path in the Library search directory. The advantage of this method

is that all of the user libraries are in one place for easy back ups.

Section 4.1 of the EAGLE manual discusses the Directories dialog.

Set a second path to your own library in Control-Panel | Options |

Directories | Libraries

 

Symbols

1.Symbol pins must always align to a 0.1”(2.54mm) grid.

2.Symbols must always have >NAME and >VALUE place holders on layers 95

Names and 96 Values respectively.

3.Place >NAME on top, and >VALUE on bottom side of the symbol.

4.Center the symbol around the origin.

 

Recommendations for Symbols

1.Power pins should generally have their pin direction parameter set to Pwr.

2.Input pins should generally have their pin direction parameter set to IN.

3.Output pins should generally have their pin direction parameter set to

OUT.

4.Passive pins should generally have their pin direction parameter set

to PAS.

5.Also IO, HIZ, NC.

6.Do not use pin direction SUP for a normal Symbols. SUP is only for

supply-pins!

7.Any symbol notes or tips should be on layer 97 info.

8.It is better to give general names(OP AMP, DIODE, etc.) to symbols

instead of specific part numbers (LM741, 1N4007, etc.). This makes it

easy to reuse the symbol if your library is going to contain many

variations of the same type of component for example a library full of

op amps can probably make use of one op amp symbol.

9.For the >NAME and >VALUE text use a text size of 70 mils.

 

Packages

1.Design a package assuming that it will be placed on top of the board

(Use t layers). The MIRROR command can then be used on the board layout

to put a component on the bottom of the board.

Use tPlace for the component silkscreen which is printed on the PCB and

should not contact solder.

Use tDocu to draw leads of components leading to pads.

Use tNames for the >NAME place holder for the reference designator that

will be on the silkscreen.

Use tValues for the >VALUE place holder, which will not be part of the

silkscreen.

Use layer 48 Document or layer 49 Reference for any artistic features or

notes that will not appear on the silkscreen.

 

2.Center the package around the origin.

Recommendations for Packages

1.For the >NAME and >VALUE text use a text size of 70 mils.

2.Draw outline of package in tPlace with wire width 8 mil or 4mil.

3.The ADD command in the board editor searches through the description

field, so a well setup description field can yield more fruitful

searches. Therefore a good description field for a package should include:

Standard package name(preferably in bold)

Any possible aliases for the package. For example a DIL08 package might

also be known as a DIP08.

If the package is based off of a standard document such as one of the

IPC standards, then it should be referenced in the description field if

possible as an HTML link. If a link is not possible then a reference to

the name of the document should be sufficient. Listing this information

will help in checking the package for correctness.

If applicable length x width dimension.

 

Devices

1.Always set a prefix, otherwise EAGLE will use U$ by default.

2.When creating multi-gated components, EAGLE will by default reference

them as G$1, G$2, etc. These names will not show up on the schematic,

therefore use the NAME command to rename the gates A, B, C, etc. A nice

way to do this is to type 'A' followed by enter when you have the gate

on your mouse cursor before placing it, EAGLE will then continue the

pattern for the other gates.

3.Use P for power symbols.

4.When naming devices use specific part numbers.

5.Always double check add levels and swap levels, otherwise your

components might not enter your schematic as you'd expect them to.

Recommendations for Devices

1.Just like packages, having a good description field can improve the

chances of the ADD command finding the component you want. A good

description field for a device should include:

Device name(preferably in bold).

Any other aliases the device might be recognized by.

A link or reference to the device's data sheet.

Manufacturer(s).

Short explanation of the device's function.

If applicable length x width dimension.

 

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Am 22.10.2011 00:38, schrieb Jorge Garcia:

    1.Do not modify EAGLE's default libraries.

     

    Yes.

     

    2.User libraries should not be stored in EAGLE's internal lib folder.

     

    For beginners, that seems to be OK. For people who only use their OWN

    libraries (and NOT the CadSoft ones), that could be cumbersome, but

    anyway...

     

    1.Symbol pins must always align to a 0.1”(2.54mm) grid.

    2.Symbols must always have >NAME and >VALUE place holders on layers 95

    Names and 96 Values respectively.

     

    Yes and Yes.

     

    3.Place >NAME on top, and >VALUE on bottom side of the symbol.

     

    That is NOT always my recommendation: For SMALL symbols (resistors,

    capacitors, and whatnots), that works very well. BUT a part's name and

    value should be NEAR each other, so that one can easily find BOTH of

    them. Therefore, for large ICs, your suggestion would mean ripping them

    apart quite considerably. For such parts, I put both of them on top.

    Since this is something of QUITE personal preference, I wouldn't give

    any recommendation, but just state that both of them SHOULD BE AVAILABLE

    (some people leave them out).

     

    4.Center the symbol around the origin.

     

    Yes. Approximately. So that all pins are STILL on a 0.1" grid.

     

    1.Power pins should generally have their pin direction parameter set to

    Pwr.

    2.Input pins should generally have their pin direction parameter set to IN.

    3.Output pins should generally have their pin direction parameter set to

    OUT.

    4.Passive pins should generally have their pin direction parameter set

    to PAS.

    5.Also IO, HIZ, NC.

    6.Do not use pin direction SUP for a normal Symbols. SUP is only for

    supply-pins!

    7.Any symbol notes or tips should be on layer 97 info.

    8.It is better to give general names(OP AMP, DIODE, etc.) to symbols

    instead of specific part numbers (LM741, 1N4007, etc.). This makes it

    easy to reuse the symbol if your library is going to contain many

    variations of the same type of component for example a library full of

    op amps can probably make use of one op amp symbol.

     

    Yes for 1 to 8.

     

    9.For the >NAME and >VALUE text use a text size of 70 mils.

     

    This perhaps is too user-dependent. I wouldn't give a recommendation

    here, but anything from 50 to 80 mils seems to be OK (I myself prefer

    60mil).

     

    1.Design a package assuming that it will be placed on top of the board

    (Use t layers). The MIRROR command can then be used on the board layout

    to put a component on the bottom of the board.

    Use tPlace for the component silkscreen which is printed on the PCB and

    should not contact solder.

     

    Yes and yes.

     

    Use tDocu to draw leads of components leading to pads.

    Use tNames for the >NAME place holder for the reference designator that

    will be on the silkscreen.

    Use tValues for the >VALUE place holder, which will not be part of the

    silkscreen.

    Use layer 48 Document or layer 49 Reference for any artistic features or

    notes that will not appear on the silkscreen.

     

    Well, erm, in principle, why not...

     

    2.Center the package around the origin.

     

    Yes. Approximately. But, if possible, still leave all pads on a DECENT

    grid. Grid position takes precedence over centering.

     

    1.For the >NAME and >VALUE text use a text size of 70 mils.

     

    I do NOT recommend that AT ALL: With typical board densities, this text

    size is TOO LARGE for the silkscreen and consumes TOO much space. In

    order to create relatively small text that can still be read, but also

    has more than 0.2mm wire thickness (which is a common minimal width for

    manufacturing) to pass typical DRCs, I recommend a text size of 50mil

    AND a text ratio of 16%.

     

    2.Draw outline of package in tPlace with wire width 8 mil or 4mil.

     

    8mil is OK, 4mil is NOT: Board manufacturers often have minimal width

    restraints of 0.2mm (8mil is JUST larger than that) or 0.15mm (4mil is

    even below THAT). 4mil is a very nice width for paper printouts, but NOT

    for the silkscreen.

     

    3.The ADD command in the board editor searches through the description

    field, so a well setup description field can yield more fruitful

    searches. Therefore a good description field for a package should include:

    Standard package name(preferably in bold)

    Any possible aliases for the package. For example a DIL08 package might

    also be known as a DIP08.

     

    Yes.

     

    If the package is based off of a standard document such as one of the

    IPC standards, then it should be referenced in the description field if

    possible as an HTML link. If a link is not possible then a reference to

    the name of the document should be sufficient. Listing this information

    will help in checking the package for correctness.

    If applicable length x width dimension.

     

    For web-based documents, that's OK. It gets harder for LOCAL references:

    What I would like to do is putting small PHOTOS of the mechanical

    component in a device description (of course not for ICs or such, but

    for mechanically special parts such as switches, connectors etc.). The

    pictures should be saved in a certain subfolder of the library path.

    Referencing such is not so easy. In my 'eagle.betatest' post form

    2010-09-29, I suggested the following:

     

    --- snip ---

      2. (This just came into my mind today) Support your nice

         '$EAGLEDIR' or '$HOME' syntax inside HTML references. This way,

         the definition of references could be platform-independent,

         clear, images could be referenced relative to the appropriate

         folder, and even the schematics could use this path without

         problems.

         DISADVANTAGES: Since your QT library surely does not support

         such a feature, a preprocessing of the string would be

         necessary.

    --- snap ---

     

    Walter Spermann answered to that:

       'That's a good idea, thanks. We keep this as a suggestion for a

       future version (not 5.11 though).'

     

    Perhaps it can be included in version 6...

     

    1.Always set a prefix, otherwise EAGLE will use U$ by default.

    2.When creating multi-gated components, EAGLE will by default reference

    them as G$1, G$2, etc. These names will not show up on the schematic,

    therefore use the NAME command to rename the gates A, B, C, etc. A nice

    way to do this is to type 'A' followed by enter when you have the gate

    on your mouse cursor before placing it, EAGLE will then continue the

    pattern for the other gates.

    3.Use P for power symbols.

    4.When naming devices use specific part numbers.

    5.Always double check add levels and swap levels, otherwise your

    components might not enter your schematic as you'd expect them to.

    Recommendations for Devices

    1.Just like packages, having a good description field can improve the

    chances of the ADD command finding the component you want. A good

    description field for a device should include:

    Device name(preferably in bold).

    Any other aliases the device might be recognized by.

    A link or reference to the device's data sheet.

    Manufacturer(s).

    Short explanation of the device's function.

    If applicable length x width dimension.

     

    Yes to all of the above.

     

    Andreas Weidner

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Andreas Weidner schrieb:

     

    Am 22.10.2011 00:38, schrieb Jorge Garcia:

    >> 1.Do not modify EAGLE's default libraries.

     

    Yes.

     

    Indeed.

     

    >> 2.User libraries should not be stored in EAGLE's internal lib folder.

     

    For beginners, that seems to be OK. For people who only use their OWN

    libraries (and NOT the CadSoft ones), that could be cumbersome, but

    anyway...

     

    Additionally: EAGLEs internal libraries should NOT be installed in a

    subdirectory of the programs installation path. This also applies to all

    other "data" directories (projects, ULPs, SCRs, CAM jobs etc.).

     

    >> 1.Symbol pins must always align to a 0.1”(2.54mm) grid.

    >> 2.Symbols must always have >NAME and >VALUE place holders on layers 95

    >> Names and 96 Values respectively.

     

    Yes and Yes.

     

    ...and yes.

     

    >> 3.Place >NAME on top, and >VALUE on bottom side of the symbol.

     

    That is NOT always my recommendation: For SMALL symbols (resistors,

    capacitors, and whatnots), that works very well. BUT a part's name and

    value should be NEAR each other, so that one can easily find BOTH of

    them. Therefore, for large ICs, your suggestion would mean ripping them

    apart quite considerably. For such parts, I put both of them on top.

    Since this is something of QUITE personal preference, I wouldn't give

    any recommendation, but just state that both of them SHOULD BE AVAILABLE

    (some people leave them out).

     

    I fully agree to this. For symbols larger than that of a resistor or

    diode, I always place >NAME and >VALUE close to each other. (Normally on

    top of the symbol, but that's my personal taste, of course.)

     

    >> 4.Center the symbol around the origin.

     

    Yes. Approximately. So that all pins are STILL on a 0.1" grid.

     

    Exactly.

     

    >> 1.Power pins should generally have their pin direction parameter set to

    >> Pwr.

    >> 2.Input pins should generally have their pin direction parameter set to IN.

    >> 3.Output pins should generally have their pin direction parameter set to

    >> OUT.

    >> 4.Passive pins should generally have their pin direction parameter set

    >> to PAS.

    >> 5.Also IO, HIZ, NC.

    >> 6.Do not use pin direction SUP for a normal Symbols. SUP is only for

    >> supply-pins!

    >> 7.Any symbol notes or tips should be on layer 97 info.

    >> 8.It is better to give general names(OP AMP, DIODE, etc.) to symbols

    >> instead of specific part numbers (LM741, 1N4007, etc.). This makes it

    >> easy to reuse the symbol if your library is going to contain many

    >> variations of the same type of component for example a library full of

    >> op amps can probably make use of one op amp symbol.

     

    Yes for 1 to 8.

     

    Pin directions are somewhat difficult since they may lead to many

    "false" DRC complaints. For example, different (ly named) power pins at

    ICs which would ask for equally named nets.

    But, "generally", this is OK. Of course, there are exceptions...

     

    I suggest an additional rule here regarding pins:

    Never name pins with respect to pad numbers/names later in the device

    resp. package. Pin names always should represent the function of the

    pin, nothing else.

     

    >> 9.For the >NAME and >VALUE text use a text size of 70 mils.

     

    This perhaps is too user-dependent. I wouldn't give a recommendation

    here, but anything from 50 to 80 mils seems to be OK (I myself prefer

    60mil).

     

    Agreed - but as a general starting point, 70 mil appears OK to me.

     

    >> 1.Design a package assuming that it will be placed on top of the board

    >> (Use t layers). The MIRROR command can then be used on the board layout

    >> to put a component on the bottom of the board.

    >> Use tPlace for the component silkscreen which is printed on the PCB and

    >> should not contact solder.

     

    Yes and yes.

     

    and yes.

     

    And one more additional suggestion, regarding pads:

    Never name pads regarding to a (real, intended or theoretical) function

    within a device. Pad names ALWAYS should represent the "official" names

    (normally numbers) of the pure package, nothing else.

     

    >> Use tDocu to draw leads of components leading to pads.

    >> Use tNames for the >NAME place holder for the reference designator that

    >> will be on the silkscreen.

    >> Use tValues for the >VALUE place holder, which will not be part of the

    >> silkscreen.

    >> Use layer 48 Document or layer 49 Reference for any artistic features or

    >> notes that will not appear on the silkscreen.

     

    Well, erm, in principle, why not...

     

    Personally I find it useful to distinguish between SMD and THT

    components - unfortunately, there aren't enough layers to fully do that,

    so I use tDocu for SMD outlines, names and values. If I want to print

    the part name in silkscreen, I can change its layer to tNames after a SMASH.

     

    As generel hints, that suggestion appears OK - at this issue, personal

    taste will greatly vary anyway...

     

    >> 2.Center the package around the origin.

     

    Yes. Approximately. But, if possible, still leave all pads on a DECENT

    grid. Grid position takes precedence over centering.

     

    No, in most cases centering takes precedence over pad grids. It's pretty

    common that packages have off-grid pads anyway, and it's no problem for

    EAGLE to deal with them (meanwhile). The mechanical position of a part

    often is relevant, and that should be easily derived from its origin

    (i.e. the center of a connector or an LED) for further mechanical design

    work.

     

    ONLY if the center of the package is not relevant at all, AND all pads

    become on-grid by that, grid position may take precedence over centering.

     

    >> 1.For the >NAME and >VALUE text use a text size of 70 mils.

     

    I do NOT recommend that AT ALL: With typical board densities, this text

    size is TOO LARGE for the silkscreen and consumes TOO much space. In

    order to create relatively small text that can still be read, but also

    has more than 0.2mm wire thickness (which is a common minimal width for

    manufacturing) to pass typical DRCs, I recommend a text size of 50mil

    AND a text ratio of 16%.

     

    Agreed. The appropriate size of the silkscreen text varies with board

    density. At low density boards, I commonly use 1.6 mm text size - and

    with increasing density, I reduce that to 1.3 or even 1.0 mm. Thanks to

    GROUP SMASH and GROUP CHANGE SIZE that's no big deal.

     

    Additionally, the texts of SMD components should be smaller anyway, or

    they wouldn't fit in even the paper printout (they're not in the

    silkscreen, anyway, but you need a proper documentation as PDF or on

    paper including the SMD parts). I commonly use 1 mm, sometimes I need to

    reduce to 0.8 mm.

     

    >> 2.Draw outline of package in tPlace with wire width 8 mil or 4mil.

     

    8mil is OK, 4mil is NOT: Board manufacturers often have minimal width

    restraints of 0.2mm (8mil is JUST larger than that) or 0.15mm (4mil is

    even below THAT). 4mil is a very nice width for paper printouts, but NOT

    for the silkscreen.

     

    Exactly. 0.2 mm (or 8 mil) are good measures.

     

    >> 3.The ADD command in the board editor searches through the description

    >> field, so a well setup description field can yield more fruitful

    >> searches. Therefore a good description field for a package should include:

    >> Standard package name(preferably in bold)

    >> Any possible aliases for the package. For example a DIL08 package might

    >> also be known as a DIP08.

     

    Yes.

     

    Yes.

     

    >> If the package is based off of a standard document such as one of the

    >> IPC standards, then it should be referenced in the description field if

    >> possible as an HTML link. If a link is not possible then a reference to

    >> the name of the document should be sufficient. Listing this information

    >> will help in checking the package for correctness.

    >> If applicable length x width dimension.

     

    For web-based documents, that's OK. It gets harder for LOCAL references:

     

    Even for web based documents, that won't work satisfying. Document URLs

    change, some disappear completely. So it's always necessary to include a

    reference in human readable text form, i.e. "IPC-xxxx, Section X.Y, case

    ABCD"). As a PCB CAD tool, EAGLE should not require dealing with the

    validity of web links...

     

    >> 1.Always set a prefix, otherwise EAGLE will use U$ by default.

    >> 2.When creating multi-gated components, EAGLE will by default reference

    >> them as G$1, G$2, etc. These names will not show up on the schematic,

    >> therefore use the NAME command to rename the gates A, B, C, etc. A nice

    >> way to do this is to type 'A' followed by enter when you have the gate

    >> on your mouse cursor before placing it, EAGLE will then continue the

    >> pattern for the other gates.

    >> 3.Use P for power symbols.

    >> 4.When naming devices use specific part numbers.

    >> 5.Always double check add levels and swap levels, otherwise your

    >> components might not enter your schematic as you'd expect them to.

    >> Recommendations for Devices

    >> 1.Just like packages, having a good description field can improve the

    >> chances of the ADD command finding the component you want. A good

    >> description field for a device should include:

    >> Device name(preferably in bold).

    >> Any other aliases the device might be recognized by.

    >> A link or reference to the device's data sheet.

    >> Manufacturer(s).

    >> Short explanation of the device's function.

    >> If applicable length x width dimension.

     

    Yes to all of the above.

     

    ...except to 4.

    Correct that to: Use generic devices wherever possible.

     

    If you use specific part numbers, you'll end up with zillions of

    identical devices, just with different names (i.e. TL072, MC1458, LM358,

    TLC272, TLV272, etc. pp.).

     

    For this particular example, I have one device for a dual opamp in

    standard pinout, with the common package variants (DIP, SO, etc.). After

    having placed it in a schematic, I simply set its VALUE to the correct one.

     

    The same applies to all parts with standard packages and pinouts: many

    transistors, thyristors and TRIACs, comparators, voltage regulators etc.

    Only those that don't share a standard pinout need their own devices.

     

    (The same rule can be applied to more complex parts as well, i.e.

    microcontrollers with different features or memory sizes, but the same

    symbol and pinout. They need only one device - with a properly set value.)

     

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Am 22.10.2011 17:33, schrieb Tilmann Reh:

    Andreas Weidner schrieb:

     

    >> Am 22.10.2011 00:38, schrieb Jorge Garcia:

    >>> 1.Do not modify EAGLE's default libraries.

    >>

    >> Yes.

     

    Indeed.

     

    >>> 2.User libraries should not be stored in EAGLE's internal lib folder.

    >>

    >> For beginners, that seems to be OK. For people who only use their OWN

    >> libraries (and NOT the CadSoft ones), that could be cumbersome, but

    >> anyway...

     

    Additionally: EAGLEs internal libraries should NOT be installed in a

    subdirectory of the programs installation path. This also applies to all

    other "data" directories (projects, ULPs, SCRs, CAM jobs etc.).

     

    >>> 1.Symbol pins must always align to a 0.1”(2.54mm) grid.

    >>> 2.Symbols must always have>NAME and>VALUE place holders on layers 95

    >>> Names and 96 Values respectively.

    >>

    >> Yes and Yes.

     

    ...and yes.

     

    wire width for symbol outlines 16 mil.

     

    >>> 3.Place>NAME on top, and>VALUE on bottom side of the symbol.

    >>

    >> That is NOT always my recommendation: For SMALL symbols (resistors,

    >> capacitors, and whatnots), that works very well. BUT a part's name and

    >> value should be NEAR each other, so that one can easily find BOTH of

    >> them. Therefore, for large ICs, your suggestion would mean ripping them

    >> apart quite considerably. For such parts, I put both of them on top.

    >> Since this is something of QUITE personal preference, I wouldn't give

    >> any recommendation, but just state that both of them SHOULD BE AVAILABLE

    >> (some people leave them out).

     

    I fully agree to this. For symbols larger than that of a resistor or

    diode, I always place>NAME and>VALUE close to each other. (Normally on

    top of the symbol, but that's my personal taste, of course.)

     

    Mine too

     

    >>> 4.Center the symbol around the origin.

    >>

    >> Yes. Approximately. So that all pins are STILL on a 0.1" grid.

     

    Exactly.

     

    >>> 1.Power pins should generally have their pin direction parameter set to

    >>> Pwr.

    >>> 2.Input pins should generally have their pin direction parameter set to IN.

    >>> 3.Output pins should generally have their pin direction parameter set to

    >>> OUT.

    >>> 4.Passive pins should generally have their pin direction parameter set

    >>> to PAS.

    >>> 5.Also IO, HIZ, NC.

    >>> 6.Do not use pin direction SUP for a normal Symbols. SUP is only for

    >>> supply-pins!

    >>> 7.Any symbol notes or tips should be on layer 97 info.

    >>> 8.It is better to give general names(OP AMP, DIODE, etc.) to symbols

    >>> instead of specific part numbers (LM741, 1N4007, etc.). This makes it

    >>> easy to reuse the symbol if your library is going to contain many

    >>> variations of the same type of component for example a library full of

    >>> op amps can probably make use of one op amp symbol.

    >>

    >> Yes for 1 to 8.

     

    Pin directions are somewhat difficult since they may lead to many

    "false" DRC complaints. For example, different (ly named) power pins at

    ICs which would ask for equally named nets.

    But, "generally", this is OK. Of course, there are exceptions...

     

    I suggest an additional rule here regarding pins:

    Never name pins with respect to pad numbers/names later in the device

    resp. package. Pin names always should represent the function of the

    pin, nothing else.

    YES

    >>> 9.For the>NAME and>VALUE text use a text size of 70 mils.

    >>

    >> This perhaps is too user-dependent. I wouldn't give a recommendation

    >> here, but anything from 50 to 80 mils seems to be OK (I myself prefer

    >> 60mil).

    I use 60 mil too

     

    Agreed - but as a general starting point, 70 mil appears OK to me.

     

    >>> 1.Design a package assuming that it will be placed on top of the board

    >>> (Use t layers). The MIRROR command can then be used on the board layout

    >>> to put a component on the bottom of the board.

    >>> Use tPlace for the component silkscreen which is printed on the PCB and

    >>> should not contact solder.

    >>

    >> Yes and yes.

     

    and yes.

     

    And one more additional suggestion, regarding pads:

    Never name pads regarding to a (real, intended or theoretical) function

    within a device. Pad names ALWAYS should represent the "official" names

    (normally numbers) of the pure package, nothing else.

     

    Yes, numbers only

     

    >>> Use tDocu to draw leads of components leading to pads.

    >>> Use tNames for the>NAME place holder for the reference designator that

    >>> will be on the silkscreen.

    >>> Use tValues for the>VALUE place holder, which will not be part of the

    >>> silkscreen.

    >>> Use layer 48 Document or layer 49 Reference for any artistic features or

    >>> notes that will not appear on the silkscreen.

    >>

    >> Well, erm, in principle, why not...

     

    Personally I find it useful to distinguish between SMD and THT

    me too

     

    components - unfortunately, there aren't enough layers to fully do that,

    maybe something can be done in future version.

     

    so I use tDocu for SMD outlines, names and values. If I want to print

    the part name in silkscreen, I can change its layer to tNames after a SMASH.

     

    As generel hints, that suggestion appears OK - at this issue, personal

    taste will greatly vary anyway...

     

    >>> 2.Center the package around the origin.

    >>

    >> Yes. Approximately. But, if possible, still leave all pads on a DECENT

    >> grid. Grid position takes precedence over centering.

     

    No, in most cases centering takes precedence over pad grids. It's pretty

    common that packages have off-grid pads anyway, and it's no problem for

    EAGLE to deal with them (meanwhile). The mechanical position of a part

    often is relevant, and that should be easily derived from its origin

    (i.e. the center of a connector or an LED) for further mechanical design

    work.

     

    ONLY if the center of the package is not relevant at all, AND all pads

    become on-grid by that, grid position may take precedence over centering.

     

    >>> 1.For the>NAME and>VALUE text use a text size of 70 mils.

    >>

    >> I do NOT recommend that AT ALL: With typical board densities, this text

    >> size is TOO LARGE for the silkscreen and consumes TOO much space. In

    >> order to create relatively small text that can still be read, but also

    >> has more than 0.2mm wire thickness (which is a common minimal width for

    >> manufacturing) to pass typical DRCs, I recommend a text size of 50mil

    >> AND a text ratio of 16%.

    I use 60 size and 12 ratio

     

    Agreed. The appropriate size of the silkscreen text varies with board

    density. At low density boards, I commonly use 1.6 mm text size - and

    with increasing density, I reduce that to 1.3 or even 1.0 mm. Thanks to

    GROUP SMASH and GROUP CHANGE SIZE that's no big deal.

     

    Additionally, the texts of SMD components should be smaller anyway, or

    they wouldn't fit in even the paper printout (they're not in the

    silkscreen, anyway, but you need a proper documentation as PDF or on

    paper including the SMD parts). I commonly use 1 mm, sometimes I need to

    reduce to 0.8 mm.

     

    >>> 2.Draw outline of package in tPlace with wire width 8 mil or 4mil.

    >>

    8 mil

     

    >> 8mil is OK, 4mil is NOT: Board manufacturers often have minimal width

    >> restraints of 0.2mm (8mil is JUST larger than that) or 0.15mm (4mil is

    >> even below THAT). 4mil is a very nice width for paper printouts, but NOT

    >> for the silkscreen.

     

    Exactly. 0.2 mm (or 8 mil) are good measures.

     

    >>> 3.The ADD command in the board editor searches through the description

    >>> field, so a well setup description field can yield more fruitful

    >>> searches. Therefore a good description field for a package should include:

    >>> Standard package name(preferably in bold)

    >>> Any possible aliases for the package. For example a DIL08 package might

    >>> also be known as a DIP08.

    >>

    >> Yes.

     

    Yes.

     

    >>> If the package is based off of a standard document such as one of the

    >>> IPC standards, then it should be referenced in the description field if

    >>> possible as an HTML link. If a link is not possible then a reference to

    >>> the name of the document should be sufficient. Listing this information

    >>> will help in checking the package for correctness.

    >>> If applicable length x width dimension.

    >>

    >> For web-based documents, that's OK. It gets harder for LOCAL references:

     

    Even for web based documents, that won't work satisfying. Document URLs

    change, some disappear completely. So it's always necessary to include a

    reference in human readable text form, i.e. "IPC-xxxx, Section X.Y, case

    ABCD"). As a PCB CAD tool, EAGLE should not require dealing with the

    validity of web links...

     

    Right. Companies are sold or bought and so the search goes astray.

    >>> 1.Always set a prefix, otherwise EAGLE will use U$ by default.

    >>> 2.When creating multi-gated components, EAGLE will by default reference

    >>> them as G$1, G$2, etc. These names will not show up on the schematic,

    >>> therefore use the NAME command to rename the gates A, B, C, etc. A nice

    >>> way to do this is to type 'A' followed by enter when you have the gate

    >>> on your mouse cursor before placing it, EAGLE will then continue the

    >>> pattern for the other gates.

    >>> 3.Use P for power symbols.

    >>> 4.When naming devices use specific part numbers.

    >>> 5.Always double check add levels and swap levels, otherwise your

    >>> components might not enter your schematic as you'd expect them to.

    >>> Recommendations for Devices

    >>> 1.Just like packages, having a good description field can improve the

    >>> chances of the ADD command finding the component you want. A good

    >>> description field for a device should include:

    >>> Device name(preferably in bold).

    >>> Any other aliases the device might be recognized by.

    >>> A link or reference to the device's data sheet.

    >>> Manufacturer(s).

    >>> Short explanation of the device's function.

    >>> If applicable length x width dimension.

    >>

    >> Yes to all of the above.

     

    ...except to 4.

    Correct that to: Use generic devices wherever possible.

     

    that would be better

     

    If you use specific part numbers, you'll end up with zillions of

    identical devices, just with different names (i.e. TL072, MC1458, LM358,

    TLC272, TLV272, etc. pp.).

     

    For this particular example, I have one device for a dual opamp in

    standard pinout, with the common package variants (DIP, SO, etc.). After

    having placed it in a schematic, I simply set its VALUE to the correct one.

     

    The same applies to all parts with standard packages and pinouts: many

    transistors, thyristors and TRIACs, comparators, voltage regulators etc.

    Only those that don't share a standard pinout need their own devices.

     

    (The same rule can be applied to more complex parts as well, i.e.

    microcontrollers with different features or memory sizes, but the same

    symbol and pinout. They need only one device - with a properly set value.)

     

    Tilmann

     

    Wih a few exceptions that seems OK image

     

    It is OT here, but labels should have their own size-(ratio)-parameter.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Am 22.10.2011 17:33, schrieb Tilmann Reh:

    Andreas Weidner schrieb:

     

    >> Am 22.10.2011 00:38, schrieb Jorge Garcia:

    >>> 1.Do not modify EAGLE's default libraries.

    >>

    >> Yes.

     

    Indeed.

     

    >>> 2.User libraries should not be stored in EAGLE's internal lib folder.

    >>

    >> For beginners, that seems to be OK. For people who only use their OWN

    >> libraries (and NOT the CadSoft ones), that could be cumbersome, but

    >> anyway...

     

    Additionally: EAGLEs internal libraries should NOT be installed in a

    subdirectory of the programs installation path. This also applies to all

    other "data" directories (projects, ULPs, SCRs, CAM jobs etc.).

     

    >>> 1.Symbol pins must always align to a 0.1”(2.54mm) grid.

    >>> 2.Symbols must always have>NAME and>VALUE place holders on layers 95

    >>> Names and 96 Values respectively.

    >>

    >> Yes and Yes.

     

    ...and yes.

     

    wire width for symbol outlines 16 mil.

     

    >>> 3.Place>NAME on top, and>VALUE on bottom side of the symbol.

    >>

    >> That is NOT always my recommendation: For SMALL symbols (resistors,

    >> capacitors, and whatnots), that works very well. BUT a part's name and

    >> value should be NEAR each other, so that one can easily find BOTH of

    >> them. Therefore, for large ICs, your suggestion would mean ripping them

    >> apart quite considerably. For such parts, I put both of them on top.

    >> Since this is something of QUITE personal preference, I wouldn't give

    >> any recommendation, but just state that both of them SHOULD BE AVAILABLE

    >> (some people leave them out).

     

    I fully agree to this. For symbols larger than that of a resistor or

    diode, I always place>NAME and>VALUE close to each other. (Normally on

    top of the symbol, but that's my personal taste, of course.)

     

    Mine too

     

    >>> 4.Center the symbol around the origin.

    >>

    >> Yes. Approximately. So that all pins are STILL on a 0.1" grid.

     

    Exactly.

     

    >>> 1.Power pins should generally have their pin direction parameter set to

    >>> Pwr.

    >>> 2.Input pins should generally have their pin direction parameter set to IN.

    >>> 3.Output pins should generally have their pin direction parameter set to

    >>> OUT.

    >>> 4.Passive pins should generally have their pin direction parameter set

    >>> to PAS.

    >>> 5.Also IO, HIZ, NC.

    >>> 6.Do not use pin direction SUP for a normal Symbols. SUP is only for

    >>> supply-pins!

    >>> 7.Any symbol notes or tips should be on layer 97 info.

    >>> 8.It is better to give general names(OP AMP, DIODE, etc.) to symbols

    >>> instead of specific part numbers (LM741, 1N4007, etc.). This makes it

    >>> easy to reuse the symbol if your library is going to contain many

    >>> variations of the same type of component for example a library full of

    >>> op amps can probably make use of one op amp symbol.

    >>

    >> Yes for 1 to 8.

     

    Pin directions are somewhat difficult since they may lead to many

    "false" DRC complaints. For example, different (ly named) power pins at

    ICs which would ask for equally named nets.

    But, "generally", this is OK. Of course, there are exceptions...

     

    I suggest an additional rule here regarding pins:

    Never name pins with respect to pad numbers/names later in the device

    resp. package. Pin names always should represent the function of the

    pin, nothing else.

    YES

    >>> 9.For the>NAME and>VALUE text use a text size of 70 mils.

    >>

    >> This perhaps is too user-dependent. I wouldn't give a recommendation

    >> here, but anything from 50 to 80 mils seems to be OK (I myself prefer

    >> 60mil).

    I use 60 mil too

     

    Agreed - but as a general starting point, 70 mil appears OK to me.

     

    >>> 1.Design a package assuming that it will be placed on top of the board

    >>> (Use t layers). The MIRROR command can then be used on the board layout

    >>> to put a component on the bottom of the board.

    >>> Use tPlace for the component silkscreen which is printed on the PCB and

    >>> should not contact solder.

    >>

    >> Yes and yes.

     

    and yes.

     

    And one more additional suggestion, regarding pads:

    Never name pads regarding to a (real, intended or theoretical) function

    within a device. Pad names ALWAYS should represent the "official" names

    (normally numbers) of the pure package, nothing else.

     

    Yes, numbers only

     

    >>> Use tDocu to draw leads of components leading to pads.

    >>> Use tNames for the>NAME place holder for the reference designator that

    >>> will be on the silkscreen.

    >>> Use tValues for the>VALUE place holder, which will not be part of the

    >>> silkscreen.

    >>> Use layer 48 Document or layer 49 Reference for any artistic features or

    >>> notes that will not appear on the silkscreen.

    >>

    >> Well, erm, in principle, why not...

     

    Personally I find it useful to distinguish between SMD and THT

    me too

     

    components - unfortunately, there aren't enough layers to fully do that,

    maybe something can be done in future version.

     

    so I use tDocu for SMD outlines, names and values. If I want to print

    the part name in silkscreen, I can change its layer to tNames after a SMASH.

     

    As generel hints, that suggestion appears OK - at this issue, personal

    taste will greatly vary anyway...

     

    >>> 2.Center the package around the origin.

    >>

    >> Yes. Approximately. But, if possible, still leave all pads on a DECENT

    >> grid. Grid position takes precedence over centering.

     

    No, in most cases centering takes precedence over pad grids. It's pretty

    common that packages have off-grid pads anyway, and it's no problem for

    EAGLE to deal with them (meanwhile). The mechanical position of a part

    often is relevant, and that should be easily derived from its origin

    (i.e. the center of a connector or an LED) for further mechanical design

    work.

     

    ONLY if the center of the package is not relevant at all, AND all pads

    become on-grid by that, grid position may take precedence over centering.

     

    >>> 1.For the>NAME and>VALUE text use a text size of 70 mils.

    >>

    >> I do NOT recommend that AT ALL: With typical board densities, this text

    >> size is TOO LARGE for the silkscreen and consumes TOO much space. In

    >> order to create relatively small text that can still be read, but also

    >> has more than 0.2mm wire thickness (which is a common minimal width for

    >> manufacturing) to pass typical DRCs, I recommend a text size of 50mil

    >> AND a text ratio of 16%.

    I use 60 size and 12 ratio

     

    Agreed. The appropriate size of the silkscreen text varies with board

    density. At low density boards, I commonly use 1.6 mm text size - and

    with increasing density, I reduce that to 1.3 or even 1.0 mm. Thanks to

    GROUP SMASH and GROUP CHANGE SIZE that's no big deal.

     

    Additionally, the texts of SMD components should be smaller anyway, or

    they wouldn't fit in even the paper printout (they're not in the

    silkscreen, anyway, but you need a proper documentation as PDF or on

    paper including the SMD parts). I commonly use 1 mm, sometimes I need to

    reduce to 0.8 mm.

     

    >>> 2.Draw outline of package in tPlace with wire width 8 mil or 4mil.

    >>

    8 mil

     

    >> 8mil is OK, 4mil is NOT: Board manufacturers often have minimal width

    >> restraints of 0.2mm (8mil is JUST larger than that) or 0.15mm (4mil is

    >> even below THAT). 4mil is a very nice width for paper printouts, but NOT

    >> for the silkscreen.

     

    Exactly. 0.2 mm (or 8 mil) are good measures.

     

    >>> 3.The ADD command in the board editor searches through the description

    >>> field, so a well setup description field can yield more fruitful

    >>> searches. Therefore a good description field for a package should include:

    >>> Standard package name(preferably in bold)

    >>> Any possible aliases for the package. For example a DIL08 package might

    >>> also be known as a DIP08.

    >>

    >> Yes.

     

    Yes.

     

    >>> If the package is based off of a standard document such as one of the

    >>> IPC standards, then it should be referenced in the description field if

    >>> possible as an HTML link. If a link is not possible then a reference to

    >>> the name of the document should be sufficient. Listing this information

    >>> will help in checking the package for correctness.

    >>> If applicable length x width dimension.

    >>

    >> For web-based documents, that's OK. It gets harder for LOCAL references:

     

    Even for web based documents, that won't work satisfying. Document URLs

    change, some disappear completely. So it's always necessary to include a

    reference in human readable text form, i.e. "IPC-xxxx, Section X.Y, case

    ABCD"). As a PCB CAD tool, EAGLE should not require dealing with the

    validity of web links...

     

    Right. Companies are sold or bought and so the search goes astray.

    >>> 1.Always set a prefix, otherwise EAGLE will use U$ by default.

    >>> 2.When creating multi-gated components, EAGLE will by default reference

    >>> them as G$1, G$2, etc. These names will not show up on the schematic,

    >>> therefore use the NAME command to rename the gates A, B, C, etc. A nice

    >>> way to do this is to type 'A' followed by enter when you have the gate

    >>> on your mouse cursor before placing it, EAGLE will then continue the

    >>> pattern for the other gates.

    >>> 3.Use P for power symbols.

    >>> 4.When naming devices use specific part numbers.

    >>> 5.Always double check add levels and swap levels, otherwise your

    >>> components might not enter your schematic as you'd expect them to.

    >>> Recommendations for Devices

    >>> 1.Just like packages, having a good description field can improve the

    >>> chances of the ADD command finding the component you want. A good

    >>> description field for a device should include:

    >>> Device name(preferably in bold).

    >>> Any other aliases the device might be recognized by.

    >>> A link or reference to the device's data sheet.

    >>> Manufacturer(s).

    >>> Short explanation of the device's function.

    >>> If applicable length x width dimension.

    >>

    >> Yes to all of the above.

     

    ...except to 4.

    Correct that to: Use generic devices wherever possible.

     

    that would be better

     

    If you use specific part numbers, you'll end up with zillions of

    identical devices, just with different names (i.e. TL072, MC1458, LM358,

    TLC272, TLV272, etc. pp.).

     

    For this particular example, I have one device for a dual opamp in

    standard pinout, with the common package variants (DIP, SO, etc.). After

    having placed it in a schematic, I simply set its VALUE to the correct one.

     

    The same applies to all parts with standard packages and pinouts: many

    transistors, thyristors and TRIACs, comparators, voltage regulators etc.

    Only those that don't share a standard pinout need their own devices.

     

    (The same rule can be applied to more complex parts as well, i.e.

    microcontrollers with different features or memory sizes, but the same

    symbol and pinout. They need only one device - with a properly set value.)

     

    Tilmann

     

    Wih a few exceptions that seems OK image

     

    It is OT here, but labels should have their own size-(ratio)-parameter.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag