Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) Is it possible?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 188 subscribers
  • Views 712 views
  • Users 0 members are here
Related

Is it possible?

e14 Contributor
e14 Contributor over 14 years ago

Good Evening Everyone,

 

I drew a simple schematic with standard LM317T power supply, a 20-pin encoder chip and a 5 pin Receiver chip. I admit I used the auto route feature (trying to save time) and converted it to a board as usual. I went ahead and made my pcb only to find that the routing was completed incorrectly!

One of the nets went directly from one pin on the encoder to one pin on the Receiver chip. I rechecked by schematic. The board should connect these two pins, but instead it goes to a completely different pin on the Rx. Also, my schematic shows clearly that pin #2 should have no connection made to it at all, but there is a connecting net to pin #2, while pin #3 is left unconnected on the board. I have checked and there are no jumper wires I am over looking. It seems to me that the program V5.11.0 just didn't convert it correctly. Is this possible.

Thanks,

 

Jeff

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Jeff Morrissey schrieb:

     

    I drew a simple schematic with standard LM317T power supply, a 20-pin

    encoder chip and a 5 pin Receiver chip. I admit I used the auto route

    feature (trying to save time) and converted it to a board as usual. I

    went ahead and made my pcb only to find that the routing was

    completed incorrectly! One of the nets went directly from one pin on

    the encoder to one pin on the Receiver chip. I rechecked by

    schematic. The board should connect these two pins, but instead it

    goes to a completely different pin on the Rx. Also, my schematic

    shows clearly that pin #2 should have no connection made to it at

    all, but there is a connecting net to pin #2, while pin #3 is left

    unconnected on the board. I have checked and there are no jumper

    wires I am over looking. It seems to me that the program V5.11.0 just

    didn't convert it correctly. Is this possible.

     

    I don't think so.

     

    Most probably the device definitions are simply wrong (Rx mirrored?).

     

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago

    Jeff Morrissey schrieb:

     

    I drew a simple schematic with standard LM317T power supply, a 20-pin

    encoder chip and a 5 pin Receiver chip. I admit I used the auto route

    feature (trying to save time) and converted it to a board as usual. I

    went ahead and made my pcb only to find that the routing was

    completed incorrectly! One of the nets went directly from one pin on

    the encoder to one pin on the Receiver chip. I rechecked by

    schematic. The board should connect these two pins, but instead it

    goes to a completely different pin on the Rx. Also, my schematic

    shows clearly that pin #2 should have no connection made to it at

    all, but there is a connecting net to pin #2, while pin #3 is left

    unconnected on the board. I have checked and there are no jumper

    wires I am over looking. It seems to me that the program V5.11.0 just

    didn't convert it correctly. Is this possible.

     

    I don't think so.

     

    Most probably the device definitions are simply wrong (Rx mirrored?).

     

    Tilmann