Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) Have Board revision track the Schematic revision
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 189 subscribers
  • Views 1727 views
  • Users 0 members are here
Related

Have Board revision track the Schematic revision

e14 Contributor
e14 Contributor over 14 years ago

It was expressed that having the board revision match the schematic revision

was a manual task often forgotten. Hence the board revision 'text' did not

match the schematic revision (text).

Project attributes were suggested as a solution.

 

The desired functionality  can be achieved currently using the attributes

features, as they are.

In use you change an attribute value in the schematic and it is

automatically corrected on the board. image

 

The method:

1) By default the frame(device)  you place around the schematic consists

only of a symbol. To this you should add a package which consists of the

fixed text to be printed on the board, followed by a text variable that

matches the name of an attribute we will assign latter  e.g. REV >REVISION

2) In the frame symbol used for the device add the text variable >REVISION

into the data area of the frame

3) In the Device editor create an attribute named REVISION, value 0.0,

variable, all.

 

To update the revision text in the Frame data area and on the board all that

is required is to change the value of the REVISION attribute of the frame

(select frame origin, lower left corner usually)

 

This technique revealed to me a feature of frames. Performing a "Library

update all", in the schematic editor, does not update the frame. Further

investigation required to see if this is documented behaviour.

I had to delete the current frame and re-add the frame.

 

HTH

Warren

 

 

 

--

Viewed / responded via the newsgroup at

news.cadsoft.de

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Warren Brayshaw wrote:

     

     

    This technique revealed to me a feature of frames. Performing a

    "Library update all", in the schematic editor, does not update the

    frame. Further investigation required to see if this is documented

    behaviour.

    I had to delete the current frame and re-add the frame.

     

    Attempts to replicate this have not been successful. (v5.11.2)

    Not saving the library change could have been the problem but the update

    warns you of that so I'm at a loss to understand what was happening

    Hopefully it all goes well for you.

     

    Warren

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • amigabill
    amigabill over 14 years ago in reply to e14 Contributor

    Warren Brayshaw wrote:

    Attempts to replicate this have not been successful. (v5.11.2)

     

    Where does one get 5.11.2? I have 5.11.0, now can only find 6.x on website.

     

    Bill

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to amigabill

    Bill Toner wrote:

    Warren Brayshaw wrote:

    >> Attempts to replicate this have not been successful. (v5.11.2)

     

    Where does one get 5.11.2? I have 5.11.0, now can only find 6.x on

    website.

     

    Bill

     

     

    5.11.2 has now become 5.12

    find it here

    ftp://ftp.cadsoft.de/eagle/program/

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to amigabill

    Bill Toner wrote:

    Warren Brayshaw wrote:

    >> Attempts to replicate this have not been successful. (v5.11.2)

     

    Where does one get 5.11.2? I have 5.11.0, now can only find 6.x on

    website.

     

    Bill

     

     

    5.11.2 has now become 5.12

    find it here

    ftp://ftp.cadsoft.de/eagle/program/

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de