Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) First Schematic - Feedback?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 190 subscribers
  • Views 1256 views
  • Users 0 members are here
Related

First Schematic - Feedback?

e14 Contributor
e14 Contributor over 14 years ago

Hello All,

      Hopefully this is the right forum for this. I just made my first schematic of and was looking to see if anyone had suggestions, corrections, etc. they would like to offer? I'm kinda new to all this (been programming on a Netduino for a while now, and gernal programming for years) and was thinking for my first project I would make a breakout board for a 8-Bit Parallel-In/Serial-Out Shift Register - 74HC165N,65274HC165N,652 from Sparkfun.com. I'm hoping to make the board and use it in a DIY Guitar Rig Controller. Anyway, I was just hoping to post a picture of my schematic and see if anyone saw any mistakes that a newbie like me might make. Any suggestions are welcome. Thanks!

 

PS>> "Pin_13", "Pin_12" & "Pin_10" refer to the pins on a Netduino the IC pins connect to

 

image


  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    On 15/02/2012 05:23, Thomas Sloan wrote:

    Hello All, Hopefully this is the right forum for this. I just made my

    first schematic of and was looking to see if anyone had suggestions,

     

    Welcome,

     

    I'd like to echo other comments, particularly Michael's, but with a

    little more explanation.

     

    SER should indeed be connected to either ground or VCC.  Even if you're

    only intending to read eight bits at a time (before re-loading the

    internal register from the A-H inputs) and won't read as far as the SER

    input, unconnected ('floating') logic inputs consume unspecified amounts

    of current and may result in generally odd behaviour propagating through

    the shift register.

     

    Each input A-H should be pulled to ground with a large resistor.  If a

    switch is open the corresponding input is left to float.  Depending on

    the characteristics of the input circuitry in the 74165, an input might

    get stuck 'HIGH' after its switch is disconnected.  This stuck condition

    may be permanent or may resolve back to 'LOW' after some charge

    dissipates.  Or you may end up with weirdness in between.

     

    100nF capacitors across chips' supplies, placed physically close to each

    chip, are always a good idea.  Google 'decoupling capacitor'.

     

    The supply pins for the 74165 aren't shown.  If these hidden supply pins

    to the 74165 are named VCC and GND (as they are in the standard

    libraries) then EAGLE will implicitly connect them to nets of the same

    name.  This will work for VCC but your ground net is called GND(T), so

    the 74165's ground connection will not be automatically made.  You may

    instead wish to use the 'GND' symbol from the supp1.lbr library.

     

    There are arguments for and against allowing EAGLE to do make implicit

    VCC and GND connections.  I prefer to avoid it because it adds

    ambiguity, particularly if you are working with many different supply

    voltages.  Instead, use the INVOKE command to obtain the second part of

    the 74165 device (The 'PWRN' gate), then connect those power pins to VCC

    and GND.  This also gives you a good place to add a decoupling capacitor

    to your schematic.

     

    Finally, just a stylistic point -- please keep supply components

    conventionally oriented.  The ground symbol should point downwards and

    the VCC symbol should point upwards.

     

    Other than that -- looks fine image

     

     

    Andrew

    0xADF

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    First off, thank you all for your responses. They are all helpful and have taught me some things I obvisouly did not know image

    I've made the corrections suggested above. I'm not sure I got the capacitor connected right, but I think I get the whole concept of "Decoupling Cap" now (draw voltage from the charged capaciter giving the power supply time to adjust for the fluction in power consumption). I did also get two new error now when I wired up the SER pin and INH pin to GND. The errors are the same which is "Only INPUT pins on GND". I think this may be something to do with EAGLE more then a error in my Schematic (from what I have been reading), but by all means please let me know if I'm mistaken. Again, thank you so much for all you help. I'm sure I'll be back with more questions!

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Hi,

     

    Firstly, +1 for Michael's advice about pull-down resistors, more info

    here: http://en.wikipedia.org/wiki/Pull-up_resistor

     

    The errors are the same which is "Only INPUT pins on GND". I

    think this may be something to do with EAGLE more then a error in my

    Schematic

     

    Ah.  Now that you have the 74165's power pins on the schematic, EAGLE no

    longer automatically connects them to GND and VCC, because it assumes

    you've INVOKEd them to connect them to something yourself (perhaps to

    connect VCC to +3V3 or something).

     

    You will need add VCC and GND connections to these pins.  EAGLE is,

    quite rightly, warning you that the only pins currently connected to GND

    are 'input' pins whereas it's normal to have at least one 'supply' pin

    on this net.

     

    EAGLE's electrical rules checker uses pin-specific information (set when

    designing a schematic symbol) to decide whether the circuit makes sense

    electrically.  If, for example, you connected QH and !QH together an

    Electrical Rules Check would warn you that two output pins are trying to

    drive the same net.

     

     

    Andrew

    0xADF

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Hi,

     

    Firstly, +1 for Michael's advice about pull-down resistors, more info

    here: http://en.wikipedia.org/wiki/Pull-up_resistor

     

    The errors are the same which is "Only INPUT pins on GND". I

    think this may be something to do with EAGLE more then a error in my

    Schematic

     

    Ah.  Now that you have the 74165's power pins on the schematic, EAGLE no

    longer automatically connects them to GND and VCC, because it assumes

    you've INVOKEd them to connect them to something yourself (perhaps to

    connect VCC to +3V3 or something).

     

    You will need add VCC and GND connections to these pins.  EAGLE is,

    quite rightly, warning you that the only pins currently connected to GND

    are 'input' pins whereas it's normal to have at least one 'supply' pin

    on this net.

     

    EAGLE's electrical rules checker uses pin-specific information (set when

    designing a schematic symbol) to decide whether the circuit makes sense

    electrically.  If, for example, you connected QH and !QH together an

    Electrical Rules Check would warn you that two output pins are trying to

    drive the same net.

     

     

    Andrew

    0xADF

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • michaelkellett
    michaelkellett over 14 years ago in reply to e14 Contributor

    Hello Thomas,

     

    I think you are OK now.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Yikes! I can't believe I totally missed the part about pulling down the pins to GND. With the Netduino, the pins have built in pull-up resistors so you could directly connect a switch to a GND pin and a input port without issue (assuming you enabled the pull-up resistor in your InterruptPort constructor). Anyways, ver3 of my shcematic (and by the way, in case you were wondering, here is the Fritzing diagram I was using as a point of refrence for building this: http://netmftoolbox.codeplex.com/wikipage?title=Toolbox.NETMF.Hardware.InputPortShift).

     

    1) Added pull-down resistors to pull the IC pins to GND when the switch is open

     

    2) INVOKED the GND and VCC pins on the IC and wired each to +3.3 and GND respecfully (Power will be comming from a Netduino at 3.3V)

     

    3) Added a decoupling capacitor connecting pins 8 and 16 on the IC (GND and VCC).

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    a liitle bit OT, but have a look at:

    http://www.williamson-labs.com/

    section Bypassing

    r