Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) output cursor location ?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 189 subscribers
  • Views 1120 views
  • Users 0 members are here
Related

output cursor location ?

e14 Contributor
e14 Contributor over 14 years ago

Hello,

 

Any way to access/output current cursor location on board editor at run

time, for example with a function key press? Interested in generating

motion control commands to an external device for inspection of boards.

 

Thanks,

Bill

 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Bill Martin wrote:

    Hello,

     

    Any way to access/output current cursor location on board editor at

    run time, for example with a function key press? Interested in

    generating motion control commands to an external device for

    inspection of boards.

     

    Thanks,

    Bill

     

    Not easily, but possible.

     

    I used the following technique.

    I wrote a ULP which was run using a function key that was assigned to that

    ULP. The process was, position the cursor and hit the Function key and I

    attained the cursor position.

     

    The secret lies in (@) which is the current mouse  position See HELP /

    Editor Commands / Command Syntax

    But you cannot simply read the cursor position within a ULP. You have to use

    it. I drew a line from the cursor position to a far distant point  on a

    custom layer that had an obscure name.

    The ULP exited and immediatly re-ran itself with a specific argument this

    time to indicate re-entry. Satisfied it was a re-entry it looked for the

    custom layer name and for a  line with one end at the known location. The

    other end of the line was recovered as this was the cursor co-ords. You have

    to write code to clean up the line on the custom layer each time you

    initially enter the ULP

     

    I hope a future subversion of V6  has cursor position obtainable from within

    the ULP.

     

    HTH

    Warren

     

     

     

     

     

     

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    On 04/27/2012 12:37 AM, Warren Brayshaw wrote:

    Bill Martin wrote:

    >> Hello,

    >>

    >> Any way to access/output current cursor location on board editor at

    >> run time, for example with a function key press? Interested in

    >> generating motion control commands to an external device for

    >> inspection of boards.

    >>

    >> Thanks,

    >> Bill

     

    Not easily, but possible.

     

    I used the following technique.

    I wrote a ULP which was run using a function key that was assigned to that

    ULP. The process was, position the cursor and hit the Function key and I

    attained the cursor position.

     

    The secret lies in (@) which is the current mouse  position See HELP /

    Editor Commands / Command Syntax

    But you cannot simply read the cursor position within a ULP. You have to use

    it. I drew a line from the cursor position to a far distant point  on a

    custom layer that had an obscure name.

    The ULP exited and immediatly re-ran itself with a specific argument this

    time to indicate re-entry. Satisfied it was a re-entry it looked for the

    custom layer name and for a  line with one end at the known location. The

    other end of the line was recovered as this was the cursor co-ords. You have

    to write code to clean up the line on the custom layer each time you

    initially enter the ULP

     

    I hope a future subversion of V6  has cursor position obtainable from within

    the ULP.

     

    HTH

    Warren

     

    >

    Thanks for that pointer. I tried what seemed the obvious way to

    circumvent the "not available in ULP" issue, with the following:

    ASSIGN F12 'RUN chk_args.ulp (@)'

    however, the (@) is not expanded and passed as an argv[] parameter as

    would be desired. So it looks like your method may be the only way to do

    this. Actually, until/if Eagle can pass coordinates to a ulp, I might do

    better to look at using gerbv to emit coordinates, there I can alter the

    source code if needed...

     

    Regards,

    Bill

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Thanks for that pointer. I tried what seemed the obvious way to

    circumvent the "not available in ULP" issue, with the following:

    ASSIGN F12 'RUN chk_args.ulp (@)'

    however, the (@) is not expanded and passed as an argv[] parameter as

    would be desired. So it looks like your method may be the only way to do

    this. Actually, until/if Eagle can pass coordinates to a ulp, I might do

    better to look at using gerbv to emit coordinates, there I can alter the

    source code if needed...

     

    Regards,

    Bill

     

    Hi Bill

    you don't get away to re-write gerbv that easily.

     

    Have a play with the attached ULP. It may have value for you.

    Place it on your ULP paths and read the description/guidance from Eagle

    Control Panel

     

    Regards

    Warren

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to dukepro

    On 05/02/2012 04:59 AM, Chuck Huber wrote:

    On 05/01/2012 06:43 PM, Bill Martin wrote:

    >> My idea is basically to construct an X-Y gantry with a USB microscope

    >> mounted on the moving stage,

    ...

    >> I'm toying with the idea of also mounting an IR

    >> laser on the gantry stage to see if I can do some no-touch soldering of

    >> smt parts.

     

    This is interesting... You'd have ramp the current up such that you

    don't induce a thermal shock on the part.  Do you have an IR laser in

    mind powerful enough to reach the melting point of solder?

     

         - Chuck

     

    Not sure how much power is needed for such a small area. The IR rework

    stations I have seen use hundreds of watts over a large area. I have

    seen a 1W blue laser burn holes in plastic panels, but that is likely

    different from a shiny metal surface. Reflection of energy could make

    the whole idea go "flop". It's really not something I know anything much

    about, perhaps that's why it is interesting. There are other obvious

    limitations as well, for example it is not going to solder down too many

    BGA parts...and inner layers of multi-layer pcbs can't really be seen

    with the scope either. So, it only fits the case of assembling the kind

    of pcbs that one might try in a non-commercial setting.

     

    -bill

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to dukepro

    On 05/02/2012 04:59 AM, Chuck Huber wrote:

    On 05/01/2012 06:43 PM, Bill Martin wrote:

    >> My idea is basically to construct an X-Y gantry with a USB microscope

    >> mounted on the moving stage,

    ...

    >> I'm toying with the idea of also mounting an IR

    >> laser on the gantry stage to see if I can do some no-touch soldering of

    >> smt parts.

     

    This is interesting... You'd have ramp the current up such that you

    don't induce a thermal shock on the part.  Do you have an IR laser in

    mind powerful enough to reach the melting point of solder?

     

         - Chuck

     

    Not sure how much power is needed for such a small area. The IR rework

    stations I have seen use hundreds of watts over a large area. I have

    seen a 1W blue laser burn holes in plastic panels, but that is likely

    different from a shiny metal surface. Reflection of energy could make

    the whole idea go "flop". It's really not something I know anything much

    about, perhaps that's why it is interesting. There are other obvious

    limitations as well, for example it is not going to solder down too many

    BGA parts...and inner layers of multi-layer pcbs can't really be seen

    with the scope either. So, it only fits the case of assembling the kind

    of pcbs that one might try in a non-commercial setting.

     

    -bill