Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) BRD and SCH not consistence ???
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 188 subscribers
  • Views 353 views
  • Users 0 members are here
Related

BRD and SCH not consistence ???

e14 Contributor
e14 Contributor over 14 years ago

I have made some smaller changes to a schematic that allready was made into

a board.

 

I've added

 

1) a "3-jumper" (male) for power -18V, GND and +18V

2) two solder points, GND_IN and GND_OUT

 

The ERC-errors reports them as consistency-errors (not found in the board)

and of cause they are, but

 

How do I add them to the board too ?

--

Best regards

KSor, Denmark

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    On 07.05.2012 16:08, Keld Sørensen wrote:

    I have made some smaller changes to a schematic that allready was made into

    a board.

     

    I've added

     

    1) a "3-jumper" (male) for power -18V, GND and +18V

    2) two solder points, GND_IN and GND_OUT

     

    The ERC-errors reports them as consistency-errors (not found in the board)

    and of cause they are, but

     

    How do I add them to the board too ?

     

    Normally EAGLE adds them autopmatically as soon as you place them

    in the schematic. But therfore both files have to be consistent

    (which means Back/Froward Annotation is running) and both files must

    be loaded simultaneously.

     

    Now it is too late. There are two options:

    Delete the parts in the schematic again, run ERC and when it is

    consistent  ADD the parts again, or add the packages in the layout,

    connect them with SIGNAl and name the nets as it is in schematic.

    ERC helps you in detecting the differences until it is conistent

    again.

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/