Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) Where do I find SOIC packages?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 188 subscribers
  • Views 2403 views
  • Users 0 members are here
Related

Where do I find SOIC packages?

Plecto
Plecto over 14 years ago

Hi. I'm having a problem finding SOIC packages. The body is 7.5mm wide and pin spacings are 1.27mm. I see people saying I can find it in 75xx library, but I'm having no luck. I also see people telling me to look in "ref-packages.lbr" but I have no idea on where to find that.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    On 7/18/2012 7:34 AM, Tor-Arne Forsmo wrote:

    Hi. I'm having a problem finding SOIC packages. The body is 7.5mm wide and pin spacings are 1.27mm. I see people saying I can find it in 75xx library, but I'm having no luck. I also see people telling me to look in "ref-packages.lbr" but I have no idea on where to find that.

     

     

    Some things to check...

     

    1.  In the Eagle control panel go to Options->Directories and make sure

    the path for Libraries is set correctly.   By default it will be

    "$EAGLEDIR\lbr"

     

    2. In the Eagle control panel tree view right click on Libraries the

    then "Use All".    Expand the Libraries node and make sure that all the

    listed lbrs (there will be a lot) are shown with a green circle next to

    the library name.

     

    3. Go to your schematic and Add a part.   When the Add dialog pops up

    you can enter a wildcard search expression in the lower left corner.

    Try searching for SO.

     

    You should also be able to access ref-packages.lbr from the control

    panel and view its contents.   I see a lot of stuff with the SO in the

    description so maybe one of those will be right for your part or at

    least a good starting point to create your own.

     

    Jim