Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) EAGLE FEATURE SURVEY
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 25 replies
  • Subscribers 192 subscribers
  • Views 2574 views
  • Users 0 members are here
Related

EAGLE FEATURE SURVEY

Jorge_Garcia
Jorge_Garcia over 13 years ago

Hello fellow EAGLE users,

 

I've made a simple GoogleDocs Form as a type of survey and I would like to gather as much feedback as possible. The survey has only one question: What features would you like to see in future versions of EAGLE? Simply select the radio button of the feature you'd like to see, type in a few comments if you so desire and hit the submit button. That's it.

 

Here's the link for the form:

 

http://docs.google.com/spreadsheet/viewform?formkey=dEF4MWdPVXgxNjdHMk9aWE5wOTNyQmc6MQ

 

If you have any questions or concerns, feel free to reply to this thread.

 

Thanks in advance for your participation.

 

Best Regards,

Jorge Garcia

Cadsoft Support

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    Quote:

    User Interface Improvements

     

    Like what?  Actually not changing things has great value here.  I've gotten

    used to how things are, so I don't want to have to re-learn some other way.

    I've also got my user interface highly customized with hot buttons,

    scripts, and ULPs.  Don't mess it up.  The easiest way to guarantee that is

    don't mess with it at all.

     

    Quote:

    3D Visualization

     

    That would require all kinds of 3D information in each part, which I don't

    see adding.  I can possibly see value to checking the mechanical fit of a

    board as part of a larger project, but this sounds like huge work, both for

    you and for me, and there are plenty of more valuable and easier to do

    things on the list.

     

    Quote:

    Pad Stack

     

    I can see the point to it, but I haven't personally run into a case where I

    would have needed more than Eagle provides now.  Probably a reasonable

    feature to have, but not high on my priority list.

     

    Quote:

    Schematic Hierarchy and Design Modularity

     

    Yes, definitely!  Designs are inherently hierarchical things, at least

    large ones.  You think of susbsystems, communicate the design that way,

    document it that way, but in Eagle it all has to be flat.  This is not all

    about documentation either (although that is important), but being able to

    re-use subsystems accross designs would be very useful.

     

    Quote:

    Simulation Facilities

     

    Not Eagle's job.  Move along.  Let's not waste time here.

     

    While simulation can be a useful tool, it is also overused and overvalued.

    Good simulation is also complex, and would require entering a lot more part

    information than there is now.  This sounds like a huge job just for me to

    make use of, let alone for you to implement.  Stick to things that I can't

    get externally to Eagle, since there are plenty of those.

     

    Quote:

    More Import/Export Formats IDF, DXF, Netlists from other programs, etc.

     

    I can see the point to this in some environments, but it wouldn't do much

    for me personally.  However, I don't see this working well.  How is

    something imported from Altium going to adhere to my part and BOM

    conventions in Eagle?  It could be useful if it really worked reliably, but

    more likely it will get to the 80% level and stall, which would still be

    largely useless.

     

    Quote:

    Auto Placement

     

    LOL

     

    I really hope you don't seriously think you can do that, and that anything

    you cooked up would actually be useful!!?

     

    Quote:

    Multi-core or GPU support

     

    Yes.  The Eagle autorouter is one of the few things I run nowadays that is

    CPU limited and takes a significant amount of time in human terms.  The

    rest of Eagle is fast enough that there is no need for more speed, but I

    want all the speed I can get from the autorouter.  I want the autorouter to

    make full use of whatever computer I am running it on.

     

    Quote:

    Other

     

    There have been many suggestions here over time.  Take a look.

     

    My #1 feature request is to allow for more flexible package definitions

    without massive DRC errors.  This has been discussed at length before, so

    no need for more now except to re-iterate this is the most importance

    enhancement on my list.

     

    Quote:

    ODB++ Export

     

    Huh?

     

    Quote:

    Electrical Planning(Residential Electrical Plans, Electrician oriented

     

    applications)

     

    Not Eagle's job.  You've got lots of features that Eagle needs that would

    help people get things done that they bought Eagle for.  It would really

    piss me off if you strayed to do these side things while there are so many

    important enhancements left to do.

     

    Quote:

    EAGLE for Tablet or Smartphones

     

    Oh yes, and it should have voice prompts too, and automatic posts to

    twitter so I can tell the world I just added a 10k resistor to a schematic!

    And while you're at it, make it work with the cloud.  Nobody knows what

    the "cloud" really is but it sounds cool.  I'm sure the customers would

    love to hear their data is out in the cloud somewhere where somebody can

    get at it somehow.  To be complete, this must come with a proper shirt,

    cool designer glasses, and special overpriced shoes.  You can't do trendy

    and cool half-assed.  Don't listen to all the nay-sayers who point out you

    can't actually do anything useful on a smart phone with a schematic.  Of

    course you can't, but that's obvious so it's clearly not the point.  It's

    about being cool and trendy.  Hey, I get paid by the hour, so I'm still

    making money when I'm talking into a smart phone getting nothing

    accomplished.

     

    Quote:

    Autorouter improvements, push and shove, shape based, etc.

     

    I can't say as you haven't defined "push", "shove", and "shape based"

    (duh).

     

    Quote:

    Simplified Library Management, speedier part creation, etc.

     

    Only on the smartphone and tablet version.  Since it's all for show, you

    can skip all the fluff for making parts.  All those pin thingies get so

    tedius, especially when you're busy tweeting about the resistor you just

    added, someplace, it doesn't really matter, 10k Ohms can go lots of

    places.

     

    Back on my PC, quality is what counts.  I can't think of what exactly you'd

    do to speed up part creation.  When you have repetitive things to do, you

    use scripts anyway.  As for one-offs, what would you leave out?  This

    sounds like nice on the outside, but I don't see how you're really going to

    make it work with all the necessary details on the inside.  All in all,

    part creation isn't that difficult as it is now, and I make all my own

    parts.

     

    Quote:

    Cloud Interface

     

    Lol.  You guys are actually serious!!?

     

    Quote:

    Version Control

     

    Already available externally, so spend your time on something more core

    that I can't get externally.

     

    Quote:

    Visual Difference Tool (Visually see differences between two boards)

     

    I can see the point to it, but not much value for me personally.

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Am 06.09.2012 17:22, schrieb Olin Lathrop:

    >> User Interface Improvements

     

    Like what?  Actually not changing things has great value here.  I've gotten

    used to how things are, so I don't want to have to re-learn some other way.

      I've also got my user interface highly customized with hot buttons,

    scripts, and ULPs.  Don't mess it up.  The easiest way to guarantee that is

    don't mess with it at all.

     

    There are TWO kinds of user interface improvements:

      1. Completely changing a useful interface to make it more trendy or

         something like it. This obviously is rubbish. See Microsoft

         'fluent' interfaces, which for the professional are anything BUT

         fluent.

      2. Using the available interface and improve things so that NEW

         users can UNDERSTAND the functions more quickly and REMEMBER them

         easier, but WITHOUT breaking the workflow of the 'professionals'.

         Here, EAGLE can be improved LOTS - see my EAGLE GUI posts in

         eagle.suggest.eng...

         (Or would you NOT like to SEE the symbol before adding it to the

         device in the device editor? The usage of the dialog would be

         COMPLETELY the same as it is now, only a symbol preview would be

         added)

     

    Andreas Weidner

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Andreas Weidner wrote on Fri, 07 September 2012 07:46

    (Or would you NOT like to SEE the symbol before adding it to the

    device in the device editor? The usage of the dialog would be

    COMPLETELY the same as it is now, only a symbol preview would be

    added)

     

    Usually there is no question as to which symbol I want to add because I

    probably just created it.  A preview does no harm as long as it doesn't

    change the current command flow and shortcut keys.  Right now, adding a

    symbol to a package is very easy, type Alt-E A.  That gives you a list of

    symbols in the library.  Now you use up and down arrows to select the right

    one, then ENTER to confirm.  This works fine.  There is no problem to

    solve.

     

    I am worried that a preview would make this process more complicated or

    bloated.  Right now each symbol uses up one line.  That's nice since a lot

    of them can fit onto the screen.  If they took up more space due a preview,

    then it would make the process more tedius.

     

    Perhaps in rare cases there might be confusion between different symbols,

    but this is the exception case I wouldn't want to have Eagle optimized for

    at the expense of the normal case where you can easily see which symbol you

    want.

     

    Maybe you need to be more careful about giving symbols useful names?

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Andreas Weidner wrote on Fri, 07 September 2012 07:46

    (Or would you NOT like to SEE the symbol before adding it to the

    device in the device editor? The usage of the dialog would be

    COMPLETELY the same as it is now, only a symbol preview would be

    added)

     

    Usually there is no question as to which symbol I want to add because I

    probably just created it.  A preview does no harm as long as it doesn't

    change the current command flow and shortcut keys.  Right now, adding a

    symbol to a package is very easy, type Alt-E A.  That gives you a list of

    symbols in the library.  Now you use up and down arrows to select the right

    one, then ENTER to confirm.  This works fine.  There is no problem to

    solve.

     

    I am worried that a preview would make this process more complicated or

    bloated.  Right now each symbol uses up one line.  That's nice since a lot

    of them can fit onto the screen.  If they took up more space due a preview,

    then it would make the process more tedius.

     

    Perhaps in rare cases there might be confusion between different symbols,

    but this is the exception case I wouldn't want to have Eagle optimized for

    at the expense of the normal case where you can easily see which symbol you

    want.

     

    Maybe you need to be more careful about giving symbols useful names?

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Am 07.09.2012 14:40, schrieb Olin Lathrop:

    Maybe you need to be more careful about giving symbols useful names?

     

    Yes. BUT:

      1. Since some of my libraries are 18 years old, and you COULD not

         give symbols useful names then (8 character limit), there is a

         lot of historical rubbish still around. And with, e.g., a

         nearly unlimited supply of OP symbols - with/without compensation,

         with/without offset, with/without shutdown, one/two/three

         output pins etc. - naming them with 8 characters IS a trifle

         difficult. And renaming ALL my symbols created in 18 years is

         QUITE a lot of work...

      2. I often do not want to reinvent the wheel, so want to search

         for a symbol that already looks NEARLY as needed, copy it and

         patch it accordingly. Saves LOTS of time. A preview would be

         GORGEOUS. OK, this would not be in the ADD dialog, but somewhere

         else, but still previews are nice.

      3. And obviously, the previews would behave as everywhere else

         in EAGLE, and NOT break the workflow. NO preview broke the

         workflow so far, so trust CadSoft not to screw everything up.

     

    Andreas Weidner