Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) EAGLE FEATURE SURVEY
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 25 replies
  • Subscribers 192 subscribers
  • Views 2574 views
  • Users 0 members are here
Related

EAGLE FEATURE SURVEY

Jorge_Garcia
Jorge_Garcia over 13 years ago

Hello fellow EAGLE users,

 

I've made a simple GoogleDocs Form as a type of survey and I would like to gather as much feedback as possible. The survey has only one question: What features would you like to see in future versions of EAGLE? Simply select the radio button of the feature you'd like to see, type in a few comments if you so desire and hit the submit button. That's it.

 

Here's the link for the form:

 

http://docs.google.com/spreadsheet/viewform?formkey=dEF4MWdPVXgxNjdHMk9aWE5wOTNyQmc6MQ

 

If you have any questions or concerns, feel free to reply to this thread.

 

Thanks in advance for your participation.

 

Best Regards,

Jorge Garcia

Cadsoft Support

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    On 8/23/2012 6:38 PM, Jorge_Garcia wrote:

    Hello fellow EAGLE users,

     

    I've made a simple GoogleDocs Form as a type of survey and I would like to gather as much feedback as possible. The survey has only one question: What features would you like to see in future versions of EAGLE? Simply select the radio button of the feature you'd like to see, type in a few comments if you so desire and hit the submit button. That's it.

     

    Here's the link for the form:

     

    http://docs.google.com/spreadsheet/viewform?formkey=dEF4MWdPVXgxNjdHMk9aWE5wOTNyQmc6MQ

     

    If you have any questions or concerns, feel free to reply to this thread.

     

    Thanks in advance for your participation.

     

    Best Regards,

    Jorge Garcia

    Cadsoft Support

     

    Thanks to everyone who has participated. I'm going to let the survey

    ride this week and then call it done. If you haven't filled out the

    survey this is the last week to do so.

     

    Thank you all for all of your input.

     

    Best Regards,

    Jorge Garcia

    Cadsoft Support

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dukepro
    dukepro over 13 years ago in reply to e14 Contributor

    On 10/15/2012 06:08 PM, Jorge Garcia wrote:

     

    Thanks to everyone who has participated. I'm going to let the survey

    ride this week and then call it done. If you haven't filled out the

    survey this is the last week to do so.

     

    Thank you all for all of your input.

     

    Jorge,

     

    Here's something that has just hounded me in the past.  I would like the

    ability to add some text (or a circle or such) to the board and have it

    associated with a component so that when the component is moved, the

    associated text moves with it.  Alternatively or additionally, I would

    like the ability to add text to a library package, and be able to smash

    the package in the board and move the text (or circle) around in the

    same manner that I can now smash and move >NAME and >VALUE.  The

    motivation for this is to better document the layout for the assembly

    house.  For example, I'd like to place the numeral 1 outside and close

    to pin 1 of an IC, and be able to move it slightly in the layout editor

    so as not to interfere with nearby components.

     

    Thanks,

        - Chuck

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to dukepro

    My top requests. I submitted only the first via the form... but here are the others, since I don't want to double-post:

     

    #1 Request - SPEED!

     

    • Problem: on a complex 300mm x 300mm panel, CAM processing of the gerbers takes around 15 minutes on an 8-core 3.6ghz machine. This makes the design process very slow when making revisions based on Gerber outputs
    • Suggested Solution: Parallel processing for the CAM processor.
    • Comment: From a programmer's perspective, this should be relatively painless, since the different CAM sections are not interdependant - they can be run in parallel without seriously changing the algortihm, eg. spawn new processes/threads for each section (*or even each aperature*!), then join back once all tasks complete. Currently, we have to open a few copies of Eagle.exe at the same time and run the CAM sections in parallel ourselves!

     

    #2 Request - LIBRARY ENHACEMENT

     

    • Problem:Loss of sync on library items if devices are renamed
    • Suggested Solution: After a update library command, detect if parts are missing in currently linked libraries, and prompt to "relink missing devices"
    • Comment: There is currently no solution to this problem, not even a ULP

     

    #3 Request - ADVANCED COPY/PASTE SCHEMATIC *WITH* BOARD LAYOUT

     

    • Problem: Copying and pasting schematic with the board layout requires too much manual intervention (opening/closing/renaming brd and sch files). The current best methods are prone to user error.
    • Suggested Solution: A new option to group copy/paste BOTH schematic+board layout at the same time, with a selectable option to "create new net names to make the copy completely independant" (such that no air-wires exist)
    • Comment: This would be incredibly useful for many of us trying to copy sections of existing designs for re-use. Currently, we have to disable forward/back annotation, then fix errors later. Sometimes, mistakes creep their way into our designs as a result, even if board consistency is re-achieved.

     

    That's it... I know it's a lot of stuff, but I have faith in the Eagle development team!

     

    Hope this makes it!

     

    PS I forget to mention, for #1, parallel processing in other areas, such as ratsnest would be AMAZING as well. eg. Each layer's ratsnest should be calculated in parallel. Currently, this can take up to 30 seconds on a complex 300mm x 300mm design, making the routing process very slow.

     

    Message was edited by: B Mac

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to dukepro

    My top requests. I submitted only the first via the form... but here are the others, since I don't want to double-post:

     

    #1 Request - SPEED!

     

    • Problem: on a complex 300mm x 300mm panel, CAM processing of the gerbers takes around 15 minutes on an 8-core 3.6ghz machine. This makes the design process very slow when making revisions based on Gerber outputs
    • Suggested Solution: Parallel processing for the CAM processor.
    • Comment: From a programmer's perspective, this should be relatively painless, since the different CAM sections are not interdependant - they can be run in parallel without seriously changing the algortihm, eg. spawn new processes/threads for each section (*or even each aperature*!), then join back once all tasks complete. Currently, we have to open a few copies of Eagle.exe at the same time and run the CAM sections in parallel ourselves!

     

    #2 Request - LIBRARY ENHACEMENT

     

    • Problem:Loss of sync on library items if devices are renamed
    • Suggested Solution: After a update library command, detect if parts are missing in currently linked libraries, and prompt to "relink missing devices"
    • Comment: There is currently no solution to this problem, not even a ULP

     

    #3 Request - ADVANCED COPY/PASTE SCHEMATIC *WITH* BOARD LAYOUT

     

    • Problem: Copying and pasting schematic with the board layout requires too much manual intervention (opening/closing/renaming brd and sch files). The current best methods are prone to user error.
    • Suggested Solution: A new option to group copy/paste BOTH schematic+board layout at the same time, with a selectable option to "create new net names to make the copy completely independant" (such that no air-wires exist)
    • Comment: This would be incredibly useful for many of us trying to copy sections of existing designs for re-use. Currently, we have to disable forward/back annotation, then fix errors later. Sometimes, mistakes creep their way into our designs as a result, even if board consistency is re-achieved.

     

    That's it... I know it's a lot of stuff, but I have faith in the Eagle development team!

     

    Hope this makes it!

     

    PS I forget to mention, for #1, parallel processing in other areas, such as ratsnest would be AMAZING as well. eg. Each layer's ratsnest should be calculated in parallel. Currently, this can take up to 30 seconds on a complex 300mm x 300mm design, making the routing process very slow.

     

    Message was edited by: B Mac