Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) EAGLE FEATURE SURVEY
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 25 replies
  • Subscribers 182 subscribers
  • Views 1888 views
  • Users 0 members are here
Related

EAGLE FEATURE SURVEY

Jorge_Garcia
Jorge_Garcia over 13 years ago

Hello fellow EAGLE users,

 

I've made a simple GoogleDocs Form as a type of survey and I would like to gather as much feedback as possible. The survey has only one question: What features would you like to see in future versions of EAGLE? Simply select the radio button of the feature you'd like to see, type in a few comments if you so desire and hit the submit button. That's it.

 

Here's the link for the form:

 

http://docs.google.com/spreadsheet/viewform?formkey=dEF4MWdPVXgxNjdHMk9aWE5wOTNyQmc6MQ

 

If you have any questions or concerns, feel free to reply to this thread.

 

Thanks in advance for your participation.

 

Best Regards,

Jorge Garcia

Cadsoft Support

  • Sign in to reply
  • Cancel
  • Former Member
    Former Member over 13 years ago in reply to Former Member

    Hi Guys,

     

    I explained earlier but it looks that the message didn't make it to the

    forum.

     

    I know some of the entries in the survey may seem ridiculous, however

    they have been requested by some users and that's why I included them.

    If they really are as useless as we think they are then that will be

    reflected in the low number of votes for those features.

     

    Market research is a pain and this is my first go at it. We will

    continue to do surveys in the future and with better methods to collect

    the feedback.

     

    In the meanwhile I appreciate all of the feedback you guys can give and

    if you can pass the survey on to colleagues.

     

    Thanks,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 13 years ago in reply to Former Member

    Am 06.09.2012 17:22, schrieb Olin Lathrop:

    >> User Interface Improvements

     

    Like what?  Actually not changing things has great value here.  I've gotten

    used to how things are, so I don't want to have to re-learn some other way.

      I've also got my user interface highly customized with hot buttons,

    scripts, and ULPs.  Don't mess it up.  The easiest way to guarantee that is

    don't mess with it at all.

     

    There are TWO kinds of user interface improvements:

      1. Completely changing a useful interface to make it more trendy or

         something like it. This obviously is rubbish. See Microsoft

         'fluent' interfaces, which for the professional are anything BUT

         fluent.

      2. Using the available interface and improve things so that NEW

         users can UNDERSTAND the functions more quickly and REMEMBER them

         easier, but WITHOUT breaking the workflow of the 'professionals'.

         Here, EAGLE can be improved LOTS - see my EAGLE GUI posts in

         eagle.suggest.eng...

         (Or would you NOT like to SEE the symbol before adding it to the

         device in the device editor? The usage of the dialog would be

         COMPLETELY the same as it is now, only a symbol preview would be

         added)

     

    Andreas Weidner

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 13 years ago in reply to Former Member

    Andreas Weidner wrote on Fri, 07 September 2012 07:46

    (Or would you NOT like to SEE the symbol before adding it to the

    device in the device editor? The usage of the dialog would be

    COMPLETELY the same as it is now, only a symbol preview would be

    added)

     

    Usually there is no question as to which symbol I want to add because I

    probably just created it.  A preview does no harm as long as it doesn't

    change the current command flow and shortcut keys.  Right now, adding a

    symbol to a package is very easy, type Alt-E A.  That gives you a list of

    symbols in the library.  Now you use up and down arrows to select the right

    one, then ENTER to confirm.  This works fine.  There is no problem to

    solve.

     

    I am worried that a preview would make this process more complicated or

    bloated.  Right now each symbol uses up one line.  That's nice since a lot

    of them can fit onto the screen.  If they took up more space due a preview,

    then it would make the process more tedius.

     

    Perhaps in rare cases there might be confusion between different symbols,

    but this is the exception case I wouldn't want to have Eagle optimized for

    at the expense of the normal case where you can easily see which symbol you

    want.

     

    Maybe you need to be more careful about giving symbols useful names?

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • sqkybeaver
    sqkybeaver over 13 years ago

    i am somewhere between version controle and a tabblett app to at least view shc and brd files.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 13 years ago

    On 23/08/2012 23:38, Jorge_Garcia wrote:

    Hello fellow EAGLE users,

     

    I've made a simple GoogleDocs Form as a type of survey and I would like to gather as much feedback as possible. The survey has only one question: What features would you like to see in future versions of EAGLE? Simply select the radio button of the feature you'd like to see, type in a few comments if you so desire and hit the submit button. That's it.

     

    Here's the link for the form:

     

    http://docs.google.com/spreadsheet/viewform?formkey=dEF4MWdPVXgxNjdHMk9aWE5wOTNyQmc6MQ

     

    If you have any questions or concerns, feel free to reply to this thread.

     

    Thanks in advance for your participation.

     

    Best Regards,

    Jorge Garcia

    Cadsoft Support

     

     

    First on a Mac using Safari I can only choose one button. Not really a

    problem because the biggest problem for me, by far, is the auto-router.

    Other things may be awkward but I can get round or by them. The auto

    router works OK on two layer boards with through hole components. On

    surface mount multilayer boards it is almost useless. It will sometimes

    not use a layer at all.

     

    For many circuits there are benefits to hand routing, especially as the

    frequency goes up, but for hundreds of I/O ports on a relatively slow

    micro-controller, hand routing is tedious and difficult in the extreme.

     

    Someone mentioned this would need a lot of code. I think they are

    missing the point. What the auto-router needs is a good algorithm that

    treats layers as equals when routing. Most people have computers with

    multiple fast cores. There is potential for a giant leap in router

    performance.

     

          Andrew

     

    PS as a benefit it would not require practically any interface changes

    so those steeped in the program would have no problems.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 13 years ago in reply to Former Member

    On 9/7/2012 12:02 PM, Andrew Forrest wrote:

    First on a Mac using Safari I can only choose one button. Not really a

    problem because the biggest problem for me, by far, is the auto-router.

    Other things may be awkward but I can get round or by them. The auto

    router works OK on two layer boards with through hole components. On

    surface mount multilayer boards it is almost useless. It will sometimes

    not use a layer at all.

     

    For many circuits there are benefits to hand routing, especially as the

    frequency goes up, but for hundreds of I/O ports on a relatively slow

    micro-controller, hand routing is tedious and difficult in the extreme.

     

    Someone mentioned this would need a lot of code. I think they are

    missing the point. What the auto-router needs is a good algorithm that

    treats layers as equals when routing. Most people have computers with

    multiple fast cores. There is potential for a giant leap in router

    performance.

     

          Andrew

     

    PS as a benefit it would not require practically any interface changes

    so those steeped in the program would have no problems.

     

    Hi Andrew,

     

    I hope you're doing well. There's a couple of things that can be done to

    guide the AUTOROUTER to do what you want to do. For example a common

    task that people like to automate is via drops to a ground or power

    plane. The general idea is that you route a short distance from the SMD

    pad and then drop a via to the power layer.

     

    The autorouter can do that for you without issue here's the setup:

     

    1. In the command line type AUTO GND VCC ... and press enter. Since you

    only want to drop to the power planes only those signals should be

    routed by specifying them before hand the autorouter will only route

    those nets.

    2. In the route and bus tabs set the maximum number of vias value to

    9999. This tells EAGLE to use as many vias as necessary to route the

    net, if you use the defaults that's when you see EAGLE start routing

    between components instead of dropping straight down.

    3. Disable the optimize runs, the purpose of the optimize runs is to

    minimize the number of vias which is not what you want for this application.

     

    If you run it with those parameters you'll find that it does a pretty

    good job of dropping straight to your power planes.

     

    This is not to take away from the suggestion, my purpose here is just to

    allow you to make better use of what's available now.

     

    hth,

    Jorge Garcia

    Cadsoft Support

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 13 years ago in reply to Former Member

    Am 07.09.2012 14:40, schrieb Olin Lathrop:

    Maybe you need to be more careful about giving symbols useful names?

     

    Yes. BUT:

      1. Since some of my libraries are 18 years old, and you COULD not

         give symbols useful names then (8 character limit), there is a

         lot of historical rubbish still around. And with, e.g., a

         nearly unlimited supply of OP symbols - with/without compensation,

         with/without offset, with/without shutdown, one/two/three

         output pins etc. - naming them with 8 characters IS a trifle

         difficult. And renaming ALL my symbols created in 18 years is

         QUITE a lot of work...

      2. I often do not want to reinvent the wheel, so want to search

         for a symbol that already looks NEARLY as needed, copy it and

         patch it accordingly. Saves LOTS of time. A preview would be

         GORGEOUS. OK, this would not be in the ADD dialog, but somewhere

         else, but still previews are nice.

      3. And obviously, the previews would behave as everywhere else

         in EAGLE, and NOT break the workflow. NO preview broke the

         workflow so far, so trust CadSoft not to screw everything up.

     

    Andreas Weidner

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jorge_Garcia
    Jorge_Garcia over 13 years ago

    I need a few more responses, I'm almost at the two hundred response mark. If I could get that I would be satisfied with the survey and start processing the info.

     

    Come one EAGLE community show me some love, end my marketing pain image

     

    Best Regards,

     

    Jorge Garcia

    Cadsoft Support

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 13 years ago in reply to Jorge_Garcia

    I've use a fair few CAD packages. EAGLE has limitations, but I keep coming back to it, because for what it is, it is powerful and, importantly, fast to use. I absolutely love the autorouting features on other platforms, but EAGLE is feature rich in other ways.

     

    One of the greatest benefits to EAGLE is that it is speedy to use - I can very quickly put together a circuit (admittedly the autorouter is slow). However, what takes up most of the time? Parts creation. Honestly, who is happy using pre-created symbols? I wouldn't trust anyones symbols. I create my own for maybe 50-60% of components, to be sure they are the way I want them.

    Here are some suggestions for speeding up parts creation:

    1. Have some profiles for common shapes (SIL, DIL, 4-sided) and allow the user to pick a pad or SMD, and enter in sufficient dimensions until EAGLE decides it can calculate all remaining dimensions. Datasheets tend to represent measurements in a few different methods, so it would need some intelligence. Some datasheets don't show the landing pattern, but they show the device pins. For that scenario, the profiles should allow the user to enter device pin dimensioning, and then later select pad size, and then allow it to automatically center them under the device pins or to have an offset from center. This is simple stuff, but requires users to perform mental arithmetic for a minute or two (and then double-check!) per device. It all adds up. Save my time and EAGLE becomes so much more valuable (time is everyones most expensive resource).

     

    Ability to have vias even in SMD pads - this is electrically essential in some RF designs.

    Abilty to have some nice 'snaps' like Powerpoint 2010, which can automatically centre objects to other objects - this is way more advanced than simple grid snap which never meets anyones needed. I want to be able to automatically center drill holes or board connectors to align with others on the board. If need be, allow the user to

    place some temporary sketch lines for alignment if you can't implement the Powerpoint 2010 method.

     

    The measurement method is dire (I know someone else mentioned that above too). I don't want to change grid size just to perform an accurate measurement. It should automatically snap to the edge and center of pads and to the center and edges of drill holes.

     

    Does the latest version of EAGLE support shaped pads? If so, then great. It is needed for modern parts.

     

    Incorporate some new features in the PCB design, such as a layer that allows you to 'draw' lines of small holes for perforating boards so they can be snapped apart. Have more than 16 colours.

    Automatically place text '>NAME' and '>VALUE' as soon as I click to create a package or symbol, and save me 30 seconds of my time - this is really obvious stuff and saves time (I can then move the text to where I want it).

     

    Ignore the person criticizing cloud and tablets - it's just a matter of time. Implement that right, and all of a sudden you don't need to maintain multiple builds for Linux, Windows and Mac, and people can work on the move, and you make more revenue.

     

    The scripting is incredible - one of the best features (if not THE best feature) of EAGLE. Keep that up for all new features!

     

    I'd also like to see some better vector fonts with curves! - we have powerful PCs, and we don't need to be restricted to such simplistic fonts. That could be a task for a student to implement, if you purchase the rights to some nice fonts. But it should support more than just 127 characters, and should allow underline and overline.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 13 years ago in reply to shabaz

    Am 2012-10-10 00:07, schrieb shabaz:

    I've use a fair few CAD packages. EAGLE has limitations, but I keep coming back to it, because for what it is, it is powerful and, importantly, fast to use. I absolutely love the autorouting features on other platforms, but EAGLE is feature rich in other ways.

     

    One of the greatest benefits to EAGLE is that it is speedy to use - I can very quickly put together a circuit (admittedly the autorouter is slow). However, what takes up most of the time? Parts creation. Honestly, who is happy using pre-created symbols? I wouldn't trust anyones symbols. I create my own for maybe 50-60% of components, to be sure they are the way I want them.

    Here are some suggestions for speeding up parts creation:

    1. Have some profiles for common shapes (SIL, DIL, 4-sided) and allow the user to pick a pad or SMD, and enter in sufficient dimensions until EAGLE decides it can calculate all remaining dimensions. Datasheets tend to represent measurements in a few different methods, so it would need some intelligence. Some datasheets don't show the landing pattern, but they show the device pins. For that scenario, the profiles should allow the user to enter device pin dimensioning, and then later select pad size, and then allow it to automatically center them under the device pins or to have an offset from center. This is simple stuff, but requires users to perform mental arithmetic for a minute or two (and then double-check!) per device. It all adds up. Save my time and EAGLE becomes so much more valuable (time is everyones most expensive resource).

     

    Ability to have vias even in SMD pads - this is electrically essential in some RF designs.

    Abilty to have some nice 'snaps' like Powerpoint 2010, which can automatically centre objects to other objects - this is way more advanced than simple grid snap which never meets anyones needed. I want to be able to automatically center drill holes or board connectors to align with others on the board. If need be, allow the user to

    place some temporary sketch lines for alignment if you can't implement the Powerpoint 2010 method.

     

    The measurement method is dire (I know someone else mentioned that above too). I don't want to change grid size just to perform an accurate measurement. It should automatically snap to the edge and center of pads and to the center and edges of drill holes.

     

    Does the latest version of EAGLE support shaped pads? If so, then great. It is needed for modern parts.

     

    Incorporate some new features in the PCB design, such as a layer that allows you to 'draw' lines of small holes for perforating boards so they can be snapped apart. Have more than 16 colours.

    Automatically place text '>NAME' and '>VALUE' as soon as I click to create a package or symbol, and save me 30 seconds of my time - this is really obvious stuff and saves time (I can then move the text to where I want it).

     

    Ignore the person criticizing cloud and tablets - it's just a matter of time. Implement that right, and all of a sudden you don't need to maintain multiple builds for Linux, Windows and Mac, and people can work on the move, and you make more revenue.

     

    The scripting is incredible - one of the best features (if not THE best feature) of EAGLE. Keep that up for all new features!

     

    I'd also like to see some better vector fonts with curves! - we have powerful PCs, and we don't need to be restricted to such simplistic fonts. That could be a task for a student to implement, if you purchase the rights to some nice fonts. But it should support more than just 127 characters, and should allow underline and overline.

     

    I support all those points with shaped pads and the library editor

    features giving highest value for me too.

     

    Also the limited colour palette hurts often.

     

    Regards, Stefan

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>