EAGLE User Chat (English) Eagle 6.4 and shortcut keys
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
  • Replies 5 replies
  • Subscribers 179 subscribers
  • Views 936 views
  • Users 0 members are here
Related

Eagle 6.4 and shortcut keys

Former Member
Former Member over 13 years ago

Hi,

I'm having a problem with setting up all the shortcuts that i need to use. In previous versions that was not a problem but since 6.4... come on! why do the keys that are once changed always return to their original configuration? Is there a system to set this up? I tried using eagle editing the eaglerc.usr file but nothing works. I've seen somewhere that there is a way to run eagle 6.4 with old config file. Is that the only way? I don't have the old config file since I upgraded to 6.4. PLEASE someone help.

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    Former Member over 13 years ago

    Am 17.01.2013 07:24, schrieb Przemyslaw Zur:

    Hi,

    I'm having a problem with setting up all the shortcuts that i need to use. In previous versions that was not a problem but since 6.4... come on! why do the keys that are once changed always return to their original configuration? Is there a system to set this up? I tried using eagle editing the eaglerc.usr file but nothing works. I've seen somewhere that there is a way to run eagle 6.4 with old config file. Is that the only way? I don't have the old config file since I upgraded to 6.4. PLEASE someone help.

     

     

    Fact is that new assignments are 1. not saved and 2. not all of them are

    shown.

    In my eaglerc I see that F10 is set as "redo". If I'm at the board

    opening the options/keys dialog I don't see F10 at all.

    If I want to set F10 key to "redo" I get a message that the key is

    already assigned as "redo", so why it is not shown?

    If I assign it new it shows up in the list until the list is closed.

    After reopening the dialog the key does not show but still works.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 13 years ago

    Am 17.01.2013 07:24, schrieb Przemyslaw Zur:

    Hi,

    I'm having a problem with setting up all the shortcuts that i need to use. In previous versions that was not a problem but since 6.4... come on! why do the keys that are once changed always return to their original configuration? Is there a system to set this up? I tried using eagle editing the eaglerc.usr file but nothing works. I've seen somewhere that there is a way to run eagle 6.4 with old config file. Is that the only way? I don't have the old config file since I upgraded to 6.4. PLEASE someone help.

     

     

    Fact is that new assignments are 1. not saved and 2. not all of them are

    shown.

    In my eaglerc I see that F10 is set as "redo". If I'm at the board

    opening the options/keys dialog I don't see F10 at all.

    If I want to set F10 key to "redo" I get a message that the key is

    already assigned as "redo", so why it is not shown?

    If I assign it new it shows up in the list until the list is closed.

    After reopening the dialog the key does not show but still works.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Former Member
    Former Member over 13 years ago in reply to Former Member

    Come on! this is starting to *$@# me off! I'm working on a important project right now and every time I open a schematic or board file the assignments are gone. Fix this!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 13 years ago in reply to Former Member

    On 1/17/2013 5:30 AM, Przemyslaw Zur wrote:

    Come on! this is starting to *$@# me off! I'm working on a important project right now and every time I open a schematic or board file the assignments are gone. Fix this!

     

     

    Hi Przemyslaw,

     

    I think the best way to setup your assignments now is to use the

    eagle.scr file. If you make the assignments there and save the eagle.scr

    file then your shortcut keys should be preserved. In 6.4.0 it comes with

    some defaults you can easily modify.

     

    You'll find the eagle.scr file in the scripts tree of the control panel.

     

    hth,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 13 years ago in reply to Former Member

    Jorge Garcia wrote on Thu, 17 January 2013 12:44

    On 1/17/2013 5:30 AM, Przemyslaw Zur wrote:

    Come on! this is starting to *$@# me off! I'm working on a

    important project right now and every time I open a schematic or board

    file the assignments are gone. Fix this!

     

     

    Hi Przemyslaw,

     

    I think the best way to setup your assignments now is to use the

    eagle.scr file. If you make the assignments there and save the

    eagle.scr

    file then your shortcut keys should be preserved. In 6.4.0 it comes

    with

    some defaults you can easily modify.

     

    You'll find the eagle.scr file in the scripts tree of the control

    panel.

     

     

    But don't edit the eagle.scr file in the install directory--it will be

    removed or overwritten when you update to the next version.  See our app

    note EAN-02 at http://www.eaglecentral.ca/eagle/application-notes for the

    same issue discussed in a larger context for libraries, ULP's, scripts,

    etc...

     

    Cheers,

     

    James.

    --

    James Morrison  ~~~  Stratford Digital

     

    Specializing in CadSoft EAGLE

    • Online Sales to North America

    • Electronic Design Services

    • EAGLE Enterprise Toolkit

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 13 years ago in reply to Former Member

    Thank's I'll try that.

    Is this a bug that is in this version or am I the only one with this problem.

    I edited the eagle.scr file added some key assignments on the schematic... I'll try them later out and let You know.

    If this is a bug please fix it. The default keys cant overwrite the changed ones in the program. What's the use of setting them up in the first place.

     

    Best regards