Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) Errant plus sign
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 188 subscribers
  • Views 652 views
  • Users 0 members are here
Related

Errant plus sign

e14 Contributor
e14 Contributor over 13 years ago

I'm using Eagle Light. When I place text or a component on the schematic, a plus sign shows up with it. I assume its a postion marker. For example, if I place text such as "-15 V", it shows up as " +-15 V". Is there a way to turn off the plus sign?

 

Thanks,

 

Steve

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    In the schematic you can prevent the display of the 'Part' origin and the

    'Text' origin

     

    Option.ShowPartOrigins

    The origins of parts in a schematic are indicated by small crosses. Set

    this parameter to '0' to turn this off.

     

    Option.ShowTextOrigins

    The origins of texts are indicated by small crosses. Set this parameter to

    '0' to turn this off.

     

    e.g. Type into the command line

    set Option.ShowTextOrigins 0

     

    See HELP SET

     

    HTH

    Warren

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago

    Op Sun, 03 Mar 2013 17:39:11 +0100 schreef Steve Magoon 

    <noreply-167654@element14.com>:

     

    I'm using Eagle Light. When I place text or a component on the 

    schematic, a plus sign shows up with it. I assume its a postion marker. 

    For example, if I place text such as "-15 V", it shows up as " +-15 

    V". Is there a way to turn off the plus sign?

     

    Thanks,

     

    Steve

     

    --

     

    Hello Steve,

     

    Yes there is: turn off the layers tOrigins and/or bOrigins, depending on 

    where your components are placed. After that you've lost the possibility 

    to move any component, you will need to turn the layer(s) on for that. 

    Keep that in mind.

     

     

    Richard