Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) Cadsoft Eagle with Python Scripting
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 54 replies
  • Subscribers 191 subscribers
  • Views 12206 views
  • Users 0 members are here
Related

Cadsoft Eagle with Python Scripting

e14 Contributor
e14 Contributor over 13 years ago

Hi,

 

I've only started using Eagle a few weeks ago, and as much as I like it, I have found what I consider some pretty fundamental features just missing. As the built in scripting language is extremely restrictive (when compared to a 'real' language like python, lua or ruby), I made an attempt to get python running with Eagle.

 

http://www.youtube.com/watch?v=_w7CECR7Dv8

 

The above is a video of a project I have been working on for the pas 3-4 days, which basically involves exposing the Cadsoft ULP and SCR to python (albeit in not the fastest way). But it does allow me to now use 90% of the ULP and all of the SCR directly from python, including the Object Heirarchies, board.grid... schematic... which have all be exposed in a pythonic way.

 

as an example, to get all the Instances in the schematic..

 

instances = Eaglepy.ULSchematic().instances()

 

or loop,

 

for instance in Eaglepy.ULSchematic().instances():

     print instance.name()

 

etc..

 

The tools in the video were very quick to knock out.. the slowest bit was figuring out the papers for approximating cubic/quadratic bezier curves with arcs, for the DXF Importer. These should be the first of many tools to come, next on the list is a group manager so I can save my selectsion.

 

Hopefully when I have had time to test this a bit more I will release the code to the community, along with any tools I have built. for others who might want this funtionality. (something that should be out of the box with proper bindings to a proper language imo...)

 

Cheers

 

Rob.

  • Sign in to reply
  • Cancel
Parents
  • rick_b
    rick_b over 9 years ago

    Does anyone know if this works with eagle 7.7?

     

    Rick

    --

    EAGLE support forums at http://www.eaglecentral.ca :: Where the EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to rick_b

    rickb wrote on Fri, 17 February 2017 14:43

    Does anyone know if this works with eagle 7.7?

     

    Do you mean the Python scripting?  I've mainly used it with version 5 and

    6.  I'll try to test it with version 7 this weekend...

    --

    EAGLE support forums at http://www.eaglecentral.ca :: Where the EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rick_b
    rick_b over 9 years ago in reply to autodeskguest

    Quote:

    Do you mean the Python scripting?

     

     

    Yes, thanks.

     

    Rick

    --

    EAGLE support forums at http://www.eaglecentral.ca :: Where the EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rick_b
    rick_b over 9 years ago in reply to autodeskguest

    Quote:

    Do you mean the Python scripting?

     

     

    Yes, thanks.

     

    Rick

    --

    EAGLE support forums at http://www.eaglecentral.ca :: Where the EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    Dietmar Schwertberger wrote on Wed, 22 February 2017 13:36

    For things like graphics, hardware interfacing, file formats,

    networking, GUIs etc. I found that development at the interpreter console

    provides the biggest boost in productivity.

     

    Yes!  It's quite fun to use pyqt from the ipython prompt to interactively

    show and hide or manipulate various parts of my GUI.

     

    You can do similar things with various JVM languages that have REPLs.  For

    example, here's some Scala typed into the Ammonite REPL to create a popup

    window with a single button:

     

     

    @ {

      import javax.swing._, java.awt.event._

      val frame = new JFrame("Hello World Window")

     

      val button = new JButton("Click Me")

      button.addActionListener(new ActionListener{

        def actionPerformed(e: ActionEvent) = button.setText("You clicked the

    button!")

      })

      button.setPreferredSize(new java.awt.Dimension(200, 100))

      frame.getContentPane.add(button)

      frame.pack()

      frame.setVisible(true)

     

      }

     

     

    --

    EAGLE support forums at http://www.eaglecentral.ca :: Where the EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    Dietmar Schwertberger wrote on Wed, 22 February 2017 13:16

    Put your core C++ code into a .pyd (i.e. actually a DLL).  Still you

    can control your code from Python, offering a scripting interface without

    much effort.

     

    Yes, I use Python for the GUI and scripting, and the C++ is for the

    rendering and math functions (using a GPU).

     

    Quote:

    The wx license is not GPL. It is LGPL, but even allows to distribute

    binaries on your own terms. So basically, it's not much different from

    MIT, BSD or similar licenses for any practical application.

     

    That is very nice.

     

    Quote:

    (Python is) also a great language to implement large applications,

    either GUI or web based.

     

    Yes, I agree.  At my "real" job during the day, I use Python and QT for

    large applications every day.

     

     

    Quote:

    If you go for wx, you should have a look at the current wxGlade version

    from the repository.

     

    I will definitely look at that.  Thank you...

     

    Quote:

    I think there are quite powerful reverse engineering tools for compiled

    binaries.

     

    I have no illusions that a determined person would not be able to reverse

    engineer my work.  If they wish to go through that effort, that is up to

    them, but since I either give my tools away for free or charge a very small

    amount of money, I hope it is not worth their trouble.

     

    --

    EAGLE support forums at http://www.eaglecentral.ca :: Where the EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    On 22.02.2017 21:08, Doug Wellington wrote:

    FWIW, the Java ecosystem is fantastic.  The build, test, code analysis,

    continuous integration, etc., tools are great!

    For things like graphics, hardware interfacing, file formats,

    networking, GUIs etc. I found that development at the interpreter

    console provides the biggest boost in productivity.

    The only comparable language that I know, is Forth. But that one is

    a bit too special for most people...

     

    Regards,

     

    Dietmar

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    On 22.02.2017 21:08, Doug Wellington wrote:

    FWIW, the Java ecosystem is fantastic.  The build, test, code analysis,

    continuous integration, etc., tools are great!

    For things like graphics, hardware interfacing, file formats,

    networking, GUIs etc. I found that development at the interpreter

    console provides the biggest boost in productivity.

    The only comparable language that I know, is Forth. But that one is

    a bit too special for most people...

     

    Regards,

     

    Dietmar

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    On 22.02.2017 20:55, Doug Wellington wrote:

    Dietmar Schwertberger wrote on Wed, 22 February 2017 12:32

    Thanks, part of my issue is that I was also writing in C++ and I didn' > want to have to release that source code.  It's my code, I wrote it

    and I> want to keep it private.  Over the years I have grown weary of people

    Put your core C++ code into a .pyd (i.e. actually a DLL).

    Still you can control your code from Python, offering a scripting

    interface without much effort.

     

     

    contacting me demanding my source code, my schematic and board files, and

    my gerbers.  It's hard to make your investment back when someone can grab

    your work and match or beat your time to market and undermine your pricing.

    Anything with GPL licensing is out for me because of that

    The wx license is not GPL. It is LGPL, but even allows to distribute

    binaries on your own terms. So basically, it's not much different from

    MIT, BSD or similar licenses for any practical application.

     

     

    For scripting, rapid prototyping and as a language to use for teaching,

    Python is fantastic.

    It's also a great language to implement large applications, either GUI

    or web based. Implementing GUIs in C++ seems to be a huge waste of

    resources. The learning curve for GUIs is a bit steep, just as for C++.

    For this reason I started improving the wxGlade GUI builder last year.

    If you go for wx, you should have a look at the current wxGlade version

    from the repository.

    (Documentation update is work in progress and not yet online.)

     

     

    Because of it being interpreted though, there is no

    way to effectively control your IP.

    Well, there are ways, but these are a bit complicated. I have one

    application where I'm using a dongle for Python code and .pyd extensions.

    But protection of the Python code requires a custom Python runtime.

    For extension of other people's code, that's probably not an option.

    On the other hand, don't forget that Python bytecode might be easier

    to decompile, but it's also possible for C++ code. I think there are

    quite powerful reverse engineering tools for compiled binaries.

     

     

    Regards,

     

    Dietmar

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    Also, switching to the Java world lets me use Groovy, Scala, Clojure, and

    even Jython or JRuby all together...

     

    FWIW, the Java ecosystem is fantastic.  The build, test, code analysis,

    continuous integration, etc., tools are great!

    --

    EAGLE support forums at http://www.eaglecentral.ca :: Where the EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    Also, switching to the Java world lets me use Groovy, Scala, Clojure, and

    even Jython or JRuby all together...

     

    FWIW, the Java ecosystem is fantastic.  The build, test, code analysis,

    continuous integration, etc., tools are great!

    --

    EAGLE support forums at http://www.eaglecentral.ca :: Where the EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    Dietmar Schwertberger wrote on Wed, 22 February 2017 12:32

    For a more liberal license, you should have considered wxPython

    instead.

     

    Thanks, part of my issue is that I was also writing in C++ and I didn't

    want to have to release that source code.  It's my code, I wrote it and I

    want to keep it private.  Over the years I have grown weary of people

    contacting me demanding my source code, my schematic and board files, and

    my gerbers.  It's hard to make your investment back when someone can grab

    your work and match or beat your time to market and undermine your pricing.

    Anything with GPL licensing is out for me because of that

     

    Quote:

    Python seems a much more natural choice for these tasks than Java.

     

    For scripting, rapid prototyping and as a language to use for teaching,

    Python is fantastic.  Because of it being interpreted though, there is no

    way to effectively control your IP.

     

    --

    EAGLE support forums at http://www.eaglecentral.ca :: Where the EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    Dietmar Schwertberger wrote on Wed, 22 February 2017 12:32

    For a more liberal license, you should have considered wxPython

    instead.

     

    Thanks, part of my issue is that I was also writing in C++ and I didn't

    want to have to release that source code.  It's my code, I wrote it and I

    want to keep it private.  Over the years I have grown weary of people

    contacting me demanding my source code, my schematic and board files, and

    my gerbers.  It's hard to make your investment back when someone can grab

    your work and match or beat your time to market and undermine your pricing.

    Anything with GPL licensing is out for me because of that

     

    Quote:

    Python seems a much more natural choice for these tasks than Java.

     

    For scripting, rapid prototyping and as a language to use for teaching,

    Python is fantastic.  Because of it being interpreted though, there is no

    way to effectively control your IP.

     

    --

    EAGLE support forums at http://www.eaglecentral.ca :: Where the EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to autodeskguest

    On 21.02.2017 19:17, Doug Wellington wrote:

    I considered using PyQt for the GUI, but the licensing didn't work for me, so

    at that point, I switched to using Java.

    For a more liberal license, you should have considered wxPython instead.

    Python seems a much more natural choice for these tasks than Java.

    Also, it would allow for easier integration if you really want to

    migrate to KiCad. The PCB part of KiCad has a Python console already.

    I would expect the Schematic part to follow sooner or later.

     

    Regards,

     

    Dietmar