Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) Cadsoft Eagle with Python Scripting
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 54 replies
  • Subscribers 192 subscribers
  • Views 12062 views
  • Users 0 members are here
Related

Cadsoft Eagle with Python Scripting

e14 Contributor
e14 Contributor over 13 years ago

Hi,

 

I've only started using Eagle a few weeks ago, and as much as I like it, I have found what I consider some pretty fundamental features just missing. As the built in scripting language is extremely restrictive (when compared to a 'real' language like python, lua or ruby), I made an attempt to get python running with Eagle.

 

http://www.youtube.com/watch?v=_w7CECR7Dv8

 

The above is a video of a project I have been working on for the pas 3-4 days, which basically involves exposing the Cadsoft ULP and SCR to python (albeit in not the fastest way). But it does allow me to now use 90% of the ULP and all of the SCR directly from python, including the Object Heirarchies, board.grid... schematic... which have all be exposed in a pythonic way.

 

as an example, to get all the Instances in the schematic..

 

instances = Eaglepy.ULSchematic().instances()

 

or loop,

 

for instance in Eaglepy.ULSchematic().instances():

     print instance.name()

 

etc..

 

The tools in the video were very quick to knock out.. the slowest bit was figuring out the papers for approximating cubic/quadratic bezier curves with arcs, for the DXF Importer. These should be the first of many tools to come, next on the list is a group manager so I can save my selectsion.

 

Hopefully when I have had time to test this a bit more I will release the code to the community, along with any tools I have built. for others who might want this funtionality. (something that should be out of the box with proper bindings to a proper language imo...)

 

Cheers

 

Rob.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 12 years ago

    Excellent work!

     

    I've been trying to import eagle schematics into Python now that they in XML format.

     

    So far I have a script that can import and return iterable objects for layers and parts.

    segments can be itstill need some work

    libraries are broken.

     

    If this is at all helpful, you can find it here:

    https://github.com/uid89626/Eagle

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 12 years ago

    Excellent work!

     

    I've been trying to import eagle schematics into Python now that they in XML format.

     

    So far I have a script that can import and return iterable objects for layers and parts.

    segments can be itstill need some work

    libraries are broken.

     

    If this is at all helpful, you can find it here:

    https://github.com/uid89626/Eagle

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • autodeskguest
    autodeskguest over 12 years ago in reply to e14 Contributor

    That's great foxx00!

     

    Here are a couple quick tools I wrote to explore EAGLE files.  The first is

    a short Python script that just displays the top few node levels.  Save it

    to an executable file (add a shebang if you need it) and put the EAGLE file

    name on the command line:

     

    import sys

    import xml.etree.ElementTree as ET

     

    if len(sys.argv)  - read EAGLE XML file" % sys.argv[0]

      sys.exit()

     

    input_file = sys.argv[1]

    try:

      input_string = open(input_file).read()

    except:

      print "Couldn't read %s..." % input_file

      sys.exit()

     

    try:

      tree = ET.fromstring(input_string)

    except:

      print "Couldn't parse file, is this an EAGLE 6 document?"

      sys.exit()

     

    print "%s consists of:" % input_file

    for child in tree:

      print child.tag

      for grandchild in child:

        print "  ", grandchild.tag

        if grandchild.tag == "schematic" or grandchild.tag == "board":

          for greatgrandchild in grandchild:

            print "    ",  greatgrandchild.tag

     

    I've been playing around with functional programming lately, so the second

    is a quick Scala (Scala is rapidly becoming my favorite language!) script

    that gives you node sequences for each of the main file sections, along

    with a couple examples of iterating through them (the filename is

    hard-coded in this one at the moment, sorry):

     

    import xml.XML

     

    val fileName  = "test.brd"

    val eagleFile = XML.loadFile(fileName)

     

    // search for drawing node, then for each child node

    // length is zero if not found (e.g. you won't find a

    // schematic in a board file...).  Comment out as

    // desired to speed things up.

    val settings  = eagleFile \ "drawing" \ "settings"

    val grid      = eagleFile \ "drawing" \ "grid"

    val layers    = eagleFile \ "drawing" \ "layers"

    val board     = eagleFile \ "drawing" \ "board"

    val schematic = eagleFile \ "drawing" \ "schematic"

     

    print("\n\nUsing xpath to search for layers:\n\n")

    for (l <- layers \ "layer" ) println(l)

    println

     

    val allLayers = (layers
    "layer")

    print("\n\nNow iterating through layers in a loop:\n\n")

    allLayers.foreach{ l =>

      val layerNumber = (l \ "@number").text

      val name = (l \ "@name").text

      val visible = (l \ "@visible").text

      println(s"Layer $layerNumber, $name, is visible: $visible")

    }

     

    I've been using XML Copy Editor and Firstobject XML Editor to display and

    edit the files...

     

    Regards,

    Doug

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.