EAGLE User Chat (English) problem with connector, 2 pins/2 pads
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
  • Replies 2 replies
  • Subscribers 178 subscribers
  • Views 218 views
  • Users 0 members are here
Related

problem with connector, 2 pins/2 pads

autodeskguest
autodeskguest over 17 years ago

Hello,

 

I tried to create a new "cage clamp connector" (symbol/package etc) that has

2 pads (A1 and B1) but only 1 pin - well, I learned from other discussions

that this is not going to work, so I added a second pin. I have now the pins

(-1) and (B-1).

 

I've been looking for a similar already existing device and used the Wago

233-102 as template.

 

When I (in schematics editor) connect a net to the pin (-1) and run "erc",

it always complains that Pin B-1 is not connected - this does not happen

with the Wago clamp, there, one pin is connected and everything is fine.

 

I guess I'm missing something and would appreciate any help,

(I'm running eagle 4.16r2)

 

thanks

Matthias

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

    M.Dehof wrote:

    Hello,

     

    I tried to create a new "cage clamp connector" (symbol/package etc)

    that has 2 pads (A1 and B1) but only 1 pin - well, I learned from

    other discussions that this is not going to work, so I added a second

    pin. I have now the pins (-1) and (B-1).

     

    I've been looking for a similar already existing device and used the

    Wago 233-102 as template.

     

    When I (in schematics editor) connect a net to the pin (-1) and run

    "erc", it always complains that Pin B-1 is not connected - this does

    not happen with the Wago clamp, there, one pin is connected and

    everything is fine.

     

    I guess I'm missing something and would appreciate any help,

    (I'm running eagle 4.16r2)

     

    thanks

    Matthias

     

    This is not all that complicated, so there is probably something simple

    that's wrong.

     

    When I get this kind of 2-pin/2-pad situation, I simply put two separate

    pins in separate locations on the schematic symbol.  Then I connect both

    those pins to the same net in the schematic.

     

    It is possible to place two pins in the symbol on top of each other.  This

    "fakes" a single pin, but makes rather a mess, and I don't think it's a very

    good idea since it hides information you might need.

     

    You might also check whether your pins and your schematic nets are on-grid.

    Try moving the part and see if all the nets you think are connected stretch

    to move with it.

     

    --

    Bert Menkveld

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago

    M.Dehof wrote:

    Hello,

     

    I tried to create a new "cage clamp connector" (symbol/package etc)

    that has 2 pads (A1 and B1) but only 1 pin - well, I learned from

    other discussions that this is not going to work, so I added a second

    pin. I have now the pins (-1) and (B-1).

     

    I've been looking for a similar already existing device and used the

    Wago 233-102 as template.

     

    When I (in schematics editor) connect a net to the pin (-1) and run

    "erc", it always complains that Pin B-1 is not connected - this does

    not happen with the Wago clamp, there, one pin is connected and

    everything is fine.

     

    I guess I'm missing something and would appreciate any help,

    (I'm running eagle 4.16r2)

     

    thanks

    Matthias

     

    This is not all that complicated, so there is probably something simple

    that's wrong.

     

    When I get this kind of 2-pin/2-pad situation, I simply put two separate

    pins in separate locations on the schematic symbol.  Then I connect both

    those pins to the same net in the schematic.

     

    It is possible to place two pins in the symbol on top of each other.  This

    "fakes" a single pin, but makes rather a mess, and I don't think it's a very

    good idea since it hides information you might need.

     

    You might also check whether your pins and your schematic nets are on-grid.

    Try moving the part and see if all the nets you think are connected stretch

    to move with it.

     

    --

    Bert Menkveld