EAGLE User Chat (English) Copy already placed parts
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
  • Replies 2 replies
  • Subscribers 180 subscribers
  • Views 376 views
  • Users 0 members are here
Related

Copy already placed parts

autodeskguest
autodeskguest over 18 years ago

I have to creat a 7 segment display with onlu 5mm LED's

Is there a way to copy already placed segments in the board, so i don't have

to place all the parts for every segment by it own.

 

So lets say i have to create A,B,C,D,E,F,G and i have already place segment

A. How do I copy segment A so i have segments B,C,D,E,F,G and the schematic

takes over the routing.

 

 

 

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 18 years ago

    You figure it Out?

    "NL2TTL" <cadsoft@ttalens.com> wrote in message

    news:forvp2$981$1@cheetah.cadsoft.de...

    I have to creat a 7 segment display with onlu 5mm LED's

    Is there a way to copy already placed segments in the board, so i don't

    have

    to place all the parts for every segment by it own.

     

    So lets say i have to create A,B,C,D,E,F,G and i have already place

    segment

    A. How do I copy segment A so i have segments B,C,D,E,F,G and the

    schematic

    takes over the routing.

     

     

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 18 years ago

    NL2TTL schrieb:

    I have to creat a 7 segment display with onlu 5mm LED's

    Is there a way to copy already placed segments in the board, so i don't have

    to place all the parts for every segment by it own.

     

    So lets say i have to create A,B,C,D,E,F,G and i have already place segment

    A. How do I copy segment A so i have segments B,C,D,E,F,G and the schematic

    takes over the routing.

     

     

     

     

    Hello,

     

    somebody recently posted this in the support newsgroup:

     

     

    Sometimes circuit boards will have duplicate sections of schematic that you

    want to layout identically.  You could do this by laying out each section

    separately, but for large or complex layouts this would be very time

    consuming.  Eagle does not have a function that allows you to directly

    duplicate your layouts, so you have to use this workaround:

     

    1. Create the schematic for the section you want to duplicate.  You can have

    additional schematic done at that time too if you like.

    2. Create the layout for that section.  You can have additional layout done

    at that time if you like.

    3. Close the layout so that you only have the schematic open.

    4. Use the window selection tool to surround the section of schematic you

    want to duplicate in the layout.

    5. Use the scissors tool to copy the selection to the buffer.

    6. Use the dropdown EDIT: PASTE to finish the copy operation.

    7. Save the schematic and close it.

    8. Open the layout. Click OK to acknowledge the warning about the schematic

    and board not being consistent. Close the schematic that opened when you

    opened the layout so that you only have the layout open.

    9. Do the same window select, scissors, paste operation on the layout.  YOU

    MUST COPY EXACTLY THE SAME ITEMS AS YOU DID IN THE SCHEMATIC.  THIS INCLUDES

    COMPONENTS AND NETS.

    10. Save the layout and open the schematic.  You should have both the

    schematic and layout open at this point.

    11. In the layout, run ERC and you'll get a long list of nets that don't

    match.  Don't worry: you only have to fix each net once.  This is usually

    only 5 or 6 nets to fix the whole list.

    12. The original section of layout will have nets named GND.  The new

    section will have them named GND1.  The original section of the schematic

    will have the nets named GND.  The new section will also have them named

    GND.  The task here is to rename the net GND1 to GND in the layout.

    13. Type "show GND1" in the command line.  This will highlight GND1.

    14. Use the name tool (R2 Icon) to change the name GND1 to GND.  If

    prompted, the rename applies to all nets.

    15. If you run ERC again, you'll find that all of the GND/GND1 errors are

    gone.  Redo this renaming process a few more times for the remaining name1

    nets and you're done.

     

    Additional note: If you don't have any airwires for the net you're trying to

    rename then you'll have to create one using the line tool and the name tool:

    Create a line.  Rename that line using the R2 tool to the net name you need

    to rename (e.g. GND1).  This will connect the line to the pad that was

    previously un-airwired.  Now you can rename the airwire or line to the right

    name (e.g. GND) to fix that net.

     

     

    HTH

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

    CadSoft Support -- hotline@cadsoft.de

    FAQ: http://www.cadsoft.de/faq.htm