EAGLE User Chat (English) How to make wire turns at 45� instead of 90 with autoroute?
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
  • Replies 2 replies
  • Subscribers 180 subscribers
  • Views 317 views
  • Users 0 members are here
Related

How to make wire turns at 45� instead of 90 with autoroute?

autodeskguest
autodeskguest over 18 years ago

 

I have read that is not a good practice to let wires to turn at 90º. All

wire turns must be formed with a couple of 45º turns.

How can I use autoroute to do this automatically?

 

thanks

 

 

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 18 years ago

    japdos wrote:

    I have read that is not a good practice to let wires to turn at 90º. All

    wire turns must be formed with a couple of 45º turns.

    How can I use autoroute to do this automatically?

     

    thanks

     

    What kind of clock rates are you running your system at?

     

    Unless you are running at very high clock rates (>>100MHz), or

    require very tight impedance control on your traces, then 45º

    is not necessary, and 90º will do just fine.

     

    There are some situations where bending traces at 45º helps

    route around obstacles but odd angles are hard for autorouters

    to deal with.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 18 years ago

    japdos schrieb:

    I have read that is not a good practice to let wires to turn at 90º. All

    wire turns must be formed with a couple of 45º turns.

    How can I use autoroute to do this automatically?

     

    thanks

     

    You could try to alter cfOrthStep and cfDiagStep. They determine the

    costs of 90° turns (OrthStep) and 45° turns (DiagStep). Set for

    example DiagStep to 2 and OrthStep to 4 and try it again. The autorouter

    should (mostly) avoid 90° turns then.

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/faq.htm