EAGLE User Chat (English) Error saying "Symbol is in use" when trying to edit symbol.
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
  • Replies 1 reply
  • Subscribers 179 subscribers
  • Views 232 views
  • Users 0 members are here
Related

Error saying "Symbol is in use" when trying to edit symbol.

autodeskguest
autodeskguest over 17 years ago

Hello

 

Is there no way to edit a symbol one it is  save and used in a part?

 

I created a symbol, then a package, then made a device, saved the whole

thing.  I have an error and want to modify the symbol but it gives me errors

no matter what I try to do.

 

 

Another issue:

 

I have some pads on a library part that are x size, but when I place the

device on a schematic and board, the pads are larger and are touching each

other, when clearly they are not touching in Library mode, I have updated

the schematic and board, but the board will not reflect the real same pad

size.

 

Thanks

 

 

 

 

 

  • Sign in to reply
  • Cancel
  • Richard_H
    Richard_H over 17 years ago

    Jon galt schrieb:

    Hello

     

    Is there no way to edit a symbol one it is  save and used in a part?

     

    I created a symbol, then a package, then made a device, saved the whole

    thing.  I have an error and want to modify the symbol but it gives me errors

    no matter what I try to do.

     

     

    You may change the Symbol, for examples, pin names, the drawing itself,

    and so on, but you are not allowed to change the number of pins.

    If you want to do so, you have to delete the Symbol in the Device first.

     

     

    Another issue:

     

    I have some pads on a library part that are x size, but when I place the

    device on a schematic and board, the pads are larger and are touching each

    other, when clearly they are not touching in Library mode, I have updated

    the schematic and board, but the board will not reflect the real same pad

    size.

     

     

    See http://www.cadsoft.de/faq.htm.en#06012601

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/faq.htm