EAGLE User Chat (English) > Hello everyone ! I made a two layer pcb in which there are analog &
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
  • Replies 3 replies
  • Subscribers 178 subscribers
  • Views 336 views
  • Users 0 members are here
Related

> Hello everyone ! I made a two layer pcb in which there are analog &

autodeskguest
autodeskguest over 17 years ago

Hello everyone ! I made a two layer pcb in which there are analog &

digital ics so , I made two gnd signals naming AGND & GND . Now I want to

connect these two signals at only at the gnd pin of power connector. When

I tried to naming these signals in Eagle I can give only one name to that

net  , But don't want That ? I want separate signals.

 

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

    "Hemant" <mhamalhemant@gmail.com> wrote in message

    news:g0bftc$1hj$1@cheetah.cadsoft.de...

    Hello everyone ! I made a two layer pcb in which there are analog &

    digital ics so , I made two gnd signals naming AGND & GND . Now I

    want to connect these two signals at only at the gnd pin of power

    connector. When I tried to naming these signals in Eagle I can give

    only one name to that net  , But don't want That ? I want separate

    signals.

     

    Robert wrote:

    The net lines on your schematic represent an electrical connection

    and once you connect 2 nets together they are automatically merged

    into a single net which can only have one name. Most, if not all,

    ECAD s/w works like that.

    So, how do you solve the common problem of 2 or more ground nets that

    need to be connected together at a single point? Well, here's how I

    do it, but I'm not saying it's the best or the only solution image

     

    - on the schematic, stick to separate nets and connect only one net

    to your power pin (e.g. the GND net)

    - on the schematic add a 2-pin jumper part, connect pin 1 to GND and

    pin 2 to AGND

    - when routing the PCB, place the jumper with pin 1 as close as

    possible to your power GND pin.

    - route the entire board and run a DRC once finished, correct DRC

    errors if any until the board is OK

    - now "violate" the design rules by shorting pins 1 & 2 of the

    jumper. Be aware that this will generate a DRC clearance error, but

    simply ignore it.

    If you dont want to use the jumper principle just leave GND and AGND

    as 2 separate nets on the schematic and connect only GND to your

    power pin. When routing the PCB, add a via with net name AGND

    somewhere close to the power pin and route the AGND net, including

    the via. Again, when routed 100% and DRC errors free, "violate" the

    design rules and connect AGND also to your power pin by routing a

    trace from the via to the power pin. Alternatively, delete the via

    and connect the open AGND track simply to the power pin.

    If anybody here knows of a better or simplier way to solve this common

    problem, I too would be very happy to hear about it image

     

    Cheers,

    Robert

     

    I've handled this by creating a library part with two pins in the schematic

    symbol.  For the footprint, I place two pads on top of each other (either

    SMT or through-hole).

     

    You can use this part in your schematic, connecting AGND to one pin and GND

    to the other pin.  In the layout, you will neatly get the pad with an air

    wire to both AGND and GND, but no other air wires between AGND and GND.

     

    Of course, DRC will complain loudly about the overlapping pads.  I always

    look through the list of errors, and ignore the ones relating to the

    overlapping pads.  WIth V5, you can now "approve" these errors so you only

    have to look at them once.

     

    Regards,

     

    Bert Menkveld

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago

    "Hemant" <mhamalhemant@gmail.com> wrote in message

    news:g0bftc$1hj$1@cheetah.cadsoft.de...

    Hello everyone ! I made a two layer pcb in which there are analog &

    digital ics so , I made two gnd signals naming AGND & GND . Now I

    want to connect these two signals at only at the gnd pin of power

    connector. When I tried to naming these signals in Eagle I can give

    only one name to that net  , But don't want That ? I want separate

    signals.

     

    Robert wrote:

    The net lines on your schematic represent an electrical connection

    and once you connect 2 nets together they are automatically merged

    into a single net which can only have one name. Most, if not all,

    ECAD s/w works like that.

    So, how do you solve the common problem of 2 or more ground nets that

    need to be connected together at a single point? Well, here's how I

    do it, but I'm not saying it's the best or the only solution image

     

    - on the schematic, stick to separate nets and connect only one net

    to your power pin (e.g. the GND net)

    - on the schematic add a 2-pin jumper part, connect pin 1 to GND and

    pin 2 to AGND

    - when routing the PCB, place the jumper with pin 1 as close as

    possible to your power GND pin.

    - route the entire board and run a DRC once finished, correct DRC

    errors if any until the board is OK

    - now "violate" the design rules by shorting pins 1 & 2 of the

    jumper. Be aware that this will generate a DRC clearance error, but

    simply ignore it.

    If you dont want to use the jumper principle just leave GND and AGND

    as 2 separate nets on the schematic and connect only GND to your

    power pin. When routing the PCB, add a via with net name AGND

    somewhere close to the power pin and route the AGND net, including

    the via. Again, when routed 100% and DRC errors free, "violate" the

    design rules and connect AGND also to your power pin by routing a

    trace from the via to the power pin. Alternatively, delete the via

    and connect the open AGND track simply to the power pin.

    If anybody here knows of a better or simplier way to solve this common

    problem, I too would be very happy to hear about it image

     

    Cheers,

    Robert

     

    I've handled this by creating a library part with two pins in the schematic

    symbol.  For the footprint, I place two pads on top of each other (either

    SMT or through-hole).

     

    You can use this part in your schematic, connecting AGND to one pin and GND

    to the other pin.  In the layout, you will neatly get the pad with an air

    wire to both AGND and GND, but no other air wires between AGND and GND.

     

    Of course, DRC will complain loudly about the overlapping pads.  I always

    look through the list of errors, and ignore the ones relating to the

    overlapping pads.  WIth V5, you can now "approve" these errors so you only

    have to look at them once.

     

    Regards,

     

    Bert Menkveld

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • autodeskguest
    autodeskguest over 17 years ago in reply to autodeskguest

    I usually just place a 0ohm 1206 smt or regular 1/4 watt thru hole resistor

    on the schematic.  One side connects to AGND the other connects to GND.

    When the board is made you can either place a real 0 ohm part on the pads or

    just solder a piece of wire (I like to use my trimmed resistor leads).  My

    wife can never understand what value I see in the little trimmed reisitor

    leads that I keem in a little bag!

     

    --Steve