EAGLE User Chat (English) Package variants with different number of pins
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
  • Replies 2 replies
  • Subscribers 179 subscribers
  • Views 595 views
  • Users 0 members are here
Related

Package variants with different number of pins

Former Member
Former Member over 17 years ago

 

I'm creating a library object for the Atmel ATmega644. This chip is

available in PDIP and TQLP packages. The PDIV vesion has 40 pins, the

TQLP version has 44 pins. The additional pins of the TQLP version are

used for additional Vcc and Gnd connections.

 

How can I have one 'device', using one 'symbol' for both packages ?

I'd like to connect 1 'symbol' pin to multiple 'package' pins.

 

It looks like I get either a good PDIP variant and a TQFP with some pins

not connected or if the symbol has multiple Gnd/Vcc pins the TQFP is

fine and the PDIP has warnings about the unconnected pins.

 

Markus

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

    Markus Baertschi wrote:

    I'm creating a library object for the Atmel ATmega644. This chip is

    available in PDIP and TQLP packages. The PDIV vesion has 40 pins, the

    TQLP version has 44 pins. The additional pins of the TQLP version are

    used for additional Vcc and Gnd connections.

     

    How can I have one 'device', using one 'symbol' for both packages ?

    I'd like to connect 1 'symbol' pin to multiple 'package' pins.

     

    It looks like I get either a good PDIP variant and a TQFP with some

    pins not connected or if the symbol has multiple Gnd/Vcc pins the

    TQFP is fine and the PDIP has warnings about the unconnected pins.

     

    Markus

     

    I'm afraid you can't get there from here -- you will have to make 2 separate

    devices.  I know it doesn't seem very elegant, so you may have to grit your

    teeth a bit.

     

    If you use a separate symbol for the supply pins, then the symbol for the

    rest of the device can be the same for both devices.

     

    --

    Bert Menkveld

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago

    Markus Baertschi wrote:

    I'm creating a library object for the Atmel ATmega644. This chip is

    available in PDIP and TQLP packages. The PDIV vesion has 40 pins, the

    TQLP version has 44 pins. The additional pins of the TQLP version are

    used for additional Vcc and Gnd connections.

     

    How can I have one 'device', using one 'symbol' for both packages ?

    I'd like to connect 1 'symbol' pin to multiple 'package' pins.

     

    It looks like I get either a good PDIP variant and a TQFP with some

    pins not connected or if the symbol has multiple Gnd/Vcc pins the

    TQFP is fine and the PDIP has warnings about the unconnected pins.

     

    Markus

     

    I'm afraid you can't get there from here -- you will have to make 2 separate

    devices.  I know it doesn't seem very elegant, so you may have to grit your

    teeth a bit.

     

    If you use a separate symbol for the supply pins, then the symbol for the

    rest of the device can be the same for both devices.

     

    --

    Bert Menkveld