EAGLE User Chat (English) Package variants with different number of pins
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
  • Replies 2 replies
  • Subscribers 179 subscribers
  • Views 589 views
  • Users 0 members are here
Related

Package variants with different number of pins

Former Member
Former Member over 17 years ago

 

I'm creating a library object for the Atmel ATmega644. This chip is

available in PDIP and TQLP packages. The PDIV vesion has 40 pins, the

TQLP version has 44 pins. The additional pins of the TQLP version are

used for additional Vcc and Gnd connections.

 

How can I have one 'device', using one 'symbol' for both packages ?

I'd like to connect 1 'symbol' pin to multiple 'package' pins.

 

It looks like I get either a good PDIP variant and a TQFP with some pins

not connected or if the symbol has multiple Gnd/Vcc pins the TQFP is

fine and the PDIP has warnings about the unconnected pins.

 

Markus

 

  • Sign in to reply
  • Cancel
Parents
  • Richard_H
    Richard_H over 17 years ago

    Markus Baertschi schrieb:

     

    I'm creating a library object for the Atmel ATmega644. This chip is

    available in PDIP and TQLP packages. The PDIV vesion has 40 pins, the

    TQLP version has 44 pins. The additional pins of the TQLP version are

    used for additional Vcc and Gnd connections.

     

    How can I have one 'device', using one 'symbol' for both packages ?

    I'd like to connect 1 'symbol' pin to multiple 'package' pins.

     

    It looks like I get either a good PDIP variant and a TQFP with some pins

    not connected or if the symbol has multiple Gnd/Vcc pins the TQFP is

    fine and the PDIP has warnings about the unconnected pins.

     

    Markus

     

     

    Sorry, but it is not possible to have 1 pin tied to more than 1

    pads. You have to define two different devices.

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/faq.htm

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Richard_H
    Richard_H over 17 years ago

    Markus Baertschi schrieb:

     

    I'm creating a library object for the Atmel ATmega644. This chip is

    available in PDIP and TQLP packages. The PDIV vesion has 40 pins, the

    TQLP version has 44 pins. The additional pins of the TQLP version are

    used for additional Vcc and Gnd connections.

     

    How can I have one 'device', using one 'symbol' for both packages ?

    I'd like to connect 1 'symbol' pin to multiple 'package' pins.

     

    It looks like I get either a good PDIP variant and a TQFP with some pins

    not connected or if the symbol has multiple Gnd/Vcc pins the TQFP is

    fine and the PDIP has warnings about the unconnected pins.

     

    Markus

     

     

    Sorry, but it is not possible to have 1 pin tied to more than 1

    pads. You have to define two different devices.

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/faq.htm