EAGLE User Chat (English) RF Layout Help
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
  • Replies 0 replies
  • Subscribers 177 subscribers
  • Views 239 views
  • Users 0 members are here
Related

RF Layout Help

autodeskguest
autodeskguest over 17 years ago

Hello,

 

I am using the lite version of Eagle, and I would like to create an RF

circuit layout that includes microstrip transmission lines.  These will be

areas of metal on the top layer that will connect to other components like

matching capacitors etc.

 

I am trying to figure out how to connect these RF transmission lines to the

rest of the circuit and maintain

sync with the schematic. Some of the RF design simulators I work with can

create a DXF output of the matching circuit, which can be imported into

Eagle. I have tried to use one of the DXF to Eagle script converters to

import such a file, but when I do this I lose forward&back annotation with

my schematic. I want to maintain this.  The other option I am thinking about

is to create an actual library part for the matching circuit, and a

schematic representation of such, thus allowing me to sync the schematic and

the board layout together- but this strikes me as a rather time consuming

approach, especially considering that the RF circuit undergoes many

iterations, thus forcing me to have to make a new library part each time.

 

I have included an attachment of an example of an RF circuit which I am

trying to lay out.

 

Thanks for your help,

 

Richard

 

 

 

 

Attachments:
imageRF Layout Example.pdf