EAGLE User Chat (English) frazzled routing dense boards
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
  • Replies 3 replies
  • Subscribers 180 subscribers
  • Views 333 views
  • Users 0 members are here
Related

frazzled routing dense boards

autodeskguest
autodeskguest over 17 years ago

Using both EAGLE v4.16r2 and v5.2, I have routed relatively simple 2 and

4 layer boards, using mostly digital logic chips and CPLDs.  I used both

through-hole and SMD parts.  And except for bypass caps, all parts are

mounted on the top (layer 1).  I've gotten pretty good at doing these

low density digital boards.

 

However, I recently routed a small 4 layer analog/digital board (EAGLE

v5.2) that has dozens of components on each side.  This board was far

more dense than any boards that I had done before.  With both the top

and bottom layers active (1 & 16), plus a spaghetti bowel of airwires, I

had some problems positioning the parts and routing the board, and I

became quite frustrated with myself and sometimes with EAGLE.  Sometimes

it hard to know if an airwire is connected to a pad, or if it's merely

passing over a pad.  I'm hoping that someone has a better, less

frustrating approach or strategy to dense board design, and who would

willing to share some tricks of the trade.

Thanks!

 

-Dave Pollum

 

 

  • Sign in to reply
  • Cancel
Parents
  • nickds1
    nickds1 over 17 years ago

    .....

     

    I have to say that for dense boards I now use Electra, which on the whole,

    is very good and EXTREMELY fast.

     

    However, Electra is not completely bug free - is anything? I just found one

    annoying one with mixed power/signal layers which, although not producing

    errors, resulted in suboptimal optimisation. However, their support is good

    and they fix stuff when its broken.

     

    Eagle's autorouter is good, but very slow and single threaded - on the

    boards I'm working on at the moment, I estimate that Eagle is at least 15 -

    20 times slower than Electra, and possibly a lot more - both are running on

    the same host using XP Pro with 4Gb RAM.

     

    Nick

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • nickds1
    nickds1 over 17 years ago

    .....

     

    I have to say that for dense boards I now use Electra, which on the whole,

    is very good and EXTREMELY fast.

     

    However, Electra is not completely bug free - is anything? I just found one

    annoying one with mixed power/signal layers which, although not producing

    errors, resulted in suboptimal optimisation. However, their support is good

    and they fix stuff when its broken.

     

    Eagle's autorouter is good, but very slow and single threaded - on the

    boards I'm working on at the moment, I estimate that Eagle is at least 15 -

    20 times slower than Electra, and possibly a lot more - both are running on

    the same host using XP Pro with 4Gb RAM.

     

    Nick