EAGLE User Chat (English) Net Classes
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
  • Replies 0 replies
  • Subscribers 177 subscribers
  • Views 189 views
  • Users 0 members are here
Related

Net Classes

autodeskguest
autodeskguest over 17 years ago

This question is somewhat related to the previous post about high-current

traces.

 

So have a net class called High Current which defines the trace width of

0.100" and have labeled the associated nets on the schematic as such. The

autorouter then routes these traces with the specified net class parameters.

 

Here's the problem..... I have some components connected to these net

classes which do not need the class definition associated with the net. Here

is an example: I have high current +24V going through a relay an am using

the same +24V source for the relay coil. The coil does not need to same

trace width as the relay contact points.

 

So, my question is, how would I specifiy a net alias with a different class?

 

I can solve this by placing a component like 0 ohm link and then changing

the class on the other side of the component. But i would like a cleaner

solution that does not require redundant components.

 

TIA.

Eldon R. Hiebert