EAGLE User Chat (English) Parts Libraries and Vendor parts list to simplify odering parts
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
  • Replies 13 replies
  • Subscribers 179 subscribers
  • Views 1395 views
  • Users 0 members are here
Related

Parts Libraries and Vendor parts list to simplify odering parts

autodeskguest
autodeskguest over 17 years ago

I am looking for a means to make ordering parts that I use in designing PCBs

easier.  It seems to me that an addition to the library of manufacturer and

part number would be useful.  Or possibly a spreadsheet showing the library

and part number with manufacturer and part number.

 

I would be happy to colaborate on making a comprehensive list of this nature

with others who use Eagle CAD.  This would save us all a ton of time in the

long run.  Maybe Mouser and Digi-key as well as other vendors could be

specified.

 

Any ideas?  Anybody want to work on this with me?  Has this already been

done?  If so, where can I get ahold of the results?

 

Please feel free to email me at

 

Tim

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

    Wouter Mense wrote:

    On Wed, 08 Oct 2008 22:22:01 +0200, Joerg

    <notthisjoergsch@removethispacbell.net> wrote:

     

    Tim wrote:

    Would anyone like to divide up the libraries between us and start

    putting in part numbers once we figure out the use of the extra

    fields in the library that Joerg mentioned?

     

     

    IMHO for R and C values this would not be the best way to go about it as you

    then need a separate R , C value for each defined value tolerance, material

    combination, etc.

     

    Anyhow, be careful. For example, there are literally dozens of part

    numbers for, say, the ubiquitous 0.1uF 0805 cap. Some folks need a

    higher voltage and can live with Z5U ceramic, others don't need high

    voltage but almost get a heart attack if the ceramic material isn't at

    least X7R.

    And also resistors. It would be nice if there was a way to also take

    into account the value in order to generate a part number. Like just put

    in the required specifications and suitable parts are loaded from the

    ordercode database or something.

     

    Have a look at the BOM-am series of ULPs- available from the cadsoft

    download area I believe

     

    What I'd suggest is that you develop external databases to use with the

    BOM-Am series of ULP's.  You then need to define a standard format for

    adding the fields to the parts in the sch/brd,and then these keys are used

    to look up the BOM-am database via the ULP.  Not sure how this works with v5

     

    The data base is also much easier to maintain as it is essentially in  a

    format that can be edited in excel or a.n. other spreadsheet.

     

    cheers

     

    David

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago

    Wouter Mense wrote:

    On Wed, 08 Oct 2008 22:22:01 +0200, Joerg

    <notthisjoergsch@removethispacbell.net> wrote:

     

    Tim wrote:

    Would anyone like to divide up the libraries between us and start

    putting in part numbers once we figure out the use of the extra

    fields in the library that Joerg mentioned?

     

     

    IMHO for R and C values this would not be the best way to go about it as you

    then need a separate R , C value for each defined value tolerance, material

    combination, etc.

     

    Anyhow, be careful. For example, there are literally dozens of part

    numbers for, say, the ubiquitous 0.1uF 0805 cap. Some folks need a

    higher voltage and can live with Z5U ceramic, others don't need high

    voltage but almost get a heart attack if the ceramic material isn't at

    least X7R.

    And also resistors. It would be nice if there was a way to also take

    into account the value in order to generate a part number. Like just put

    in the required specifications and suitable parts are loaded from the

    ordercode database or something.

     

    Have a look at the BOM-am series of ULPs- available from the cadsoft

    download area I believe

     

    What I'd suggest is that you develop external databases to use with the

    BOM-Am series of ULP's.  You then need to define a standard format for

    adding the fields to the parts in the sch/brd,and then these keys are used

    to look up the BOM-am database via the ULP.  Not sure how this works with v5

     

    The data base is also much easier to maintain as it is essentially in  a

    format that can be edited in excel or a.n. other spreadsheet.

     

    cheers

     

    David