EAGLE User Chat (English) No Connect Symbol
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
  • Replies 1 reply
  • Subscribers 177 subscribers
  • Views 1002 views
  • Users 0 members are here
Related

No Connect Symbol

autodeskguest
autodeskguest over 17 years ago

Does EAGLE have a no connect symbol to assign unused pins on the

schematic?  Whenever I run an ERC it throws allkinds of warnings for

unconnected pins.  Although not a show stopper, it does become annoying

at times.

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    On Wed, 29 Oct 2008, Eagle User wrote to us saying :

    Does EAGLE have a no connect symbol to assign unused pins on the

    schematic?

     

    No, but there's no reason you couldn't make one. Or you could use a test

    point. That will create an object on the board, but it could be just a

    tiny copper dot, which is hardly a major issue.

     

    Whenever I run an ERC it throws allkinds of warnings for

    unconnected pins.  Although not a show stopper, it does become annoying

    at times.

     

    Yes, I've had that. In one specific case (a thermocouple amplifier) that

    has pins for two "unused" resistors, I just put the resistors on the

    schematic with a value of "do not fit".

     

    However, you should be aware that Eagle normally only complains about

    pins that are marked on the library component so as to suggest that it's

    probably bad practice to leave them floating. If the pin is explicitly

    marked as an output, Eagle won't usually object. If it's an input then

    it shouldn't be left floating.

    --

    Rob Pearce                       http://www.bdt-home.demon.co.uk

     

    The contents of this | Windows NT crashed.

    message are purely   | I am the Blue Screen of Death.

    my opinion. Don't    | No one hears your screams.

    believe a word.      |