EAGLE User Chat (English) Advice on BGA device pad design , layout and routing...
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
  • Replies 8 replies
  • Subscribers 178 subscribers
  • Views 1294 views
  • Users 0 members are here
Related

Advice on BGA device pad design , layout and routing...

autodeskguest
autodeskguest over 17 years ago

All,

 

I've been using through-hole and lately SMD devices extensively on one

and two layer boards, but I'm about to make my first foray into (what I

consider to be ) big BGA components and thats pushing me to 4 layers

(hopefully not higher) boards and more complexity.

 

So I'm looking for experienced viewpoints... since the excercies has

brought several questions up when I've been thinking about this...

 

- I have a 289 pin MAPBGA device (a freescale i.MX21 processor), that

I've created a footprint for , its a 0.8mm pitch part (there is a 0.65mm

version too... yikes), the pad layout seems pretty straightforward,

there is a 7x7 central cluster of pads, surrounded by a 2 pad space then

a 4 deep row of pads around the periphery of the chip.

 

- the recommendations for solder mask seem to be make the mask slightly

smaller than the pads (, balls = 30mil diameter, pads=30mil, mask=25mil)

to encourage good reflow of the solder balls.

 

- Next comes the routing and layout of the board..., can I create a

package with pads in a figure 8 shape (sometimes called dog-bone),  one

end being the pad the other being a via to one of the four layers of my

board or a simple connection to this layer and out to the rest of the board.

 

- I think I can get away with a 4 layer board, 4 layers should be enough

for me to route all the pins I need, BUT... will the board houses allow

me to put a bunch of signals on the two internal layers that they seem

to expect are power supply and ground planes..., is this just

terminology/convention or is there a real limitation here. I'd be

bringing those signals up or down to the conventional two layers as soon

as practical but there won't be ONLY VCC and GND on those middle layers

 

- Most of these signals are fairly low frequency, apart from the LCD TFT

driver signals...  so hopefully I won;t run into layout issues for

signa/noise problems.

 

- I really don't want to have to think about a 6 layer design since that

means a more expensive Eagle license and a more expensive board

manufacturing cost.. this is all hobby based stuff..

 

I'm calling for the voice of experience with this and any related issues

you've run into ....

 

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

    Matthias Weisser wrote:

    Bert Menkveld schrieb:

    all the proper equipment they had (including X-ray inspection).  I

    don't think BGA assembly is suited for hobbyist DIY assembly.  Are you

    sure you

     

    Do you know http://www.lrr.in.tum.de/~acher/bga/index.html? It is in

    German but maybe you get an idea of how to solder a BGA with an electric

    iron and some other simple stuff most of us have at home.

     

     

    If you type the link into the Google search window and search for it,

    you will get only one hit - Then click on the 'Translate this page' link

    and you will get the webpage (somewhat) translated into English. It is

    good enough to get a pretty good idea of what is being said.

     

    Jack

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago

    Matthias Weisser wrote:

    Bert Menkveld schrieb:

    all the proper equipment they had (including X-ray inspection).  I

    don't think BGA assembly is suited for hobbyist DIY assembly.  Are you

    sure you

     

    Do you know http://www.lrr.in.tum.de/~acher/bga/index.html? It is in

    German but maybe you get an idea of how to solder a BGA with an electric

    iron and some other simple stuff most of us have at home.

     

     

    If you type the link into the Google search window and search for it,

    you will get only one hit - Then click on the 'Translate this page' link

    and you will get the webpage (somewhat) translated into English. It is

    good enough to get a pretty good idea of what is being said.

     

    Jack