Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) Laying out Ethernet
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 187 subscribers
  • Views 277 views
  • Users 0 members are here
Related

Laying out Ethernet

autodeskguest
autodeskguest over 17 years ago

Hi all,

 

I would like -- probably quite stupidly -- to ask if anyone has built a

working Ethernet device using only a dual-layer board.  All the appnotes

seem to assume you have multiple power and ground planes, which pretty

much assumes a four-layer board or more.  I'm assuming an integrated

MAC-PHY chip and a magjack here, so at least the number of spans on the

board is only one, as opposed to three.

 

It would be good to hear how critical placement is and if there is any

particularly good/bad ways to do it.

 

Additionally, most modern silicon is available only in very small

packages (typically 0.5 mm TQFP and so on.)  Anyone has any suggestion

for how best to deal with the change from an inch-based grid (for the

larger components) to a metric grid (for the small ones)?  This has to

fit into a Eurocard chassis, completely with a B/AB connector, so using

an all-metric grid is unfortunately not possible (although "everything

except the connector is on a metric grid", of course, is.)

 

Many thanks,

 

     -hpa

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    On Wed, 10 Dec 2008 17:30:04 -0800, H. Peter Anvin wrote:

     

    Hi all,

     

    I would like -- probably quite stupidly -- to ask if anyone has built a

    working Ethernet device using only a dual-layer board.  All the appnotes

    seem to assume you have multiple power and ground planes, which pretty

    much assumes a four-layer board or more.  I'm assuming an integrated

    MAC-PHY chip and a magjack here, so at least the number of spans on the

    board is only one, as opposed to three.

     

    It would be good to hear how critical placement is and if there is any

    particularly good/bad ways to do it.

     

    Additionally, most modern silicon is available only in very small

    packages (typically 0.5 mm TQFP and so on.)  Anyone has any suggestion

    for how best to deal with the change from an inch-based grid (for the

    larger components) to a metric grid (for the small ones)?  This has to

    fit into a Eurocard chassis, completely with a B/AB connector, so using

    an all-metric grid is unfortunately not possible (although "everything

    except the connector is on a metric grid", of course, is.)

     

    Many thanks,

     

         -hpa

     

    You might want to have a look at the XPort and/or the WIZnet devices.

    Both have plain-vanilla through-hole mounting, and provide both PHY and

    MAC layers. All the necessary smarts are built into the sockets

    themselves.

     

    As for mixed English/metric boards, my suggestion would be to position

    the English parts and lock them down, then switch to metric and position

    those parts. As has been mentioned here before, when laying out boards

    with differently-gridded parts, the best bet is to do the layout from the

    coarsest part until you're almost ready to make the final connection,

    then finish the layout from the finely-gridded part to the endpoint of

    the track as indicated by the high-quality graphic below image

     

    ----


    X  

    --


    X<[E]

     

    Hope this helps...

     

    Dave Merriman