EAGLE User Chat (English) .DRL is different than the .DRD File
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
  • Replies 2 replies
  • Subscribers 181 subscribers
  • Views 726 views
  • Users 0 members are here
Related

.DRL is different than the .DRD File

Former Member
Former Member over 17 years ago

Hi all,

 

I thought I remembered a posting about this but am unable to find it. When I

generate the drill files and run the drill configuration ULP, the drill file

(/DRD)  has 13 tools and the drill wheel (.DRL) has only 12.  Is this

because tools 7 & 8 would share a common size?

 

Thanks ~ Terri

 

 

.DRL

 

T01 0.028in

T02 0.031in

T03 0.032in

T04 0.035in

T05 0.039in

T06 0.040in

T07 0.043in

T08 0.047in

T09 0.067in

T10 0.098in

T11 0.120in

T12 0.126in

 

.DRD

 

M48

M72

T01C0.0276

T02C0.0315

T03C0.0320

T04C0.0354

T05C0.0394

T06C0.0400

T07C0.0430

T08C0.0433

T09C0.0472

T10C0.0669

T11C0.0980

T12C0.1200

T13C0.1260

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • Richard_H
    Richard_H over 17 years ago

    Terri Miller schrieb:

    Hi all,

     

    I thought I remembered a posting about this but am unable to find it. When I

    generate the drill files and run the drill configuration ULP, the drill file

    (/DRD)  has 13 tools and the drill wheel (.DRL) has only 12.  Is this

    because tools 7 & 8 would share a common size?

     

    Thanks ~ Terri

     

     

    .DRL

     

    T01 0.028in

    T02 0.031in

    T03 0.032in

    T04 0.035in

    T05 0.039in

    T06 0.040in

    T07 0.043in

    T08 0.047in

    T09 0.067in

    T10 0.098in

    T11 0.120in

    T12 0.126in

     

    .DRD

     

    M48

    M72

    T01C0.0276

    T02C0.0315

    T03C0.0320

    T04C0.0354

    T05C0.0394

    T06C0.0400

    T07C0.0430

    T08C0.0433

    T09C0.0472

    T10C0.0669

    T11C0.0980

    T12C0.1200

    T13C0.1260

     

     

     

    The drl file has a precision of 3 digits, the integrated drill

    table of the EXCELLON drd file 4 digits.

    The values 0.0430 and 0.0433 willbe rounded and result in a

    common value of 0.043 in the drl file.

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

    CadSoft Support -- hotline@cadsoft.de

    FAQ: http://www.cadsoft.de/faq.htm

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Richard_H
    Richard_H over 17 years ago

    Terri Miller schrieb:

    Hi all,

     

    I thought I remembered a posting about this but am unable to find it. When I

    generate the drill files and run the drill configuration ULP, the drill file

    (/DRD)  has 13 tools and the drill wheel (.DRL) has only 12.  Is this

    because tools 7 & 8 would share a common size?

     

    Thanks ~ Terri

     

     

    .DRL

     

    T01 0.028in

    T02 0.031in

    T03 0.032in

    T04 0.035in

    T05 0.039in

    T06 0.040in

    T07 0.043in

    T08 0.047in

    T09 0.067in

    T10 0.098in

    T11 0.120in

    T12 0.126in

     

    .DRD

     

    M48

    M72

    T01C0.0276

    T02C0.0315

    T03C0.0320

    T04C0.0354

    T05C0.0394

    T06C0.0400

    T07C0.0430

    T08C0.0433

    T09C0.0472

    T10C0.0669

    T11C0.0980

    T12C0.1200

    T13C0.1260

     

     

     

    The drl file has a precision of 3 digits, the integrated drill

    table of the EXCELLON drd file 4 digits.

    The values 0.0430 and 0.0433 willbe rounded and result in a

    common value of 0.043 in the drl file.

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

    CadSoft Support -- hotline@cadsoft.de

    FAQ: http://www.cadsoft.de/faq.htm