Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) USB microscopes are better than i thought for that cost...
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 188 subscribers
  • Views 366 views
  • Users 0 members are here
Related

USB microscopes are better than i thought for that cost...

autodeskguest
autodeskguest over 17 years ago

(Just another tip)

 

I bought a small "USB Microscope", Manufacturer "Shenzhen".

 

Turned out to be useful image

 

It was very easy to get going in Mandriva Linux, full functionality.

Basically just plug it in and the Video for Linux was automatically working.

Installed the program luvcview to get live video with exposure control

etc, snapshot images and video recording.

See http://forum.mandriva.com/viewtopic.php?t=101155

 

(Weird that manufacturers often forget to mention Linux compatibility)

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    Nick de Smith wrote:

     

    This is a very good device - loads and loads of them are available

    rebranded - I bought mine on eBay for a lot less than you paid - see auction

    280299227851 for an example.

     

    About the same i paid at Tradera image

     

    The inbuilt white LED light ring is very good,

    but can lead to a bit of glare if directed at a perpendicular surface...

    best to use it at a slight angle.

     

    Only complaint is that the light stand and relatively stiff USB cable mean

    that its very easy to knock the camera off focus etc. and that the depth of

    field is not great.

     

    Yes to all that.

    I ponder to dismantle the front half to get it less clumsy, and attach

    it to a better stand.

     

    Sidenote: mine was not manufactured properly, it often lost connection

    to the imager until i opened it and connected the shield properly, it

    was occasionally contacting wrong points when manouvering the camera!

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • nickds1
    nickds1 over 17 years ago

    "Morgan Leijström" <temp@tribun.eu> wrote in message

    news:gk2kpj$bm8$1@cheetah.cadsoft.de...

    (Just another tip)

     

    I bought a small "USB Microscope", Manufacturer "Shenzhen".

     

    Turned out to be useful image

     

    I've been using one of these for about 10 months under windows xp on my

    laptop.

     

    As I get a (little bit) older, I've tended to "long sight", as do most

    people. This has made working on anything smaller than 0805/SOT23 etc. quite

    tricky, and reading the markings on som SMDs is almost impossible.

     

    This is a very good device - loads and loads of them are available

    rebranded - I bought mine on eBay for a lot less than you paid - see auction

    280299227851 for an example. The inbuilt white LED light ring is very good,

    but can lead to a bit of glare if directed at a perpendicular surface...

    best to use it at a slight angle.

     

    Only complaint is that the light stand and relatively stiff USB cable mean

    that its very easy to knock the camera off focus etc. and that the depth of

    field is not great.

     

    In terms of value for money, portability etc. (lives in my laptop bag) I'll

    give it 10/10.

     

    Nick