Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) Noob Frustrated - Can't find a part !
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 190 subscribers
  • Views 3104 views
  • Users 0 members are here
Related

Noob Frustrated - Can't find a part !

e14 Contributor
e14 Contributor over 12 years ago

Hi. I was hoping someone can help a new eagle user.

 

I am trying to create my first schematic and can't find a part I need. It's in an SOT-89 package (MC78L05ACHX). I searched and found a couple Fairchild libraries but they don't have that part in an SOT-89.

 

I will resort to making a part but it seems like a common part so I'm surprised I can find it. Matter of fact I can't find anything in SOT-89. What am I doing wrong ?

 

Any hints on how to search for parts ?

 

Bob

  • Sign in to reply
  • Cancel
Parents
  • mraureliusr
    mraureliusr over 12 years ago

    Have you added more libraries to EAGLE? The default libraries that come with the program are far from complete. I would recommend downloading the Newark part libraries, they have tons of extra parts and many many footprints.

     

    Often you can just use a similar part or a different part with the same footprint, that way your board layout will be identical. Or you can find a part with the same footprint and just edit it to match the pinout of your part.

     

    If you need more help I'm online for a while now!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to mraureliusr

    Hi Alexander,

     

    Yes I downloaded an Element 14 library that has the part but is a different package. I tried using the search function in eagle to find another SOT-89 and it comes back with nothing.

     

    I've designed in ExpressPCB many times and they had Common packages SOT-89, 223, etc.. but since I'm new to the software I don't know how to find a basic 3 pin linear regulator.

     

    I will search on Newark now..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mraureliusr
    mraureliusr over 12 years ago in reply to e14 Contributor

    Bob --

     

    I found a part in SOT-89 that you can add to your library and use in your design. I can email it to you if you want.

     

    EDIT: find it attached.

    Attachments:
    sot-89.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 12 years ago in reply to e14 Contributor

    On 22/02/2014 4:42 p.m., Bob Karr wrote:

    Thank you so much. I found the part from the library you posted.

     

    Is there any way to search for the package type in the ADD component

    screen?

     

    Bob

     

     

      If you wish to search for a package then you should do it from the ADD

    in the board editor as that will search package names.  Once you have

    identified the which libraries contain the package, abort the Add.

     

    You can also do it from the control panel but it is strange and slow on

    the large Eagle library.

    Right click on a Libraries folder and select Search in Folder, entering

    you r search text at the bottom. It search one find at a time as you

    click next.

     

    HTH

    Warren

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mraureliusr
    mraureliusr over 12 years ago in reply to e14 Contributor

    Yes, I just type the package name into the search box at the bottom (not the attributes one) and usually it displays every part in that package. Try typing SOIC8 or SOT-23 for example.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • mraureliusr
    mraureliusr over 12 years ago in reply to e14 Contributor

    Yes, I just type the package name into the search box at the bottom (not the attributes one) and usually it displays every part in that package. Try typing SOIC8 or SOT-23 for example.