EAGLE User Chat (English) Board routing question re. ratsnest
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
  • Replies 1 reply
  • Subscribers 178 subscribers
  • Views 212 views
  • Users 0 members are here
Related

Board routing question re. ratsnest

autodeskguest
autodeskguest over 16 years ago

 

Dear All,

 

I am currently routing a 2 layer board and have run into a problem to which

I am sure there must be a solution.

 

Basically, I have a few signals remaining to be routed. One of these has a

clear path and routing would be simple were it not for one inconvenient

problem; Eagle doesn't seem to want to let me route it that way. I tried

regenerating the ratsnest but that didn't work. What I need to do is force

Eagle to understand that I want to route differently, or just force a manual

route in some way.

 

The solution to this, surely, has to be extremely simple! Can someone give

me some pointers?

 

Thanks

 

Richard H

 

 

 

  • Sign in to reply
  • Cancel
  • Richard_H
    Richard_H over 16 years ago

    Richard Hince schrieb:

    Dear All,

     

    I am currently routing a 2 layer board and have run into a problem to which

    I am sure there must be a solution.

     

    Basically, I have a few signals remaining to be routed. One of these has a

    clear path and routing would be simple were it not for one inconvenient

    problem; Eagle doesn't seem to want to let me route it that way. I tried

    regenerating the ratsnest but that didn't work. What I need to do is force

    Eagle to understand that I want to route differently, or just force a manual

    route in some way.

     

    The solution to this, surely, has to be extremely simple! Can someone give

    me some pointers?

     

    Thanks

     

    Richard H

     

     

     

    The ROUTE command offers several options with the different mouse

    buttons, also in combination with the Ctrl and Shift key.

     

      Ctrl + Left      starts routing at any given point along a wire or via

      Shift + Left     if the airwire begins at an already existing wire and

                       this wire has a different width, the new wire adopts

                       this width 

      Center           selects the layer

      Right            changes the wire bend style

      Shift +Right     reverses the direction of switching bend styles

      Ctrl + Right     toggles between corresponding bend styles

      Shift + Left     places a via at the end point of the wire

      Ctrl + Left      defines arc radius when placing a wire's end point

     

     

    I think Ctrl + Left will solve your problem.....

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

    CadSoft Support -- hotline@cadsoft.de

    FAQ: http://www.cadsoft.de/faq.htm