Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) Eagle Software
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 45 replies
  • Subscribers 191 subscribers
  • Views 5043 views
  • Users 0 members are here
  • eagle
  • software
Related

Eagle Software

e14 Contributor
e14 Contributor over 12 years ago

Greetings

 

My name is Brian, and I am a new user of Eagle, for right now the free version.

 

First question, is there any way to stop Eagle from carrying on point to point connections.   I am sure at times this is a very useful feature, but I need it to stop after automatically after it connects 2 points.   I hope this is possible, as if this is a persistent feature, it will really turn me off to Eagle.

 

But more importantly, I did a practice design and have a problem.

 

I am using a XF2H-3415 surface mount connector, .5 mm spacing.   I have a bit of a problem with the datasheet, as it doesn't clearly state the measurement units, but since the first page notes a measurement in mm, I'm assuming they are smart enough to carry those units throughout the datasheet.

 

Let me describe what I did, and perhaps did not do.

 

I have my board layout done, I have two 12 pin single row headers on each side of the board, and the other connector on the other side.   And I see the Ratsnest.

 

I think the pad color denotes side of board, but I'm not sure how to check or change that.

 

This is where the confusion starts.

 

I can't get the autorouter to start, and I come up with 34 DRC errors.

 

I'm a beginner, probably making a silly mistake, but Eagle also has a much more complicated set of DRC rules than I'm used to.

 

I have attached an image.

 

Help is most appreciated.

 

Thanks

 

Brian K

BKM Engineering

Attachments:
image
  • Sign in to reply
  • Cancel
  • AnalogNotes
    AnalogNotes over 12 years ago in reply to e14 Contributor

    Brian Mcclung wrote:

    How do you change the units.

     

    How do you define the grid in such a way that your measurement steps are smaller than the area to be measured.

     

    Use the grid command.  (Either click on the grid icon, or just type "grid".)  You can set the grid to whatever you want.  There's even a "Finest" button if you really want to go crazy...

     

    But this is even more important, because I tend to be very critical of software.  I'm self taught, with help obviously, but software with a steep learning curve is very distasteful.

     

     

    Some of the best tools have the steepest learning curves, but the climb is worth it...

     

    Why is Eagle not self adjusting, and is this going to be a persistent feature when using Eagle.  Is this something that every time I do a board, I am going to have to go in adjust my design rules?

     

    Pardon me if I'm jumping into the middle of things and missed something, but have you set up your own directory structure yet?  In other words, if you use the EAGLE control panel and go to options->directories, is everything still pointing to something that starts with "$EAGLEDIR"?  I'd suggest changing at least the Design Rules and Projects entries to point to something in your own documents directory.  Copy the default.dru file from the $EAGLEDIR into your own Design Rules directory, and edit it to suit your needs.  Every time you start EAGLE, it will load that file.

     

    It's also probably worth taking a look in the Scripts directory at the eagle.scr file.  A lot of settings can be changed there, and they will be loaded every time...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to dukepro

    Hi Chuck

     

    I'm still having the same problem, but other questions first.

     

    How do you change the units.

     

    How do you define the grid in such a way that your measurement steps are smaller than the area to be measured.

     

    Back to my original problem.

     

    I checked the parameter I think you specified, and the size is already set to 10 mils.

     

    But this is even more important, because I tend to be very critical of software.   I'm self taught, with help obviously, but software with a steep learning curve is very distasteful.

     

    What I want to know is if these errors are caused by a design rule, why is Eagle not self adjusting to what is a standard part.

     

    Why is Eagle not self adjusting, and is this going to be a persistent feature when using Eagle.  Is this something that every time I do a board, I am going to have to go in adjust my design rules?

     

    I'm really hoping I'm misunderstanding something here.

     

    Thanks

     

    Brian

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to autodeskguest

    That was the problem.

     

    Thank you very much.

     

    Brian K

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 12 years ago

    On 13/03/14 05:49, Brian Mcclung wrote:

    First question, is there any way to stop Eagle from carrying on point to

    point connections.   I am sure at times this is a very useful feature,

    but I need it to stop after automatically after it connects 2 points. 

     

    I'm guessing your context because you don't say, but if this is in the

    schematic editor you've probably fallen into the mistake of using the

    "wire" tool when you should be using the "net" tool. They seem at first

    sight to behave similarly but the latter is the correct one for

    connecting up pins that are electrically connected. It also has the

    useful feature of automatically stopping the net when you click on a

    pin, and automatically adding a junction when you start or end a new

    segment on an existing net.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dukepro
    dukepro over 12 years ago

    Good morning, Brian,

     

    On 03/13/2014 01:49 AM, Brian Mcclung wrote:

    ...

    First question, is there any way to stop Eagle from carrying on point to

    point connections.

     

    Not sure of your context here.  If it has to do with the autorouter, I

    can't help.  I don't use it.

     

    I am using a XF2H-3415 surface mount connector, .5 mm spacing.

    ...

    I have my board layout done, I have two 12 pin single row headers on

    each side of the board, and the other connector on the other side.   And

    I see the Ratsnest.

     

    I think the pad color denotes side of board, but I'm not sure how to

    check or change that.

    The default colors are red for the top layer (layer 1), and blue for the

    bottom layer (layer 16).  All SMD parts are designed in the library to

    go on the top.  The part can then be mirrored in the board design to

    place it on the bottom.

     

    This is where the confusion starts.

     

    I can't get the autorouter to start,and I come up with 34 DRC errors.

    The Width error you're getting is because the pads are narrower than the

    minimum width setting in DRC.  Go to DRC=>Sizes and change the minimum

    width.  The datasheet recommends a 0.25mm minimum width.  Go ahead and

    enter "0.25mm" in this field and click Apply.

     

    In general, the DRC settings should be the greater of the limitations of

    the board fabrication house, and your design requirements.  Each fab

    house should publish these limitations, usually under "capabilities".

     

    DRC also pays attention to your Class settings.  Each net can be

    assigned a Class that describes further restrictions on wires of that

    class.  DRC will use the greater of the values assigned in the DRC

    settings and those of the net's class.  For instance, your DRC settings

    may define a minimum trace width of 8 mils, and a minimum clearance of 8

    mils, which is fine for signal level wires.  Our designs sometimes use

    high voltages close to 3,000 V.  I assign HV nets to a "HighVoltage"

    class and force a clearance of 40 mils.

     

    You may wish to add a high current class for power supply wires and give

    them a relatively large width and drill size.

     

    Your board layout alone does not indicate a need for such classes.

     

    As far as not being able to start the auto-router, this problem may be

    related to the fact that there's a DRC error on every pad.

     

    I'm a beginner, probably making a silly mistake, but Eagle also has a

    much more complicated set of DRC rules than I'm used to.

     

    There's one other very important point I need to make.  The hashed black

    and yellow bar across the top indicates that forward and back annotation

    has been severed.  This is caused by closing the schematic while working

    on the board, or vice versa.  When working on a design both the

    schematic and board editors should be open.  This allows changes to in

    one editor to be reflected in the other.

     

    To restore consistency, run "ERC" from .  The resulting report will

    identify the differences between the board and the schematic.  If there

    are any differences, these need to be fixed before consistency is restored.

     

    More of a personal preference, I would suggest using a black background

    on the board editor, and a white background on the schematic editor.

    This can be changed in Options=>User Interface.

     

    HTH,

        - Chuck

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<