Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) Invite testing of hershey-text.ulp
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 188 subscribers
  • Views 2151 views
  • Users 0 members are here
Related

Invite testing of hershey-text.ulp

autodeskguest
autodeskguest over 12 years ago

Hello,

 

TL;DR: I invite you to help me improve a ULP to render Hershey fonts for

PCBs in EAGLE.  See the ULP downloads section of the Cadsoft website or:

http://www.avon-tech-solutions.co.nz/hershey.html or

https://github.com/nallison/hershey-text-eagle

GROUP the text to render then RUN hershey-text.ulp

 

 

Longer story.

 

Many will recall various threads on how some of us would like "pretty

text" on our pcb "artworks" rather than just using the default vector

font.  For example:

"EAGLE 6 vector font (was: Teaser peek at Version 6 XML Format)",

15-Sep-2011, eagle.userchat.eng

"Addition of a new standardized font", 18-Jan-2012, user.suggest.eng

 

Having used "other" CAD applications that produced more visually

appealing fonts in the silkscreen, I've always wanted to develop a

"Pretty Text" ULP for my pcb design work.  A few weeks ago I discovered

an Inkscape extension that uses Hershey fonts for engraving.  I already

knew about the copy-text-as-wire.ulp and I thought it would be possible

to combine these approaches for EAGLE.

 

So, I've written hershey-text.ulp to render text in Hershey fonts using

wires.  My goal was to convert smashed reference designators (tNames) or

text on any copper, stop, milling or silkscreen layer into any Hershey

font.  I wanted to be able to adjust the slope and stroke (wire) width.

  Rather than render text directly on the layer, the default ULP options

"automagically" make a package of the wires comprising the Hershey font

and then add it to the board at the text insertion point.  Of course,

directly rendering it in the board is possible.

 

I've modified a copy of the futural.jhf simplex font to produce

eagles.jhf that also includes some characters from the extend ascii

range present in the EAGLE fonts: 169 copyright, 176 degree, 177

plus-minus, 181 micro, 216 diameter, 219 Ohm/omega.

 

I have produced gerber outputs using rowmant.jhf and eagles.jhf fonts

that I think are satisfactory but I've not sent the boards to be

manufactured yet.  I choose to put the Hershey text on user layers, e.g.

121, 125, etc, and change the CAM job layer settings to match this.

 

I offer the ULP in the hope it might be useful for others.  I invite

other EAGLE users to test it and suggest improvements.  I developed this

ULP in v5.10 and v5.12 Professional on WinXP.  I have made some

preliminary tests on Debian7 with v5.12 Professional and v6.5.0 Light

and I invite you to test using recent versions and/or the GNU/Linux and

Mac platforms.

 

The new text alignment and multi-line facilities of V6 are not currently

supported in the ULP.  I've a conceptual solution but have not started

developing or testing it yet.

 

hershey-text.ulp meets my current needs.  However, I have some ideas to

improve the ULP for others and will do my best to support the ULP as my

commitments allow.   I have also made ULP my first attempt at using

GitHub for a project.  Initially I envisage some incremental

improvements will be available on the GitHub site and only major

advances would be submitted to the Cadsoft ULP downloads area.

 

Comments and suggestions welcome.

 

Kind regards,

Neil

--

Neil Allison

Avon Technical Solutions Ltd

Christchurch, New Zealand

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 12 years ago

    Neil Allison schrieb:

     

    TL;DR: I invite you to help me improve a ULP to render Hershey fonts for

    PCBs in EAGLE.  See the ULP downloads section of the Cadsoft website or:

    http://www.avon-tech-solutions.co.nz/hershey.html or

    https://github.com/nallison/hershey-text-eagle

    GROUP the text to render then RUN hershey-text.ulp

     

    Many thanks, this is a great idea to finally let us see some better text

    on our boards!

     

    However, the ULP obviously ignores text rotation, currently. Maybe that

    can be fixed.

     

    Another suggestion: instead of using a fixed stroke width, it might be

    better to use a percentual width (just as we are used with EAGLEs vector

    font). In my test case, I had a board with several very differently

    sized texts, and in the result part of them were much too fat while

    others were much too thin.

     

    MANY thanks,

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 12 years ago in reply to autodeskguest

    On 01/04/2014 03:06, Tilmann Reh wrote:

     

    However, the ULP obviously ignores text rotation, currently. Maybe that

    can be fixed.

     

    Yes, I have put it on my list of issues.

    https://github.com/nallison/hershey-text-eagle/issues/11

     

    Text rotation is currently supported when the "Make a Package in

    library" option is selected: when the package is added to the board, it

    is inserted with the same "angle" and origin setting as the text.  The

    "spin" setting is not (yet) supported.

     

    But perhaps you want to rotate the text directly without creating a

    package?   I think it is a worthwhile enhancement.

     

    Another suggestion: instead of using a fixed stroke width, it might be

    better to use a percentual width (just as we are used with EAGLEs vector

    font). In my test case, I had a board with several very differently

    sized texts, and in the result part of them were much too fat while

    others were much too thin.

     

    Yes, a very good idea thank you, I've added it to the issues list too:

    https://github.com/nallison/hershey-text-eagle/issues/12

     

    Thank you for taking the time to test and comment on this ULP.

     

    Regards,

    Neil

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 12 years ago in reply to autodeskguest

    Hello Tilmann,

     

    Another suggestion: instead of using a fixed stroke width, it might be

    better to use a percentual width (just as we are used with EAGLEs vector

    font).

     

    Github is updated with a fix for this issue (#12).  As a default, the

    ULP now sets the hershey text stroke (wire) width separately for each

    text item in the group.  It calculates the width from (size * ratio) and

    so is the same as the wires that create the 'source' vector text.

     

    Checkbox and command line options allow one to revert to a fixed width

    for all text.

     

    Kind regards,

    Neil

    https://github.com/nallison/hershey-text-eagle

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 12 years ago in reply to autodeskguest

    Hello Tilmann,

     

    Another suggestion: instead of using a fixed stroke width, it might be

    better to use a percentual width (just as we are used with EAGLEs vector

    font).

     

    Github is updated with a fix for this issue (#12).  As a default, the

    ULP now sets the hershey text stroke (wire) width separately for each

    text item in the group.  It calculates the width from (size * ratio) and

    so is the same as the wires that create the 'source' vector text.

     

    Checkbox and command line options allow one to revert to a fixed width

    for all text.

     

    Kind regards,

    Neil

    https://github.com/nallison/hershey-text-eagle