EAGLE User Chat (English) Autoroute a subset of signals?
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
  • Replies 1 reply
  • Subscribers 180 subscribers
  • Views 409 views
  • Users 0 members are here
Related

Autoroute a subset of signals?

autodeskguest
autodeskguest over 17 years ago

I have 4 groups of signals b1-1 to b1-52, b2-1 to b2-52 etc. Is there a

way to autoroute a subset at a time -just b2-1 to b2-52 for example?

 

I read through the eagle manual (was 4.1) but could not find it.

 

Also tried selecting via the group command but could not get that to work.

 

Thanks

 

Glenn

 

  • Sign in to reply
  • Cancel
  • blewis999
    blewis999 over 17 years ago

    use auto

    then click on the select button

    next click each signal one at a time until you have all the signals

    then click the green stop light on the tool bar

     

    you can do this

     

    auto vdd gnd my_signal1 my signal2

     

    and it will route without clicking

     

    I have not done so for the autorouter but have for setting board

    dimensions,  but I am sure there is a way to write a script or ULP to

    contain the above commands if you want to select the same signals

    using a file

    On Sat, 14 Mar 2009 16:48:24 -0400, Glenn Jones <rg.jones@rogers.com>

    wrote:

     

    I have 4 groups of signals b1-1 to b1-52, b2-1 to b2-52 etc. Is there a

    way to autoroute a subset at a time -just b2-1 to b2-52 for example?

     

    I read through the eagle manual (was 4.1) but could not find it.

     

    Also tried selecting via the group command but could not get that to work.

     

    Thanks

     

    Glenn