EAGLE User Chat (English) Overlapping solder masks
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
  • Replies 1 reply
  • Subscribers 177 subscribers
  • Views 305 views
  • Users 0 members are here
Related

Overlapping solder masks

amerdsp
amerdsp over 16 years ago

Hello again,

   Can someone please enlighten me what pad size would you use for the

package on page one of http://focus.ti.com/lit/ml/mpbg832d/mpbg832d.pdf ?

 

It seems to vary between 0.36 mm and 0.46 mm.  However if I use the

larger value, the default solder masks overlap. They do not overlap if I

use the median value.

 

Also what does 0.15 M with a circle mean?

 

Thank you for all your help.

 

A

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 16 years ago

    On Sat, 21 Mar 2009 08:33:02 +0100, Amer Abufadel <amer.abufadel@gmail.com> wrote:

     

    Hello again,

       Can someone please enlighten me what pad size would you use for the 

    package on page one of http://focus.ti.com/lit/ml/mpbg832d/mpbg832d.pdf ?

     

    It seems to vary between 0.36 mm and 0.46 mm.  However if I use the 

    larger value, the default solder masks overlap. They do not overlap if I 

    use the median value.

    I would just use 0.4mm, since the values given are to indicate the fabrication tolerances. Your fabricated PCB will also have some tolerances so don't make too much of a problem out of it. Also, BGA works best if the pads on the PCB are of the same diameter as those on the BGA chip.

     

    Also what does 0.15 M with a circle mean?

    It is the pad surface area, so approximately 0.15mm².

     

    Thank you for all your help.

     

    A

     

     

     

    --

    Using Opera's revolutionary e-mail client: http://www.opera.com/mail/