Hi,
To create Audio PCB consisting two PCB's one for each channel.
Each channel will be on individual PCB , which will be mounted on heat sink
facing opposite, such that wiring pads are in same position(near to each
other)
Now I create one channel then Mirror the whole board using mirror-board.ulp
But this mirrors the also changes layers of components, also inverts
routing layers, silk etc.
i.e inverts everything and also changes the layout to other side.
What I now do to get desired output (only change layout - mirrored layout),
after I run mirror-board.ulp
I mirror each components , then rotate them in proper position, then
rip-up nets then route again, change layer of polygon etc..
Purpose is to create another PCB with Mirror Layout (with out changing
layers),so that when two PCB are placed opposite to each other, wiring pads
are at same place.
Is There any ULP to this ?
Thanks
suds