EAGLE User Chat (English) Pad Dilema
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
  • Replies 7 replies
  • Subscribers 178 subscribers
  • Views 537 views
  • Users 0 members are here
Related

Pad Dilema

autodeskguest
autodeskguest over 16 years ago

Greetings,

 

I need advice for the following, I attached a 5 KB GIF drawing:

 

I want to place four pads on a board and connect one wire to each pad.

 

I want the four pads to be tied together on top and bottom layers with

either polygons or rectangles or something else.

 

I want the area on the finished board to appear as one big pad with four

through-holes in it. Bare copper with no mask over the area.

 

Each hole will have a wire attached and soldered in the final assembly and

all wires carry the same signal..

 

Should I use polygons or rectangles or something else to make this.

 

Thanks in advance for any help you can give me.

 

 

 

 

 

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 16 years ago

    Biff schrieb:

     

    I want to place four pads on a board and connect one wire to each pad.

     

    I want the four pads to be tied together on top and bottom layers with

    either polygons or rectangles or something else.

     

    I want the area on the finished board to appear as one big pad with four

    through-holes in it. Bare copper with no mask over the area.

     

    Each hole will have a wire attached and soldered in the final assembly and

    all wires carry the same signal..

     

    Should I use polygons or rectangles or something else to make this.

     

    Polygons will serve this purpose best (in the board, not in a library!).

    Don't forget to also draw the stop masks (for those, rectangles will do).

     

    Tilman

    ......................................................

     

    Thanks Tilman,

     

    Here is the complete drawing on the board (see attached GIF).

     

    I have the 4 pads that accept one wire each. The other 2 pads are connected

    to one relay contact. The relay contact has 2 pins on it that's why there

    are 2 pads.

     

    I want all 6 pads connected together on the Top and Bottom layers.

     

    I have Polygons around all 6 pads on Top and Bottom layers.

     

    I have a rectangle around the 6 pads in Tsop and Bstop layers.

     

    Is this the correct way to do this? Do I need to set or apply anything else?

     

    Many Thanks

     

     

     

     

    Attachments:
    image
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 16 years ago

    Biff schrieb:

     

    I want to place four pads on a board and connect one wire to each pad.

     

    I want the four pads to be tied together on top and bottom layers with

    either polygons or rectangles or something else.

     

    I want the area on the finished board to appear as one big pad with four

    through-holes in it. Bare copper with no mask over the area.

     

    Each hole will have a wire attached and soldered in the final assembly and

    all wires carry the same signal..

     

    Should I use polygons or rectangles or something else to make this.

     

    Polygons will serve this purpose best (in the board, not in a library!).

    Don't forget to also draw the stop masks (for those, rectangles will do).

     

    Tilman

    ......................................................

     

    Thanks Tilman,

     

    Here is the complete drawing on the board (see attached GIF).

     

    I have the 4 pads that accept one wire each. The other 2 pads are connected

    to one relay contact. The relay contact has 2 pins on it that's why there

    are 2 pads.

     

    I want all 6 pads connected together on the Top and Bottom layers.

     

    I have Polygons around all 6 pads on Top and Bottom layers.

     

    I have a rectangle around the 6 pads in Tsop and Bstop layers.

     

    Is this the correct way to do this? Do I need to set or apply anything else?

     

    Many Thanks

     

     

     

     

    Attachments: