EAGLE User Chat (English) Pad Dilema
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
  • Replies 7 replies
  • Subscribers 177 subscribers
  • Views 531 views
  • Users 0 members are here
Related

Pad Dilema

autodeskguest
autodeskguest over 16 years ago

Greetings,

 

I need advice for the following, I attached a 5 KB GIF drawing:

 

I want to place four pads on a board and connect one wire to each pad.

 

I want the four pads to be tied together on top and bottom layers with

either polygons or rectangles or something else.

 

I want the area on the finished board to appear as one big pad with four

through-holes in it. Bare copper with no mask over the area.

 

Each hole will have a wire attached and soldered in the final assembly and

all wires carry the same signal..

 

Should I use polygons or rectangles or something else to make this.

 

Thanks in advance for any help you can give me.

 

 

 

 

 

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 16 years ago

    Biff wrote:

    Biff schrieb:

     

    I want to place four pads on a board and connect one wire to each pad.

     

    I want the four pads to be tied together on top and bottom layers with

    either polygons or rectangles or something else.

     

    I want the area on the finished board to appear as one big pad with four

    through-holes in it. Bare copper with no mask over the area.

     

    Each hole will have a wire attached and soldered in the final assembly and

    all wires carry the same signal..

     

    Should I use polygons or rectangles or something else to make this.

     

    Polygons will serve this purpose best (in the board, not in a library!).

    Don't forget to also draw the stop masks (for those, rectangles will do).

     

    Tilman

    .......................................................

     

    Thanks Tilman,

     

    Here is the complete drawing on the board (see attached GIF).

     

    I have the 4 pads that accept one wire each. The other 2 pads are connected

    to one relay contact. The relay contact has 2 pins on it that's why there

    are 2 pads.

     

    I want all 6 pads connected together on the Top and Bottom layers.

     

    I have Polygons around all 6 pads on Top and Bottom layers.

     

    I have a rectangle around the 6 pads in Tsop and Bstop layers.

     

    Is this the correct way to do this? Do I need to set or apply anything else?

     

    Many Thanks

     

     

     

    The polygon needs to be named the same net as the pads to connect. Run

    ratsnest to see the fill.

    Also options such as isolate and width of polygon trace affect what you get.

    Paul R.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 16 years ago

    Biff wrote:

    Biff schrieb:

     

    I want to place four pads on a board and connect one wire to each pad.

     

    I want the four pads to be tied together on top and bottom layers with

    either polygons or rectangles or something else.

     

    I want the area on the finished board to appear as one big pad with four

    through-holes in it. Bare copper with no mask over the area.

     

    Each hole will have a wire attached and soldered in the final assembly and

    all wires carry the same signal..

     

    Should I use polygons or rectangles or something else to make this.

     

    Polygons will serve this purpose best (in the board, not in a library!).

    Don't forget to also draw the stop masks (for those, rectangles will do).

     

    Tilman

    .......................................................

     

    Thanks Tilman,

     

    Here is the complete drawing on the board (see attached GIF).

     

    I have the 4 pads that accept one wire each. The other 2 pads are connected

    to one relay contact. The relay contact has 2 pins on it that's why there

    are 2 pads.

     

    I want all 6 pads connected together on the Top and Bottom layers.

     

    I have Polygons around all 6 pads on Top and Bottom layers.

     

    I have a rectangle around the 6 pads in Tsop and Bstop layers.

     

    Is this the correct way to do this? Do I need to set or apply anything else?

     

    Many Thanks

     

     

     

    The polygon needs to be named the same net as the pads to connect. Run

    ratsnest to see the fill.

    Also options such as isolate and width of polygon trace affect what you get.

    Paul R.